<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic EIM read errors in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/EIM-read-errors/m-p/250536#M22766</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the i.MX6S EIM to interface to an FPGA.&amp;nbsp; I am using 16-bit synchronous reads on a multiplexed A/D bus mostly successfully.&amp;nbsp; Occasionally when the processor core reads a 32-bit word from the FPGA instead of reading the word correctly it reads the first 16 bits twice in a row.&amp;nbsp; I am using the WAIT signal to start the data transfer.&amp;nbsp; I am not using continuous BCLK.&amp;nbsp; The WAIT and DATA signals all transition very close to the falling edge of BCLK.&amp;nbsp; I have tried varying the timing on the WAIT and DATA signals from the FPGA without making any difference.&amp;nbsp; The problem only manifests itself when the processor core is busy with transmitting another file via Ethernet FTP at the same time it is reading data from the FPGA.&amp;nbsp; The problem often disappears completely when I probe the BCLK line.&amp;nbsp; Any suggestions?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Jan 2014 03:23:18 GMT</pubDate>
    <dc:creator>kwise</dc:creator>
    <dc:date>2014-01-23T03:23:18Z</dc:date>
    <item>
      <title>EIM read errors</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EIM-read-errors/m-p/250536#M22766</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the i.MX6S EIM to interface to an FPGA.&amp;nbsp; I am using 16-bit synchronous reads on a multiplexed A/D bus mostly successfully.&amp;nbsp; Occasionally when the processor core reads a 32-bit word from the FPGA instead of reading the word correctly it reads the first 16 bits twice in a row.&amp;nbsp; I am using the WAIT signal to start the data transfer.&amp;nbsp; I am not using continuous BCLK.&amp;nbsp; The WAIT and DATA signals all transition very close to the falling edge of BCLK.&amp;nbsp; I have tried varying the timing on the WAIT and DATA signals from the FPGA without making any difference.&amp;nbsp; The problem only manifests itself when the processor core is busy with transmitting another file via Ethernet FTP at the same time it is reading data from the FPGA.&amp;nbsp; The problem often disappears completely when I probe the BCLK line.&amp;nbsp; Any suggestions?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jan 2014 03:23:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EIM-read-errors/m-p/250536#M22766</guid>
      <dc:creator>kwise</dc:creator>
      <dc:date>2014-01-23T03:23:18Z</dc:date>
    </item>
    <item>
      <title>Re: EIM read errors</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EIM-read-errors/m-p/250537#M22767</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;FYI the errors were caused by a decoupling problem on the RGMII interface.&amp;nbsp; The EIM and RGMII are sharing a power supply and insufficient decoupling caused the RGMII to inject noise onto the EIM supply pins.&amp;nbsp; Since BCLK is fed back as an input and used to clock the input data, noise at just the wrong time caused a double clock.&amp;nbsp; This can be avoided by turning on hysteresis on the BCLK pad.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jan 2014 19:16:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EIM-read-errors/m-p/250537#M22767</guid>
      <dc:creator>kwise</dc:creator>
      <dc:date>2014-01-30T19:16:49Z</dc:date>
    </item>
  </channel>
</rss>