<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Encrypted Bootloader</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Encrypted-Bootloader/m-p/1939000#M227624</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Will reply back to you in another case that is from you.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
    <pubDate>Fri, 23 Aug 2024 06:13:50 GMT</pubDate>
    <dc:creator>Harvey021</dc:creator>
    <dc:date>2024-08-23T06:13:50Z</dc:date>
    <item>
      <title>Encrypted Bootloader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Encrypted-Bootloader/m-p/1938537#M227600</link>
      <description>&lt;P&gt;Support,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have been following the guide &lt;A href="https://github.com/nxp-imx/uboot-imx/blob/lf_v2024.04/doc/imx/ahab/guides/mx8ulp_9x_encrypted_boot.txt" target="_self"&gt;mx8ulp_9x_encrypted_boot.txt&lt;/A&gt;&amp;nbsp;&lt;SPAN&gt;and have encountered an issue.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;In Step:&amp;nbsp;&lt;A href="https://github.com/nxp-imx/uboot-imx/blob/lf_v2024.04/doc/imx/ahab/guides/mx8ulp_9x_encrypted_boot.txt#L211" target="_self"&gt;1.7 Generating the DEK Blob&lt;/A&gt; the instructions state:&amp;nbsp;&lt;/P&gt;&lt;P&gt;Copy dek_2 and dek_3 to the i.MX8ULP or 9x and run the following commands from&lt;BR /&gt;U-Boot prompt. Boot the flash.bin generated earlier with mkimage on board. Halt at&lt;BR /&gt;U-Boot and connect to host computer with USB Mass Storage (UMS):&lt;/P&gt;&lt;P&gt;mmc2(part 0) is current device&lt;BR /&gt;flash target is MMC:2&lt;BR /&gt;Net: eth0...&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any Key to stop autoboot: 0&lt;BR /&gt;=&amp;gt; ums 0 mmc 2:1&lt;BR /&gt;&lt;BR /&gt;Copy both DEK over to the board using the computer's file system. Now use fatload&lt;BR /&gt;and dek_blob to create and encapsulate the DEK blob.&lt;BR /&gt;=&amp;gt; mmc list&lt;BR /&gt;FSL_SDHC: 1&lt;BR /&gt;FSL_SDHC: 2 (eMMC)&lt;BR /&gt;=&amp;gt; fatload mmc 2:1 0x80280000 dek_2.bin&lt;BR /&gt;=&amp;gt; dek_blob 0x80280000 0x80281000 128&lt;BR /&gt;=&amp;gt; fatwrite mmc 2:1 0x80281000 dek_blob2.bin 0x48&lt;BR /&gt;=&amp;gt; fatload mmc 2:1 0x80280000 dek_3.bin&lt;BR /&gt;=&amp;gt; dek_blob 0x80280000 0x80281000 128&lt;BR /&gt;=&amp;gt; fatwrite mmc 2:1 0x80281000 dek_blob3.bin 0x48&lt;/P&gt;&lt;P&gt;Use UMS to copy the dek blobs back to the host PC. In host PC copy the generated&lt;BR /&gt;dek_blob binaries to the CST directory.&lt;/P&gt;&lt;P&gt;--&lt;/P&gt;&lt;P&gt;My question is: Can the above procedure be done using MFGTool &lt;STRONG&gt;uuu&lt;/STRONG&gt; directly to copy the DEK blob back and forth? If yes, what are the &lt;STRONG&gt;uuu&lt;/STRONG&gt; commands?&lt;/P&gt;&lt;P&gt;Additionally, I am trying to understand how this procedure will affect the mass manufacturing process. Is there any guide we can provide to the manufacturer so they can understand the process when flashing the OS to the board together with encrypted bootloader?&lt;/P&gt;&lt;P&gt;Your assistance in this matter would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;</description>
      <pubDate>Thu, 22 Aug 2024 14:19:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Encrypted-Bootloader/m-p/1938537#M227600</guid>
      <dc:creator>pilotnite</dc:creator>
      <dc:date>2024-08-22T14:19:38Z</dc:date>
    </item>
    <item>
      <title>Re: Encrypted Bootloader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Encrypted-Bootloader/m-p/1939000#M227624</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Will reply back to you in another case that is from you.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Fri, 23 Aug 2024 06:13:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Encrypted-Bootloader/m-p/1939000#M227624</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2024-08-23T06:13:50Z</dc:date>
    </item>
    <item>
      <title>Re: Encrypted Bootloader</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Encrypted-Bootloader/m-p/1939206#M227628</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/192970"&gt;@Harvey021&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Fri, 23 Aug 2024 10:46:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Encrypted-Bootloader/m-p/1939206#M227628</guid>
      <dc:creator>pilotnite</dc:creator>
      <dc:date>2024-08-23T10:46:56Z</dc:date>
    </item>
  </channel>
</rss>