<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Can a HAB Encrypted Image Boot and Run from Internal Flash in i.MXRT10xx ? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-a-HAB-Encrypted-Image-Boot-and-Run-from-Internal-Flash-in-i/m-p/1936668#M227488</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;I wish to confirm my understanding of HAB Secure/Encrypted boot in that a HAB Encrypted image cannot be flashed or be booted and run XIP from the internal flash on an IMXRT10xx MCU.&amp;nbsp; HAB encrypted flashing/boot XIP is only supported using external flash (or executing from OCRAM) ?&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 20 Aug 2024 18:31:49 GMT</pubDate>
    <dc:creator>mjpovi</dc:creator>
    <dc:date>2024-08-20T18:31:49Z</dc:date>
    <item>
      <title>Can a HAB Encrypted Image Boot and Run from Internal Flash in i.MXRT10xx ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-a-HAB-Encrypted-Image-Boot-and-Run-from-Internal-Flash-in-i/m-p/1936668#M227488</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;I wish to confirm my understanding of HAB Secure/Encrypted boot in that a HAB Encrypted image cannot be flashed or be booted and run XIP from the internal flash on an IMXRT10xx MCU.&amp;nbsp; HAB encrypted flashing/boot XIP is only supported using external flash (or executing from OCRAM) ?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Aug 2024 18:31:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-a-HAB-Encrypted-Image-Boot-and-Run-from-Internal-Flash-in-i/m-p/1936668#M227488</guid>
      <dc:creator>mjpovi</dc:creator>
      <dc:date>2024-08-20T18:31:49Z</dc:date>
    </item>
    <item>
      <title>回复： Can a HAB Encrypted Image Boot and Run from Internal Flash in i.MXRT10xx ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-a-HAB-Encrypted-Image-Boot-and-Run-from-Internal-Flash-in-i/m-p/1938289#M227584</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/198987"&gt;@mjpovi&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your interest in NXP MIMXRT series!&lt;/P&gt;
&lt;P&gt;No. In fact, for the RT series, there is little difference between the so-called internal Flash and external Flash, both of which are connected using the FlexSPI. And HAB encrypted boot, does not support XIP.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Gavin&lt;/P&gt;</description>
      <pubDate>Thu, 22 Aug 2024 09:00:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-a-HAB-Encrypted-Image-Boot-and-Run-from-Internal-Flash-in-i/m-p/1938289#M227584</guid>
      <dc:creator>Gavin_Jia</dc:creator>
      <dc:date>2024-08-22T09:00:06Z</dc:date>
    </item>
  </channel>
</rss>