<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Problem in Hardware flow control - i.MX28</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Problem-in-Hardware-flow-control-i-MX28/m-p/250405#M22741</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello PeterChan,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I have solved the problem as well in my case i was using AUART1 which has CTS and RTS pins configured as some other functionality in the kernel for EVK. I changed it to CTS and RTS and it works fine for me. Thanks for the link.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Feb 2013 10:30:03 GMT</pubDate>
    <dc:creator>prateekraghuvan</dc:creator>
    <dc:date>2013-02-15T10:30:03Z</dc:date>
    <item>
      <title>Problem in Hardware flow control - i.MX28</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-in-Hardware-flow-control-i-MX28/m-p/250403#M22739</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am using i.MX28 AUART1 for communication with XBEE module, in which i need hardware flow control.&lt;/P&gt;&lt;P&gt;When i open minicom with H/W flow control enabled. RTS line of Processor never goes low. because of which &lt;/P&gt;&lt;P&gt;there is no communication happening at all. But when i Connect RTS of Processor to CTS of XBEE and then&lt;/P&gt;&lt;P&gt;CTS of Processor to RTS of XBEE (Note that i do it in sequence that is manually with wires with some delay) It starts working.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if any one have any Idea why is it behaving like this, Please help.&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Feb 2013 10:14:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-in-Hardware-flow-control-i-MX28/m-p/250403#M22739</guid>
      <dc:creator>prateekraghuvan</dc:creator>
      <dc:date>2013-02-07T10:14:52Z</dc:date>
    </item>
    <item>
      <title>Re: Problem in Hardware flow control - i.MX28</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-in-Hardware-flow-control-i-MX28/m-p/250404#M22740</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Prateek,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I saw similar issue before and eventually found that the problem came from the serial cable itself. For the cable, the RTS &amp;amp; CTS signals at one end is connecting to same signals at the other end! After rewiring the RTS to CTS, the serial hardware flow control works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In community, there is another i.MX28 AUART hardware flow control issue under discussion. Please also take a look to the thread &lt;A _jive_internal="true" href="https://community.nxp.com/message/311942#311942"&gt;https://community.freescale.com/message/311942#311942&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Feb 2013 06:29:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-in-Hardware-flow-control-i-MX28/m-p/250404#M22740</guid>
      <dc:creator>PeterChan</dc:creator>
      <dc:date>2013-02-14T06:29:44Z</dc:date>
    </item>
    <item>
      <title>Re: Problem in Hardware flow control - i.MX28</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-in-Hardware-flow-control-i-MX28/m-p/250405#M22741</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello PeterChan,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I have solved the problem as well in my case i was using AUART1 which has CTS and RTS pins configured as some other functionality in the kernel for EVK. I changed it to CTS and RTS and it works fine for me. Thanks for the link.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Feb 2013 10:30:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-in-Hardware-flow-control-i-MX28/m-p/250405#M22741</guid>
      <dc:creator>prateekraghuvan</dc:creator>
      <dc:date>2013-02-15T10:30:03Z</dc:date>
    </item>
  </channel>
</rss>