<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: package installation on pre-built linux in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/package-installation-on-pre-built-linux/m-p/1934707#M227396</link>
    <description>&lt;P&gt;in the end i building the yocto from beginning, bc it is easier than using dpkg&lt;/P&gt;</description>
    <pubDate>Mon, 19 Aug 2024 04:17:23 GMT</pubDate>
    <dc:creator>uriuri</dc:creator>
    <dc:date>2024-08-19T04:17:23Z</dc:date>
    <item>
      <title>package installation on pre-built linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/package-installation-on-pre-built-linux/m-p/1916839#M226583</link>
      <description>&lt;P&gt;i am new to this board&lt;BR /&gt;&lt;BR /&gt;i want to ask, is it possible to install package like opencv or tensorflow lite to the pre-built linux installed at emmc? if possible can you tell me how to do it?&lt;BR /&gt;&lt;BR /&gt;also it seems i get error when trying the apt-get update&lt;BR /&gt;&lt;BR /&gt;thx&lt;/P&gt;</description>
      <pubDate>Thu, 25 Jul 2024 05:33:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/package-installation-on-pre-built-linux/m-p/1916839#M226583</guid>
      <dc:creator>uriuri</dc:creator>
      <dc:date>2024-07-25T05:33:14Z</dc:date>
    </item>
    <item>
      <title>Re: package installation on pre-built linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/package-installation-on-pre-built-linux/m-p/1917061#M226595</link>
      <description>&lt;P&gt;Have a try with command dpkg&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Thu, 25 Jul 2024 10:00:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/package-installation-on-pre-built-linux/m-p/1917061#M226595</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2024-07-25T10:00:09Z</dc:date>
    </item>
    <item>
      <title>Re: package installation on pre-built linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/package-installation-on-pre-built-linux/m-p/1917647#M226615</link>
      <description>&lt;P&gt;ok lemme try it first&lt;BR /&gt;but installing package with dpkg really abit troublesome&lt;BR /&gt;&lt;BR /&gt;also can i ask if the pre-built linux on emmc is same as bsp linux on the start guide embedded linux part?&lt;/P&gt;</description>
      <pubDate>Fri, 26 Jul 2024 01:09:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/package-installation-on-pre-built-linux/m-p/1917647#M226615</guid>
      <dc:creator>uriuri</dc:creator>
      <dc:date>2024-07-26T01:09:55Z</dc:date>
    </item>
    <item>
      <title>Re: package installation on pre-built linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/package-installation-on-pre-built-linux/m-p/1917691#M226619</link>
      <description>&lt;P&gt;Should be same.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 26 Jul 2024 02:28:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/package-installation-on-pre-built-linux/m-p/1917691#M226619</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2024-07-26T02:28:29Z</dc:date>
    </item>
    <item>
      <title>Re: package installation on pre-built linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/package-installation-on-pre-built-linux/m-p/1934707#M227396</link>
      <description>&lt;P&gt;in the end i building the yocto from beginning, bc it is easier than using dpkg&lt;/P&gt;</description>
      <pubDate>Mon, 19 Aug 2024 04:17:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/package-installation-on-pre-built-linux/m-p/1934707#M227396</guid>
      <dc:creator>uriuri</dc:creator>
      <dc:date>2024-08-19T04:17:23Z</dc:date>
    </item>
  </channel>
</rss>