<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: u-boot imx-weim driver in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-imx-weim-driver/m-p/1932565#M227321</link>
    <description>&lt;P&gt;Hi &lt;/P&gt;
&lt;P&gt;You could port this driver in Uboot referring the linux driver.&lt;BR /&gt;&lt;BR /&gt;Best Regards&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
    <pubDate>Thu, 15 Aug 2024 01:28:36 GMT</pubDate>
    <dc:creator>Zhiming_Liu</dc:creator>
    <dc:date>2024-08-15T01:28:36Z</dc:date>
    <item>
      <title>u-boot imx-weim driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-imx-weim-driver/m-p/1931616#M227287</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are trying to upgrade to the latest version of U-Boot on our i.MX6 boards. During this process, we would like to synchronize the device tree from Linux to U-Boot.&lt;/P&gt;&lt;P&gt;Currently, WEIM register initialization is handled in a board-specific file. However, the device tree expects a WEIM parent node for the WEIM child driver to function properly.&lt;/P&gt;&lt;P&gt;As a result, we are unable to synchronize because the i.MX WEIM driver is not present in the U-Boot source code.&lt;/P&gt;&lt;P&gt;is there any solution for this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Aug 2024 04:34:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-imx-weim-driver/m-p/1931616#M227287</guid>
      <dc:creator>vishwaec08</dc:creator>
      <dc:date>2024-08-14T04:34:07Z</dc:date>
    </item>
    <item>
      <title>Re: u-boot imx-weim driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-imx-weim-driver/m-p/1932565#M227321</link>
      <description>&lt;P&gt;Hi &lt;/P&gt;
&lt;P&gt;You could port this driver in Uboot referring the linux driver.&lt;BR /&gt;&lt;BR /&gt;Best Regards&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Thu, 15 Aug 2024 01:28:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-imx-weim-driver/m-p/1932565#M227321</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2024-08-15T01:28:36Z</dc:date>
    </item>
    <item>
      <title>Re: u-boot imx-weim driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/u-boot-imx-weim-driver/m-p/1933440#M227353</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/151788"&gt;@Zhiming_Liu&lt;/a&gt;&amp;nbsp;,&lt;BR /&gt;&lt;BR /&gt;Thanks for the reply.&lt;BR /&gt;&lt;BR /&gt;Sure, we will port the driver from Linux to u-boot.&lt;BR /&gt;&lt;BR /&gt;Since many board files use the WIEM interface and are already synced with the Linux device tree, I’m wondering if anyone has faced this issue before.&lt;BR /&gt;&lt;BR /&gt;Regards and Thanks&amp;nbsp;&lt;/P&gt;&lt;P&gt;Vishwa&lt;/P&gt;</description>
      <pubDate>Fri, 16 Aug 2024 06:33:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/u-boot-imx-weim-driver/m-p/1933440#M227353</guid>
      <dc:creator>vishwaec08</dc:creator>
      <dc:date>2024-08-16T06:33:06Z</dc:date>
    </item>
  </channel>
</rss>