<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PCIE MSI-X support in I.MX8QM board in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PCIE-MSI-X-support-in-I-MX8QM-board/m-p/1931163#M227269</link>
    <description>&lt;P&gt;Dear Team,&lt;BR /&gt;&lt;BR /&gt;I am configuring my I.MX8QM board as PCIe Root Complex, Custom Board as Endpoint.&lt;/P&gt;&lt;P&gt;Now I am generating MSI-X interrupt from Endpoint, I have to handle Received MSI-X interrupt in my Root complex, Is I.MX8QM board will support handling of MSI-X interrupt or not?&lt;/P&gt;&lt;P&gt;Here at RC side handling of MSI interrupt code only available, MSI-x code is not available.&lt;/P&gt;&lt;P&gt;In Dts file also only msi related properties are given, MSI-x properties not provided.&lt;BR /&gt;&lt;BR /&gt;Kernel Vesion: 5.15.32.&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Mallikarjuna&lt;/P&gt;</description>
    <pubDate>Tue, 13 Aug 2024 13:23:51 GMT</pubDate>
    <dc:creator>mallibeerala</dc:creator>
    <dc:date>2024-08-13T13:23:51Z</dc:date>
    <item>
      <title>PCIE MSI-X support in I.MX8QM board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIE-MSI-X-support-in-I-MX8QM-board/m-p/1931163#M227269</link>
      <description>&lt;P&gt;Dear Team,&lt;BR /&gt;&lt;BR /&gt;I am configuring my I.MX8QM board as PCIe Root Complex, Custom Board as Endpoint.&lt;/P&gt;&lt;P&gt;Now I am generating MSI-X interrupt from Endpoint, I have to handle Received MSI-X interrupt in my Root complex, Is I.MX8QM board will support handling of MSI-X interrupt or not?&lt;/P&gt;&lt;P&gt;Here at RC side handling of MSI interrupt code only available, MSI-x code is not available.&lt;/P&gt;&lt;P&gt;In Dts file also only msi related properties are given, MSI-x properties not provided.&lt;BR /&gt;&lt;BR /&gt;Kernel Vesion: 5.15.32.&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Mallikarjuna&lt;/P&gt;</description>
      <pubDate>Tue, 13 Aug 2024 13:23:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIE-MSI-X-support-in-I-MX8QM-board/m-p/1931163#M227269</guid>
      <dc:creator>mallibeerala</dc:creator>
      <dc:date>2024-08-13T13:23:51Z</dc:date>
    </item>
    <item>
      <title>Re: PCIE MSI-X support in I.MX8QM board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIE-MSI-X-support-in-I-MX8QM-board/m-p/1932079#M227313</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The MX8 does&amp;nbsp; not support MSI-X but Can you try it with disabled MSI interrupts?&lt;/P&gt;
&lt;DIV id="bodyDisplay_2" class="lia-message-body lia-component-message-view-widget-body lia-component-body-signature-highlight-escalation lia-component-message-view-widget-body-signature-highlight-escalation"&gt;
&lt;DIV class="lia-message-body-content"&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;In u-boot:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;setenv mmcargs setenv bootargs console=${console} root=${mmcroot} pci=nomsi&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;saveenv&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;
&lt;/DIV&gt;
&lt;/DIV&gt;</description>
      <pubDate>Wed, 14 Aug 2024 14:10:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIE-MSI-X-support-in-I-MX8QM-board/m-p/1932079#M227313</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-08-14T14:10:29Z</dc:date>
    </item>
  </channel>
</rss>