<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックFlexcan Listen-only</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Flexcan-Listen-only/m-p/1928286#M227138</link>
    <description>&lt;P&gt;Hi ,&lt;BR /&gt;I want to put my board flexcan in listen-only mode. Could you help tell us which bits are needed to place the Flexcan in listen-only mode? I'm using the i.MX6&lt;BR /&gt;These are the bits that will be enabled if I set the Flexcan to read-write mode in control register. 0011 0001 0010 0000 0000 0101 0011 0001 0011 0001&lt;BR /&gt;Similarly, if I use the IP Link command to enable the listen-only mode (ip link set can1 up type can bitrate 500000 listen-only on), these bits will be enabled in the control bit: 0000 0100 0011 0001 0010 0000 0000 1101.&lt;BR /&gt;I verified with this command (ip -d -s link show can1) to confirm that it was set to listen only.&lt;BR /&gt;However, if I send data from another board the data is not receiving and please let us know what could be the reason.&lt;BR /&gt;Regards,&lt;BR /&gt;Jamal Deen&lt;/P&gt;</description>
    <pubDate>Thu, 08 Aug 2024 12:57:07 GMT</pubDate>
    <dc:creator>Jamal</dc:creator>
    <dc:date>2024-08-08T12:57:07Z</dc:date>
    <item>
      <title>Flexcan Listen-only</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flexcan-Listen-only/m-p/1928286#M227138</link>
      <description>&lt;P&gt;Hi ,&lt;BR /&gt;I want to put my board flexcan in listen-only mode. Could you help tell us which bits are needed to place the Flexcan in listen-only mode? I'm using the i.MX6&lt;BR /&gt;These are the bits that will be enabled if I set the Flexcan to read-write mode in control register. 0011 0001 0010 0000 0000 0101 0011 0001 0011 0001&lt;BR /&gt;Similarly, if I use the IP Link command to enable the listen-only mode (ip link set can1 up type can bitrate 500000 listen-only on), these bits will be enabled in the control bit: 0000 0100 0011 0001 0010 0000 0000 1101.&lt;BR /&gt;I verified with this command (ip -d -s link show can1) to confirm that it was set to listen only.&lt;BR /&gt;However, if I send data from another board the data is not receiving and please let us know what could be the reason.&lt;BR /&gt;Regards,&lt;BR /&gt;Jamal Deen&lt;/P&gt;</description>
      <pubDate>Thu, 08 Aug 2024 12:57:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flexcan-Listen-only/m-p/1928286#M227138</guid>
      <dc:creator>Jamal</dc:creator>
      <dc:date>2024-08-08T12:57:07Z</dc:date>
    </item>
    <item>
      <title>Re: Flexcan Listen-only</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Flexcan-Listen-only/m-p/1928317#M227146</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;it could be expected behavior, if a message is not acknowledged by other node&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Bio_TICFSL_0-1723125214167.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/292622i9FB4F793147A3CD0/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Bio_TICFSL_0-1723125214167.png" alt="Bio_TICFSL_0-1723125214167.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 08 Aug 2024 13:53:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Flexcan-Listen-only/m-p/1928317#M227146</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-08-08T13:53:53Z</dc:date>
    </item>
  </channel>
</rss>