<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Implement a point and line drawing application based on coordinate points, etc</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Implement-a-point-and-line-drawing-application-based-on/m-p/1924962#M226982</link>
    <description>&lt;P&gt;When equipped with the TP framework, touch coordinates are driven by IIC and interrupt INT notifications are sent to the Input subsystem; Tslib must be combined with the input event event;&lt;BR /&gt;If the TP pin is given to the M core and the TP reporting point coordinate data and status are transmitted to the A core, how can tslib be called? First, transfer the app from core A of the dual core communication to the lower layer, and then transfer it to tslib from the upper layer; Can the A core APP of dual core communication be directly mapped to tslib?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 05 Aug 2024 05:47:15 GMT</pubDate>
    <dc:creator>ximenbingmeng</dc:creator>
    <dc:date>2024-08-05T05:47:15Z</dc:date>
    <item>
      <title>Implement a point and line drawing application based on coordinate points, etc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Implement-a-point-and-line-drawing-application-based-on/m-p/1924962#M226982</link>
      <description>&lt;P&gt;When equipped with the TP framework, touch coordinates are driven by IIC and interrupt INT notifications are sent to the Input subsystem; Tslib must be combined with the input event event;&lt;BR /&gt;If the TP pin is given to the M core and the TP reporting point coordinate data and status are transmitted to the A core, how can tslib be called? First, transfer the app from core A of the dual core communication to the lower layer, and then transfer it to tslib from the upper layer; Can the A core APP of dual core communication be directly mapped to tslib?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 05 Aug 2024 05:47:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Implement-a-point-and-line-drawing-application-based-on/m-p/1924962#M226982</guid>
      <dc:creator>ximenbingmeng</dc:creator>
      <dc:date>2024-08-05T05:47:15Z</dc:date>
    </item>
    <item>
      <title>Re: Implement a point and line drawing application based on coordinate points, etc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Implement-a-point-and-line-drawing-application-based-on/m-p/1925440#M226998</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&amp;nbsp; &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196885"&gt;@ximenbingmeng&lt;/a&gt;!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;We don´t have any documentation about tslib.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards!&lt;/P&gt;
&lt;P&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Mon, 05 Aug 2024 14:58:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Implement-a-point-and-line-drawing-application-based-on/m-p/1925440#M226998</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2024-08-05T14:58:34Z</dc:date>
    </item>
  </channel>
</rss>