<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックHAB process error shown</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/HAB-process-error-shown/m-p/1924030#M226952</link>
    <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;I have been working on a project which uses the Toradex Colibri IMX6ULL. I have flashed a custom Linux distro to the SOM which was built using Yocto.&lt;BR /&gt;For enabling SecureBoot in the SOM, I was following the document provided by NXP -&amp;gt;&lt;A href="https://www.google.com/url?sa=t&amp;amp;source=web&amp;amp;rct=j&amp;amp;opi=89978449&amp;amp;url=https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/imx-processors/60046/1/i.MX_6_Linux_High_Assurance_Boot_(HAB)_User%2527s_Guide.pdf&amp;amp;ved=2ahUKEwicmOTrq9aHAxWHUGwGHYalIf0QFnoECBEQAQ&amp;amp;usg=AOvVaw3KfpbSCOakrVf3iJCP6h0M" target="_blank"&gt;https://www.google.com/url?sa=t&amp;amp;source=web&amp;amp;rct=j&amp;amp;opi=89978449&amp;amp;url=https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/imx-processors/60046/1/i.MX_6_Linux_High_Assurance_Boot_(HAB)_User%2527s_Guide.pdf&amp;amp;ved=2ahUKEwicmOTrq9aHAxWHUGwGHYalIf0QFnoECBEQAQ&amp;amp;usg=AOvVaw3KfpbSCOakrVf3iJCP6h0M&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Referring the above doc, I was able to create a signed u-boot binary, after which on trying to create a signed kernel image binary, I got some error.&lt;BR /&gt;I had followed the steps as per the document, and then on step 16, while running the script 'habUimagegen', I am getting the following error:&lt;BR /&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "Unsupported argument: Blocks in command InstallKey"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;I could not understand the error or how it is coming. For the uImage input, I had taken the kernel image after doing bitbake. Is it the issue with the kernel image input?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Kindly look into the above error and advise a proper solution for it.&lt;/P&gt;&lt;P&gt;Thanks in Advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 02 Aug 2024 12:54:40 GMT</pubDate>
    <dc:creator>divakaran</dc:creator>
    <dc:date>2024-08-02T12:54:40Z</dc:date>
    <item>
      <title>HAB process error shown</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HAB-process-error-shown/m-p/1924030#M226952</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;I have been working on a project which uses the Toradex Colibri IMX6ULL. I have flashed a custom Linux distro to the SOM which was built using Yocto.&lt;BR /&gt;For enabling SecureBoot in the SOM, I was following the document provided by NXP -&amp;gt;&lt;A href="https://www.google.com/url?sa=t&amp;amp;source=web&amp;amp;rct=j&amp;amp;opi=89978449&amp;amp;url=https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/imx-processors/60046/1/i.MX_6_Linux_High_Assurance_Boot_(HAB)_User%2527s_Guide.pdf&amp;amp;ved=2ahUKEwicmOTrq9aHAxWHUGwGHYalIf0QFnoECBEQAQ&amp;amp;usg=AOvVaw3KfpbSCOakrVf3iJCP6h0M" target="_blank"&gt;https://www.google.com/url?sa=t&amp;amp;source=web&amp;amp;rct=j&amp;amp;opi=89978449&amp;amp;url=https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/imx-processors/60046/1/i.MX_6_Linux_High_Assurance_Boot_(HAB)_User%2527s_Guide.pdf&amp;amp;ved=2ahUKEwicmOTrq9aHAxWHUGwGHYalIf0QFnoECBEQAQ&amp;amp;usg=AOvVaw3KfpbSCOakrVf3iJCP6h0M&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Referring the above doc, I was able to create a signed u-boot binary, after which on trying to create a signed kernel image binary, I got some error.&lt;BR /&gt;I had followed the steps as per the document, and then on step 16, while running the script 'habUimagegen', I am getting the following error:&lt;BR /&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "Unsupported argument: Blocks in command InstallKey"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;I could not understand the error or how it is coming. For the uImage input, I had taken the kernel image after doing bitbake. Is it the issue with the kernel image input?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Kindly look into the above error and advise a proper solution for it.&lt;/P&gt;&lt;P&gt;Thanks in Advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 02 Aug 2024 12:54:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HAB-process-error-shown/m-p/1924030#M226952</guid>
      <dc:creator>divakaran</dc:creator>
      <dc:date>2024-08-02T12:54:40Z</dc:date>
    </item>
    <item>
      <title>Re: HAB process error shown</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HAB-process-error-shown/m-p/1926114#M227028</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Please check the uImage.csf file if there are&amp;nbsp;Unsupported argument under the "[Install Key]".&lt;/P&gt;
&lt;P&gt;The document is quite old for old BSP and would suggest to raise a case to Toradex and referring their new references for the signing.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;harvey&lt;/P&gt;</description>
      <pubDate>Tue, 06 Aug 2024 08:00:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HAB-process-error-shown/m-p/1926114#M227028</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2024-08-06T08:00:15Z</dc:date>
    </item>
  </channel>
</rss>