<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: HDMI resolution effected when we enabled LVDS display</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-resolution-effected-when-we-enabled-LVDS-display/m-p/1923741#M226944</link>
    <description>Hi&lt;BR /&gt;&lt;BR /&gt;- Yes , we are using -d lvds-panel&lt;BR /&gt;- Both HDMI and LVDS are connected to target&lt;BR /&gt;&lt;BR /&gt;sudo ./imx-sdcard-partition.sh -d lvds-panel -f imx8mp -c 28 /dev/sdc&lt;BR /&gt;</description>
    <pubDate>Fri, 02 Aug 2024 07:13:10 GMT</pubDate>
    <dc:creator>shiva141</dc:creator>
    <dc:date>2024-08-02T07:13:10Z</dc:date>
    <item>
      <title>HDMI resolution effected when we enabled LVDS display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-resolution-effected-when-we-enabled-LVDS-display/m-p/1922927#M226885</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;IMX8MP Android 13 we have build the bsp based on user guide.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We were able to see full resolution on HDMI ,while HDMI was only enabled.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;When we enabled LVDS support in the BSP, we observed &amp;nbsp;that the LVDS resolution had an impact on the HDMI resolution.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When LVDS is enabled in the Android BSP, is it possible to attain full resolution on HDMI?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;LI-PRODUCT title="IMX8MPLUS" id="IMX8MPLUS"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;#Andorid13&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 01 Aug 2024 10:47:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HDMI-resolution-effected-when-we-enabled-LVDS-display/m-p/1922927#M226885</guid>
      <dc:creator>shiva141</dc:creator>
      <dc:date>2024-08-01T10:47:54Z</dc:date>
    </item>
    <item>
      <title>Re: HDMI resolution effected when we enabled LVDS display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-resolution-effected-when-we-enabled-LVDS-display/m-p/1923493#M226926</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Are you using lvds-panel dtbo.image?&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;To test LVDS panel display, execute the tool with &lt;STRONG&gt;-d lvds-panel&lt;/STRONG&gt;. MIPI-to-HDMI and physical HDMI&lt;BR /&gt;are also supported in this condition&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;Best Regards&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Fri, 02 Aug 2024 02:16:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HDMI-resolution-effected-when-we-enabled-LVDS-display/m-p/1923493#M226926</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2024-08-02T02:16:08Z</dc:date>
    </item>
    <item>
      <title>Re: HDMI resolution effected when we enabled LVDS display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HDMI-resolution-effected-when-we-enabled-LVDS-display/m-p/1923741#M226944</link>
      <description>Hi&lt;BR /&gt;&lt;BR /&gt;- Yes , we are using -d lvds-panel&lt;BR /&gt;- Both HDMI and LVDS are connected to target&lt;BR /&gt;&lt;BR /&gt;sudo ./imx-sdcard-partition.sh -d lvds-panel -f imx8mp -c 28 /dev/sdc&lt;BR /&gt;</description>
      <pubDate>Fri, 02 Aug 2024 07:13:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HDMI-resolution-effected-when-we-enabled-LVDS-display/m-p/1923741#M226944</guid>
      <dc:creator>shiva141</dc:creator>
      <dc:date>2024-08-02T07:13:10Z</dc:date>
    </item>
  </channel>
</rss>