<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Linux 3.0.35 for iMX53 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Re-Linux-3-0-35-for-iMX53/m-p/250254#M22686</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We're developing custom board based on IMX53QSB. Kernel 2.5.35 from LTIB works fine. u-boot from LTIB works fine.&lt;/P&gt;&lt;P&gt;Even u-boot from git works fine (and with 1Ghz clock).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Linux kernel 3.8.2 compiles with imx_v6_v7_defconfig, but hangs up on device. And I can't understand why: load address? Entry point? DRAM setting (but it's U-boot's work)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you public you .config or at least .diff from imx_v6_v7_defconfig? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Apr 2013 09:05:56 GMT</pubDate>
    <dc:creator>SergeVShistarev</dc:creator>
    <dc:date>2013-04-01T09:05:56Z</dc:date>
    <item>
      <title>Re: Linux 3.0.35 for iMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Re-Linux-3-0-35-for-iMX53/m-p/250254#M22686</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We're developing custom board based on IMX53QSB. Kernel 2.5.35 from LTIB works fine. u-boot from LTIB works fine.&lt;/P&gt;&lt;P&gt;Even u-boot from git works fine (and with 1Ghz clock).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Linux kernel 3.8.2 compiles with imx_v6_v7_defconfig, but hangs up on device. And I can't understand why: load address? Entry point? DRAM setting (but it's U-boot's work)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you public you .config or at least .diff from imx_v6_v7_defconfig? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Apr 2013 09:05:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Re-Linux-3-0-35-for-iMX53/m-p/250254#M22686</guid>
      <dc:creator>SergeVShistarev</dc:creator>
      <dc:date>2013-04-01T09:05:56Z</dc:date>
    </item>
    <item>
      <title>Re: Linux 3.0.35 for iMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Re-Linux-3-0-35-for-iMX53/m-p/250255#M22687</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Serge,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tested the Stable: 3.8.5 on i.MX53QSB and it's booting. I'm using the &lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;imx_v6_v7_defconfig&lt;/SPAN&gt; as you mentioned.&lt;/P&gt;&lt;P&gt;Please, take a look on &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-1604" title="https://community.freescale.com/docs/DOC-1604"&gt;https://community.freescale.com/docs/DOC-1604&lt;/A&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; - Section "Building Kernel Mainline"&lt;/P&gt;&lt;P&gt;and check if you're missing any step.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Rgds&lt;/P&gt;&lt;P&gt;Rogerio&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Apr 2013 13:15:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Re-Linux-3-0-35-for-iMX53/m-p/250255#M22687</guid>
      <dc:creator>rogerio_silva</dc:creator>
      <dc:date>2013-04-01T13:15:58Z</dc:date>
    </item>
    <item>
      <title>Re: Linux 3.0.35 for iMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Re-Linux-3-0-35-for-iMX53/m-p/250256#M22688</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rogerio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks for link. I wonder how I skip it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Apr 2013 15:54:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Re-Linux-3-0-35-for-iMX53/m-p/250256#M22688</guid>
      <dc:creator>SergeVShistarev</dc:creator>
      <dc:date>2013-04-01T15:54:20Z</dc:date>
    </item>
    <item>
      <title>Re: Linux 3.0.35 for iMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Re-Linux-3-0-35-for-iMX53/m-p/250257#M22689</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rogerio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I need to use the PREEMPT_RT patches [1], I am currently looking at two options for the i.MX51 platform:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Either use a mainline 3.8.4 (or one of a few available earlier versions) kernel with the official PREEMPT_RT patches&lt;/LI&gt;&lt;LI&gt;Or try a modified [2] 2.6.31-imx&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would prefer to use a mainline 3.8.4 kernel. So, have you experienced or do you know of any obvious problems with that version (e.g. basic features or hardware that is not supported)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[1] &lt;A href="https://www.kernel.org/pub/linux/kernel/projects/rt/" title="https://www.kernel.org/pub/linux/kernel/projects/rt/"&gt;Index of /pub/linux/kernel/projects/rt&lt;/A&gt;&lt;/P&gt;&lt;P&gt;[2] &lt;A href="https://community.nxp.com/message/235432"&gt;Real-Time patch on iMX51&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Apr 2013 14:01:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Re-Linux-3-0-35-for-iMX53/m-p/250257#M22689</guid>
      <dc:creator>goodvibr</dc:creator>
      <dc:date>2013-04-03T14:01:42Z</dc:date>
    </item>
    <item>
      <title>Re: Linux 3.0.35 for iMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Re-Linux-3-0-35-for-iMX53/m-p/250258#M22690</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Goodvibr,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry but I'm not familiar with PREEMPT_RT patches.&lt;/P&gt;&lt;P&gt;The kernels from Freescale are more complete in terms of i.MX drivers, but I don't think you will have problems if you choose mainline kernel. You will have to check if kernel mainline has all features you need. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Rgds,&lt;/P&gt;&lt;P&gt;Rogerio&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Apr 2013 20:20:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Re-Linux-3-0-35-for-iMX53/m-p/250258#M22690</guid>
      <dc:creator>rogerio_silva</dc:creator>
      <dc:date>2013-04-03T20:20:37Z</dc:date>
    </item>
    <item>
      <title>Re: Linux 3.0.35 for iMX53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Re-Linux-3-0-35-for-iMX53/m-p/250259#M22691</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can reference mx51evk device tree code to check what is currently supported in 3.8.5:&lt;/P&gt;&lt;P&gt;&lt;A href="https://git.kernel.org/cgit/linux/kernel/git/stable/linux-stable.git/tree/arch/arm/boot/dts/imx51-babbage.dts?id=refs/tags/v3.8.5" title="https://git.kernel.org/cgit/linux/kernel/git/stable/linux-stable.git/tree/arch/arm/boot/dts/imx51-babbage.dts?id=refs/tags/v3.8.5"&gt;https://git.kernel.org/cgit/linux/kernel/git/stable/linux-stable.git/tree/arch/arm/boot/dts/imx51-babbage.dts?id=refs/tags/v3.8.5&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Apr 2013 01:01:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Re-Linux-3-0-35-for-iMX53/m-p/250259#M22691</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2013-04-04T01:01:36Z</dc:date>
    </item>
  </channel>
</rss>