<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Display flickering when set to lower brightness in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Display-flickering-when-set-to-lower-brightness/m-p/1922100#M226838</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/237393"&gt;@fsong1&lt;/a&gt;&amp;nbsp;, The brightness-levels is an array(separated by spaces) and not a range. Pls refer to the&amp;nbsp;&lt;A href="https://www.kernel.org/doc/Documentation/devicetree/bindings/leds/backlight/pwm-backlight.txt" target="_blank"&gt;https://www.kernel.org/doc/Documentation/devicetree/bindings/leds/backlight/pwm-backlight.txt&lt;/A&gt;&amp;nbsp;for additional information on the parameters.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;In your dts file configuration, 120 is not defined.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 31 Jul 2024 20:59:13 GMT</pubDate>
    <dc:creator>praveen_adi</dc:creator>
    <dc:date>2024-07-31T20:59:13Z</dc:date>
    <item>
      <title>Display flickering when set to lower brightness</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-flickering-when-set-to-lower-brightness/m-p/1920286#M226747</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using i.MX8M Mini EVK and rm67199 panel, and original &lt;STRONG&gt;evk-rm67199.dtb&lt;/STRONG&gt; for the board. After board bootup, the default display of weston-desktop-shell looks fine, no blink and no flicker.&lt;/P&gt;&lt;P&gt;Under a special scenario, we need a lower level of brightness. Adjust the brightness from normal value 255 to lower value such as 150, using the command:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;EM&gt;&lt;FONT color="#0000FF"&gt;# echo 150 &amp;gt; /sys/devices/platform/soc@0/32c00000.bus/32e10000.mipi_dsi/32e10000.mipi_dsi.0/backlight/32e10000.mipi_dsi.0/brightness&lt;/FONT&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;The screen becomes not bright as before. This is what I expected.&amp;nbsp; But it is flickering. And lower value of brightness, higher frequency of flicker.&lt;/P&gt;&lt;P&gt;So any tips on this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Frank&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 30 Jul 2024 08:50:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-flickering-when-set-to-lower-brightness/m-p/1920286#M226747</guid>
      <dc:creator>fsong1</dc:creator>
      <dc:date>2024-07-30T08:50:04Z</dc:date>
    </item>
    <item>
      <title>Re: Display flickering when set to lower brightness</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-flickering-when-set-to-lower-brightness/m-p/1920600#M226764</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Which image are you using on your setup?&amp;nbsp; Please try the latest bsp&amp;nbsp; should come with default image, did you make tests only using the one you generated or with the default one too?&lt;/P&gt;
&lt;P&gt;I made a small test here flashing the most recent reference multimedia image&amp;nbsp; and it worked as expected, the brightness changes according to the values provided on &lt;A href="https://git.toradex.com/cgit/linux-toradex.git/tree/arch/arm64/boot/dts/freescale/imx8mm-verdin.dtsi?h=toradex_5.4-2.3.x-imx#n22" target="_blank"&gt;https://git.toradex.com/cgit/linux-toradex.git/tree/arch/arm64/boot/dts/freescale/imx8mm-verdin.dtsi?h=toradex_5.4-2.3.x-imx#n22&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;of the device tree backlight node. After flashing the image the only modification I did is writing the correct .dtbo&lt;/P&gt;
&lt;P&gt;I made this with the EVK and kernel 5.1.15.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 30 Jul 2024 14:35:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-flickering-when-set-to-lower-brightness/m-p/1920600#M226764</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-07-30T14:35:41Z</dc:date>
    </item>
    <item>
      <title>Re: Display flickering when set to lower brightness</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-flickering-when-set-to-lower-brightness/m-p/1921084#M226785</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Thanks a lot for your support.&amp;nbsp; We are using mickledore release (kernel 6.1.22), and the multimedia image we generated for the EVK board.&lt;/P&gt;&lt;P&gt;The backlight node in device tree is as below (the entire dts file is attached):&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;FONT color="#0000FF"&gt;backlight: backlight {&lt;/FONT&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;FONT color="#0000FF"&gt;compatible = "pwm-backlight";&lt;/FONT&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;FONT color="#0000FF"&gt;pwms = &amp;lt;&amp;amp;pwm1 0 5000000 0&amp;gt;;&lt;/FONT&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;FONT color="#0000FF"&gt;brightness-levels = &amp;lt;0 255&amp;gt;;&lt;/FONT&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;FONT color="#0000FF"&gt;num-interpolated-steps = &amp;lt;255&amp;gt;;&lt;/FONT&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;FONT color="#0000FF"&gt;default-brightness-level = &amp;lt;250&amp;gt;;&lt;/FONT&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;FONT color="#0000FF"&gt;};&lt;/FONT&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;I can see the screen brightness changes with different settings of brightness value. The issue is, when set lower brightness value, e.g 120, there are obvious display flickers.&lt;/P&gt;&lt;P&gt;It is OLED panel. I'm not clear if more need done for setting brightness. I just input the command for this:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;FONT color="#0000FF"&gt;# echo 120 &amp;gt; /sys/devices/platform/soc@0/32c00000.bus/32e10000.mipi_dsi/32e10000.mipi_dsi.0/backlight/32e10000.mipi_dsi.0/brightness&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Frank&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 31 Jul 2024 02:45:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-flickering-when-set-to-lower-brightness/m-p/1921084#M226785</guid>
      <dc:creator>fsong1</dc:creator>
      <dc:date>2024-07-31T02:45:44Z</dc:date>
    </item>
    <item>
      <title>Re: Display flickering when set to lower brightness</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-flickering-when-set-to-lower-brightness/m-p/1922100#M226838</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/237393"&gt;@fsong1&lt;/a&gt;&amp;nbsp;, The brightness-levels is an array(separated by spaces) and not a range. Pls refer to the&amp;nbsp;&lt;A href="https://www.kernel.org/doc/Documentation/devicetree/bindings/leds/backlight/pwm-backlight.txt" target="_blank"&gt;https://www.kernel.org/doc/Documentation/devicetree/bindings/leds/backlight/pwm-backlight.txt&lt;/A&gt;&amp;nbsp;for additional information on the parameters.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;In your dts file configuration, 120 is not defined.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 31 Jul 2024 20:59:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-flickering-when-set-to-lower-brightness/m-p/1922100#M226838</guid>
      <dc:creator>praveen_adi</dc:creator>
      <dc:date>2024-07-31T20:59:13Z</dc:date>
    </item>
    <item>
      <title>Re: Display flickering when set to lower brightness</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-flickering-when-set-to-lower-brightness/m-p/1922687#M226865</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks a lot for your advice. Let me look into the linked documentation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Frank&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 01 Aug 2024 07:38:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-flickering-when-set-to-lower-brightness/m-p/1922687#M226865</guid>
      <dc:creator>fsong1</dc:creator>
      <dc:date>2024-08-01T07:38:45Z</dc:date>
    </item>
  </channel>
</rss>