<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Problems with im6 booting when connected to HDMI in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Problems-with-im6-booting-when-connected-to-HDMI/m-p/1921688#M226823</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The i.MX6 does not have HDMI you must check which device are you using? maybe it is for another vendor and from nxp, contact your vendor.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Wed, 31 Jul 2024 14:39:46 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2024-07-31T14:39:46Z</dc:date>
    <item>
      <title>Problems with im6 booting when connected to HDMI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-with-im6-booting-when-connected-to-HDMI/m-p/1920400#M226751</link>
      <description>&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;We are using the IMX6 with Yocto 2.1 and kernel 4.1.15. when we connected the HDMI, performing a software reboot results in the system halting at U-Boot and failing to proceed into the kernel.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Adv-Boot SPL 2016.03-3430A1LIV8940+g8aa465eb (Apr 29 2019 - 15:02:28)&lt;BR /&gt;BOOT_DEVICE_AUTO&lt;BR /&gt;MMC: no card present&lt;BR /&gt;spl: mmc dev 0 init failed&lt;BR /&gt;MMC read: dev # 1, block # 3,count 1200 ...&lt;BR /&gt;booting from iNAND&lt;BR /&gt;Jumping to U-Boot&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot 2016.03-3430A1LIV8940+g8aa465eb (Apr 29 2019 - 15:02:28 +0000)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6D rev1.5 996 MHz (running at 792 MHz)&lt;BR /&gt;CPU: Extended Commercial temperature grade (-20C to 105C) at 49C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Board: MX6-SabreSD&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: 1 GiB&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;JEDEC ID: 0xef:0x40:0x16&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;JEDEC ID: 0xef:0x40:0x16&lt;BR /&gt;MAC addr = 0x74:0xFE:0x48:0x98:0x4F:0x0A&lt;BR /&gt;booting from iNAND&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;flash target is MMC:1&lt;BR /&gt;Net: FEC [PRIME]&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1(part 0) is current device&lt;BR /&gt;reading boot.scr&lt;BR /&gt;** Unable to read file boot.scr **&lt;BR /&gt;reading zImage&lt;BR /&gt;6514216 bytes read in 321 ms (19.4 MiB/s)&lt;BR /&gt;Booting from mmc ...&lt;BR /&gt;reading imx6q-rsb3430-a1.dtb&lt;BR /&gt;49936 bytes read in 19 ms (2.5 MiB/s)&lt;BR /&gt;Kernel image @ 0x12000000 [ 0x000000 - 0x636628 ]&lt;BR /&gt;## Flattened Device Tree blob at 18000000&lt;BR /&gt;Booting using the fdt blob at 0x18000000&lt;BR /&gt;Using Device Tree in place at 18000000, end 1800f30f&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 30 Jul 2024 10:22:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-with-im6-booting-when-connected-to-HDMI/m-p/1920400#M226751</guid>
      <dc:creator>charleshuang</dc:creator>
      <dc:date>2024-07-30T10:22:05Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with im6 booting when connected to HDMI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-with-im6-booting-when-connected-to-HDMI/m-p/1921688#M226823</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The i.MX6 does not have HDMI you must check which device are you using? maybe it is for another vendor and from nxp, contact your vendor.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 31 Jul 2024 14:39:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-with-im6-booting-when-connected-to-HDMI/m-p/1921688#M226823</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-07-31T14:39:46Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with im6 booting when connected to HDMI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-with-im6-booting-when-connected-to-HDMI/m-p/1928185#M227130</link>
      <description>I am currently using the i.MX 6Quad Evaluation Kit with the operating system version L4.1.15_2.0.0. When I use the command to start HDMI:"setenv mmcargs setenv bootargs console=${console},${baudrate} ${smp} root=${mmcroot} ${bootargs} video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24".&lt;BR /&gt;it causes the system to be unable to boot. The link to the video is as follows. &lt;A href="https://drive.google.com/file/d/1qp7K_O0OaKXG8FWFuXtlbC7mbigGqbxb/view?usp=sharing" target="_blank"&gt;https://drive.google.com/file/d/1qp7K_O0OaKXG8FWFuXtlbC7mbigGqbxb/view?usp=sharing&lt;/A&gt;</description>
      <pubDate>Thu, 08 Aug 2024 10:13:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-with-im6-booting-when-connected-to-HDMI/m-p/1928185#M227130</guid>
      <dc:creator>charleshuang</dc:creator>
      <dc:date>2024-08-08T10:13:31Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with im6 booting when connected to HDMI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problems-with-im6-booting-when-connected-to-HDMI/m-p/1928319#M227148</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Before build new UBoot image, the display type can be selected from file uboot-imx\include\configs\mx6q_sabresd.h&lt;BR /&gt;// Select one of the output mode&lt;BR /&gt;#define IPU_OUTPUT_MODE_HDMI&lt;BR /&gt;//#define IPU_OUTPUT_MODE_LVDS&lt;BR /&gt;//#define IPU_OUTPUT_MODE_LCD&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-- Uboot parameters for video mode&lt;BR /&gt;&amp;nbsp;&amp;nbsp; 1080P HDMI:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24,bpp=32 fb0base=0x27b00000 fbmem=28M hdmi_audio_clk=148500000"&lt;/P&gt;
&lt;P style="padding: 0px; min-height: 8pt;"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp; 720P HDMI:&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24,bpp=32 fb0base=0x27b00000 fbmem=28M hdmi_audio_clk=74250000"&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 08 Aug 2024 13:58:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problems-with-im6-booting-when-connected-to-HDMI/m-p/1928319#M227148</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-08-08T13:58:44Z</dc:date>
    </item>
  </channel>
</rss>