<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピック回复： IMX8MP, WM8962, aplay: pcm_write:2127: write error: Input/output error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-WM8962-aplay-pcm-write-2127-write-error-Input-output/m-p/1920239#M226741</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I referred to the case you provided and used the methods in it to correct it.&lt;BR /&gt;ASoC: error at soc_component_read_no_lock on wm8962.2-001a: -16&lt;BR /&gt;Now dmesg will not cause this error , thank you.&lt;/P&gt;&lt;P&gt;But aplay: pcm_write:2127: write error: Input/output error is not resolved&lt;BR /&gt;I refer to /arch/arm64/boot/dts/freescale/imx8mm-beacon-baseboard.dtsi to set the same clocks&lt;BR /&gt;"assigned-clock-rates = &amp;lt;24576000&amp;gt;;"&lt;BR /&gt;Use an oscilloscope to measure that when he plays music, it is indeed the same as the clock I set.&lt;BR /&gt;Are there any other areas that need attention and need to be checked?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 30 Jul 2024 07:57:41 GMT</pubDate>
    <dc:creator>Lex_tracy</dc:creator>
    <dc:date>2024-07-30T07:57:41Z</dc:date>
    <item>
      <title>IMX8MP, WM8962, aplay: pcm_write:2127: write error: Input/output error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-WM8962-aplay-pcm-write-2127-write-error-Input-output/m-p/1911814#M226368</link>
      <description>&lt;P&gt;An error occurred when specifying wm8962 to play music on IMX8MP&lt;BR /&gt;Can help me solve this problem?&lt;/P&gt;&lt;P&gt;root@imx8mpevk:~# aplay -l&lt;BR /&gt;**** List of PLAYBACK Hardware Devices ****&lt;BR /&gt;card 0: btscoaudio [bt-sco-audio], device 0: 30c20000.sai-bt-sco-pcm-wb bt-sco-pcm-wb-0 [30c20000.sai-bt-sco-pcm-wb bt-sco-pcm-wb-0]&lt;BR /&gt;Subdevices: 1/1&lt;BR /&gt;Subdevice #0: subdevice #0&lt;BR /&gt;card 1: audiohdmi [audio-hdmi], device 0: i.MX HDMI i2s-hifi-0 [i.MX HDMI i2s-hifi-0]&lt;BR /&gt;Subdevices: 1/1&lt;BR /&gt;Subdevice #0: subdevice #0&lt;BR /&gt;card 3: wm8962audio [wm8962-audio], device 0: HiFi wm8962-0 [HiFi wm8962-0]&lt;BR /&gt;Subdevices: 1/1&lt;BR /&gt;Subdevice #0: subdevice #0&lt;BR /&gt;card 4: imxaudioxcvr [imx-audio-xcvr], device 0: XCVR PCM snd-soc-dummy-dai-0 [XCVR PCM snd-soc-dummy-dai-0]&lt;BR /&gt;Subdevices: 1/1&lt;BR /&gt;Subdevice #0: subdevice #0&lt;/P&gt;&lt;P&gt;root@imx8mpevk:~# aplay -Dhw:3,0 -r 44100 JAX_V.wav&lt;BR /&gt;Playing WAVE 'JAX_V.wav' : Signed 16 bit Little Endian, Rate 44100 Hz, Stereo&lt;BR /&gt;aplay: pcm_write:2127: write error: Input/output error&lt;BR /&gt;root@imx8mpevk:~#&lt;/P&gt;</description>
      <pubDate>Fri, 19 Jul 2024 04:15:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-WM8962-aplay-pcm-write-2127-write-error-Input-output/m-p/1911814#M226368</guid>
      <dc:creator>Lex_tracy</dc:creator>
      <dc:date>2024-07-19T04:15:08Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP, WM8962, aplay: pcm_write:2127: write error: Input/output error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-WM8962-aplay-pcm-write-2127-write-error-Input-output/m-p/1913502#M226429</link>
      <description>&lt;P&gt;Hi &lt;BR /&gt;&lt;BR /&gt;Please also test other devices, try to play the file on a different audio device to see if the issue is specific to hw:3,0.&lt;/P&gt;
&lt;P&gt;Then check and update the ALSA configuration to ensure it is correctly set up for the device, editing the /etc/asound.conf or ~/.asoundrc files.&lt;/P&gt;
&lt;P&gt;You can use dmesg to view the logs:&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;dmesg | grep -i snd
&lt;/LI-CODE&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Mon, 22 Jul 2024 01:34:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-WM8962-aplay-pcm-write-2127-write-error-Input-output/m-p/1913502#M226429</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2024-07-22T01:34:57Z</dc:date>
    </item>
    <item>
      <title>回复： IMX8MP, WM8962, aplay: pcm_write:2127: write error: Input/output error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-WM8962-aplay-pcm-write-2127-write-error-Input-output/m-p/1918917#M226681</link>
      <description>&lt;P&gt;HI&amp;nbsp;&lt;/P&gt;&lt;P&gt;problem is specific to hw:3,0.&lt;BR /&gt;I check asound.conf no find problem , I not find .asoundrc files&lt;BR /&gt;I use dmesg | grep -i snd, no find anything&lt;BR /&gt;but use dmesg |grep 8962 ,find error&lt;BR /&gt;ASoC: error at soc_component_read_no_lock on wm8962.2-001a: -16&lt;BR /&gt;this error effect audio aplay?&lt;/P&gt;</description>
      <pubDate>Mon, 29 Jul 2024 02:18:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-WM8962-aplay-pcm-write-2127-write-error-Input-output/m-p/1918917#M226681</guid>
      <dc:creator>Lex_tracy</dc:creator>
      <dc:date>2024-07-29T02:18:08Z</dc:date>
    </item>
    <item>
      <title>回复： IMX8MP, WM8962, aplay: pcm_write:2127: write error: Input/output error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-WM8962-aplay-pcm-write-2127-write-error-Input-output/m-p/1919899#M226723</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Please refer this case to check MCLK setting and your hardware.&lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/i-mx8mp%E7%A7%BB%E6%A4%8Dwm8962%E8%8A%AF%E7%89%87%E6%8A%A5%E9%94%99/m-p/1617217/highlight/true" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/i-mx8mp%E7%A7%BB%E6%A4%8Dwm8962%E8%8A%AF%E7%89%87%E6%8A%A5%E9%94%99/m-p/1617217/highlight/true&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Tue, 30 Jul 2024 02:26:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-WM8962-aplay-pcm-write-2127-write-error-Input-output/m-p/1919899#M226723</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2024-07-30T02:26:25Z</dc:date>
    </item>
    <item>
      <title>回复： IMX8MP, WM8962, aplay: pcm_write:2127: write error: Input/output error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-WM8962-aplay-pcm-write-2127-write-error-Input-output/m-p/1920239#M226741</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I referred to the case you provided and used the methods in it to correct it.&lt;BR /&gt;ASoC: error at soc_component_read_no_lock on wm8962.2-001a: -16&lt;BR /&gt;Now dmesg will not cause this error , thank you.&lt;/P&gt;&lt;P&gt;But aplay: pcm_write:2127: write error: Input/output error is not resolved&lt;BR /&gt;I refer to /arch/arm64/boot/dts/freescale/imx8mm-beacon-baseboard.dtsi to set the same clocks&lt;BR /&gt;"assigned-clock-rates = &amp;lt;24576000&amp;gt;;"&lt;BR /&gt;Use an oscilloscope to measure that when he plays music, it is indeed the same as the clock I set.&lt;BR /&gt;Are there any other areas that need attention and need to be checked?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 30 Jul 2024 07:57:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-WM8962-aplay-pcm-write-2127-write-error-Input-output/m-p/1920239#M226741</guid>
      <dc:creator>Lex_tracy</dc:creator>
      <dc:date>2024-07-30T07:57:41Z</dc:date>
    </item>
  </channel>
</rss>