<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: [Camera] RPI-CAM-MIPI can't be loaded.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Camera-RPI-CAM-MIPI-can-t-be-loaded/m-p/1919967#M226729</link>
    <description>&lt;P&gt;Probably it's due to the driver is not built with core image, let's see if this is reproducible on the full image.&lt;/P&gt;</description>
    <pubDate>Tue, 30 Jul 2024 04:38:24 GMT</pubDate>
    <dc:creator>JosephAtNXP</dc:creator>
    <dc:date>2024-07-30T04:38:24Z</dc:date>
    <item>
      <title>[Camera] RPI-CAM-MIPI can't be loaded.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Camera-RPI-CAM-MIPI-can-t-be-loaded/m-p/1918911#M226680</link>
      <description>&lt;P&gt;Hi, everyone.&lt;/P&gt;&lt;P&gt;I'm working on a project with the iMX93 EVK board and tried testing my RPI-CAM-MIPI camera. However, I encountered the following problem:&lt;/P&gt;&lt;P&gt;```sh&lt;BR /&gt;root@imx93-11x11-lpddr4x-evk:~# dmesg | grep -E 'ap1302|mx8-img-md'&lt;BR /&gt;[ 0.339795] platform 4ae00000.csi: Fixed dependency cycle(s) with /soc@0/bus@42000000/i2c@42530000/ap1302_mipi@3c&lt;BR /&gt;[ 2.642404] ap1302_mipi 2-003c: AP1302 Chip ID is 0x265&lt;BR /&gt;[ 2.647704] ap1302_mipi 2-003c: Direct firmware load for imx/camera/ap1302.fw failed with error -2&lt;BR /&gt;[ 2.651999] ap1302_mipi 2-003c: AP1302 is found&lt;BR /&gt;[ 2.656681] ap1302_mipi 2-003c: Falling back to sysfs fallback for: imx/camera/ap1302.fw&lt;BR /&gt;root@imx93-11x11-lpddr4x-evk:~# [ 64.661849] cfg80211: failed to load regulatory.db&lt;BR /&gt;[ 64.661854] ap1302_mipi 2-003c: Failed to request_firmware&lt;BR /&gt;```&lt;/P&gt;&lt;P&gt;Here are the details of my workspace:&lt;/P&gt;&lt;P&gt;- DISTRO: poky&lt;BR /&gt;- Bitbake image: core-image-base&lt;/P&gt;&lt;P&gt;I've followed the RPI-CAM-MIPI QSG document thoroughly and ensured I did everything as instructed.&lt;/P&gt;&lt;P&gt;Is there any problem with my DISTRO setting or image configuration? I would appreciate any advice or suggestions.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Mon, 29 Jul 2024 02:13:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Camera-RPI-CAM-MIPI-can-t-be-loaded/m-p/1918911#M226680</guid>
      <dc:creator>dpcivl</dc:creator>
      <dc:date>2024-07-29T02:13:35Z</dc:date>
    </item>
    <item>
      <title>Re: [Camera] RPI-CAM-MIPI can't be loaded.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Camera-RPI-CAM-MIPI-can-t-be-loaded/m-p/1919746#M226711</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;What revision is your board?&lt;/P&gt;
&lt;P&gt;Does the issue repeat when using prebuilts from nxp.com?&lt;/P&gt;
&lt;P&gt;NXP colleagues used the i.MX93-EVK prebuilt image downloaded from the NXP website, followed the &lt;A href="https://www.nxp.com/docs/en/release-note/IMX_LINUX_RELEASE_NOTES.pdf" target="_self"&gt;release notes&lt;/A&gt; and downloaded the firmware using git clone.&lt;/P&gt;
&lt;P&gt;This should be OK since they have successfully run this.&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;$ gst-launch-1.0 v4l2src device=/dev/video0 ! autovideosink&lt;/LI-CODE&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Mon, 29 Jul 2024 19:27:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Camera-RPI-CAM-MIPI-can-t-be-loaded/m-p/1919746#M226711</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2024-07-29T19:27:19Z</dc:date>
    </item>
    <item>
      <title>Re: [Camera] RPI-CAM-MIPI can't be loaded.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Camera-RPI-CAM-MIPI-can-t-be-loaded/m-p/1919837#M226714</link>
      <description>I'm trying to build my own BSP with Yocto Project. I know that you provide pre-built image and I could build it. For my learning, I just want to make layers for my project. Though I'm building 'imx-image-full' right now, I was curious about how I could use RPI-CAM-MIPI with poky distro in Yocto Project.</description>
      <pubDate>Tue, 30 Jul 2024 00:24:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Camera-RPI-CAM-MIPI-can-t-be-loaded/m-p/1919837#M226714</guid>
      <dc:creator>dpcivl</dc:creator>
      <dc:date>2024-07-30T00:24:19Z</dc:date>
    </item>
    <item>
      <title>Re: [Camera] RPI-CAM-MIPI can't be loaded.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Camera-RPI-CAM-MIPI-can-t-be-loaded/m-p/1919967#M226729</link>
      <description>&lt;P&gt;Probably it's due to the driver is not built with core image, let's see if this is reproducible on the full image.&lt;/P&gt;</description>
      <pubDate>Tue, 30 Jul 2024 04:38:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Camera-RPI-CAM-MIPI-can-t-be-loaded/m-p/1919967#M226729</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2024-07-30T04:38:24Z</dc:date>
    </item>
  </channel>
</rss>