<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IMX8 bitbake image fail with package depend error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-bitbake-image-fail-with-package-depend-error/m-p/1917696#M226621</link>
    <description>&lt;P&gt;I try to build the full image with host &amp;lt;22.04.1-Ubuntu &amp;gt; with success.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
    <pubDate>Fri, 26 Jul 2024 02:33:20 GMT</pubDate>
    <dc:creator>Harvey021</dc:creator>
    <dc:date>2024-07-26T02:33:20Z</dc:date>
    <item>
      <title>IMX8 bitbake image fail with package depend error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-bitbake-image-fail-with-package-depend-error/m-p/1914887#M226502</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;I got the erro message from 'bitbake imx-image-full'&amp;nbsp;&lt;/P&gt;&lt;P&gt;```&lt;/P&gt;&lt;P&gt;ERROR: imx-image-full-1.0-r0 do_rootfs: Unable to install packages. Command '/home/vmware/imx-yocto-bsp/build-xwayland/tmp/work/imx8mm_lpddr4_evk-poky-linux/imx-image-full/1.0/recipe-sysroot-native/usr/bin/apt-get install --allow-downgrades --allow-remove-essential --allow-change-held-packages --allow-unauthenticated --no-remove apt curl docker dpkg firmwared imx-g2d-samples jailhouse opencv-apps opencv-samples optee-client optee-os os-release packagegroup-base-extended packagegroup-core-boot packagegroup-core-full-cmdline packagegroup-core-nfs-client packagegroup-core-sdk packagegroup-core-ssh-openssh packagegroup-core-standalone-sdk-target packagegroup-core-tools-debug packagegroup-core-tools-profile packagegroup-core-tools-testapps packagegroup-core-weston packagegroup-fsl-gstreamer1.0 packagegroup-fsl-gstreamer1.0-full packagegroup-fsl-optee-imx packagegroup-fsl-tools-audio packagegroup-fsl-tools-benchmark packagegroup-fsl-tools-gpu packagegroup-fsl-tools-gpu-external packagegroup-fsl-tools-testapps packagegroup-imx-isp packagegroup-imx-ml packagegroup-imx-security packagegroup-qt6-imx packagegroup-security-parsec packagegroup-security-tpm2 packagegroup-tools-bluetooth psplash python3-opencv run-postinsts softhsm swtpm tzdata weston-xwayland xterm' returned 100:&lt;BR /&gt;Reading package lists...&lt;BR /&gt;Building dependency tree...&lt;BR /&gt;Reading state information...&lt;BR /&gt;Some packages could not be installed. This may mean that you have&lt;BR /&gt;requested an impossible situation or if you are using the unstable&lt;BR /&gt;distribution that some required packages have not yet been created&lt;BR /&gt;or been moved out of Incoming.&lt;BR /&gt;The following information may help to resolve the situation:&lt;/P&gt;&lt;P&gt;The following packages have unmet dependencies:&lt;BR /&gt;kernel-module-jailhouse-6.6.23-lts-next-gb586a521770e : Depends: kernel-6.6.23-lts-next-gb586a521770e but it is not installable&lt;BR /&gt;packagegroup-fsl-tools-testapps : Depends: cryptodev-module but it is not installable&lt;BR /&gt;E: Unable to correct problems, you have held broken packages.&lt;/P&gt;&lt;P&gt;ERROR: Logfile of failure stored in: /home/vmware/imx-yocto-bsp/build-xwayland/tmp/work/imx8mm_lpddr4_evk-poky-linux/imx-image-full/1.0/temp/log.do_rootfs.229769&lt;BR /&gt;ERROR: Task (/home/vmware/imx-yocto-bsp/sources/meta-imx/meta-imx-sdk/dynamic-layers/qt6-layer/recipes-fsl/images/imx-image-full.bb:do_rootfs) failed with exit code '1'&lt;/P&gt;&lt;P&gt;```&lt;/P&gt;&lt;P&gt;What's the meaning of this error and what should we do next.&lt;/P&gt;</description>
      <pubDate>Tue, 23 Jul 2024 09:42:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8-bitbake-image-fail-with-package-depend-error/m-p/1914887#M226502</guid>
      <dc:creator>Mingheng</dc:creator>
      <dc:date>2024-07-23T09:42:28Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8 bitbake image fail with package depend error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-bitbake-image-fail-with-package-depend-error/m-p/1917696#M226621</link>
      <description>&lt;P&gt;I try to build the full image with host &amp;lt;22.04.1-Ubuntu &amp;gt; with success.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Fri, 26 Jul 2024 02:33:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8-bitbake-image-fail-with-package-depend-error/m-p/1917696#M226621</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2024-07-26T02:33:20Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8 bitbake image fail with package depend error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-bitbake-image-fail-with-package-depend-error/m-p/1917878#M226630</link>
      <description>Thanks for your reply&lt;BR /&gt;&lt;BR /&gt;I tried to removed the build directory and rebuild, with success.&lt;BR /&gt;I think the reason is that there was no enouth memory for building so that the tasks were closed by ubuntu system, seems like input stopped command(ctrl + C).&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;Mingheng</description>
      <pubDate>Fri, 26 Jul 2024 07:06:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8-bitbake-image-fail-with-package-depend-error/m-p/1917878#M226630</guid>
      <dc:creator>Mingheng</dc:creator>
      <dc:date>2024-07-26T07:06:42Z</dc:date>
    </item>
  </channel>
</rss>