<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic imx-usb with windows in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx-usb-with-windows/m-p/1916857#M226585</link>
    <description>&lt;P&gt;I am trying to use the imx_usb binary with an i.MX6ULL device.&lt;/P&gt;&lt;P&gt;I built the imx-usb binary using the following steps in the Cygwin terminal:&lt;/P&gt;&lt;P&gt;git clone &lt;A href="https://github.com/boundarydevices/imx_usb_loader.git" target="_blank"&gt;https://github.com/boundarydevices/imx_usb_loader.git&lt;/A&gt;&lt;BR /&gt;cd imx_usb_loader&lt;BR /&gt;git reset --hard c598fd14d67&lt;BR /&gt;make&lt;/P&gt;&lt;P&gt;After completing the above steps, the imx_usb binary is generated.&lt;/P&gt;&lt;P&gt;Next, I put the board into flashing mode and executed the imx_usb binary in the Cygwin terminal.&lt;/P&gt;&lt;P&gt;However, I encountered the following error message on the console:&lt;/P&gt;&lt;P&gt;failed to run ./imx_usb&lt;/P&gt;&lt;P&gt;Could you please let me know if there is anything else that needs to be done?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in Advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Sandhya&lt;/P&gt;</description>
    <pubDate>Thu, 25 Jul 2024 05:58:09 GMT</pubDate>
    <dc:creator>sandhya_05</dc:creator>
    <dc:date>2024-07-25T05:58:09Z</dc:date>
    <item>
      <title>imx-usb with windows</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-usb-with-windows/m-p/1916857#M226585</link>
      <description>&lt;P&gt;I am trying to use the imx_usb binary with an i.MX6ULL device.&lt;/P&gt;&lt;P&gt;I built the imx-usb binary using the following steps in the Cygwin terminal:&lt;/P&gt;&lt;P&gt;git clone &lt;A href="https://github.com/boundarydevices/imx_usb_loader.git" target="_blank"&gt;https://github.com/boundarydevices/imx_usb_loader.git&lt;/A&gt;&lt;BR /&gt;cd imx_usb_loader&lt;BR /&gt;git reset --hard c598fd14d67&lt;BR /&gt;make&lt;/P&gt;&lt;P&gt;After completing the above steps, the imx_usb binary is generated.&lt;/P&gt;&lt;P&gt;Next, I put the board into flashing mode and executed the imx_usb binary in the Cygwin terminal.&lt;/P&gt;&lt;P&gt;However, I encountered the following error message on the console:&lt;/P&gt;&lt;P&gt;failed to run ./imx_usb&lt;/P&gt;&lt;P&gt;Could you please let me know if there is anything else that needs to be done?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in Advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Sandhya&lt;/P&gt;</description>
      <pubDate>Thu, 25 Jul 2024 05:58:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-usb-with-windows/m-p/1916857#M226585</guid>
      <dc:creator>sandhya_05</dc:creator>
      <dc:date>2024-07-25T05:58:09Z</dc:date>
    </item>
  </channel>
</rss>