<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Error booting Linux in imx8qm</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Error-booting-Linux-in-imx8qm/m-p/1916769#M226576</link>
    <description>&lt;P&gt;hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/235870"&gt;@carloscs11&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;what is your DDR type? what is your BSP version?&lt;/P&gt;</description>
    <pubDate>Thu, 25 Jul 2024 03:04:04 GMT</pubDate>
    <dc:creator>pengyong_zhang</dc:creator>
    <dc:date>2024-07-25T03:04:04Z</dc:date>
    <item>
      <title>Error booting Linux in imx8qm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-booting-Linux-in-imx8qm/m-p/1915564#M226532</link>
      <description>&lt;P&gt;Hello guys!&lt;/P&gt;&lt;P&gt;I am trying to boot a Linux Image in the imx8qm. Unfortunately, I'm getting a panic message in the memory initialization. This is kernel messages:&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:735] [ 0.000000] Initmem setup node 0 [mem 0x0000000080200000-0x00000000a01fffff]&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:735] [ 0.000000] SError Interrupt on CPU0, code 0xbf000002 -- SError&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:751] [ 0.000000] CPU: 0 PID: 0 Comm: swapper Not tainted 5.4.24 #2&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:751] [ 0.000000] Hardware name: fsl,imx8qm-mek (DT)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:751] [ 0.000000] pstate: 40000085 (nZcv daIf -PAN -UAO)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:767] [ 0.000000] pc : set_pageblock_migratetype+0x0/0x50&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:767] [ 0.000000] lr : memmap_init_zone+0x18c/0x1b0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:767] [ 0.000000] sp : ffff800012883ce0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:767] [ 0.000000] x29: ffff800012883ce0 x28: 0000000000080200 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:783] [ 0.000000] x27: ffff8000128ac6c8 x26: ffff800011932000 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:783] [ 0.000000] x25: 0ffff00000000000 x24: 0000000000000000 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:783] [ 0.000000] x23: 00000000000a0200 x22: 0000000000000000 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:799] [ 0.000000] x21: 0ffff00000001000 x20: ffff800012b36560 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:799] [ 0.000000] x19: 0000000000080200 x18: ffff800012b0fcda &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:799] [ 0.000000] x17: 0000000000000000 x16: 0000000000000000 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:815] [ 0.000000] x15: ffff8000128a1b50 x14: 0000000000000000 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:815] [ 0.000000] x13: ffff800012b0f000 x12: ffff8000128a1000 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:815] [ 0.000000] x11: ffff800012b0f328 x10: 0000000000000000 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:831] [ 0.000000] x9 : 0000000000000000 x8 : 0000000020000000 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:831] [ 0.000000] x7 : 0000000000000018 x6 : ffff800012b36618 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:831] [ 0.000000] x5 : 0000000000000001 x4 : 00000000ffffffff &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:847] [ 0.000000] x3 : fffffdffffe08008 x2 : 0000000002008000 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:847] [ 0.000000] x1 : 0000000000000001 x0 : fffffdffffe08000 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:847] [ 0.000000] Kernel panic - not syncing: Asynchronous SError Interrupt&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:863] [ 0.000000] CPU: 0 PID: 0 Comm: swapper Not tainted 5.4.24 #2&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:863] [ 0.000000] Hardware name: fsl,imx8qm-mek (DT)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:863] [ 0.000000] Call trace:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:879] [ 0.000000] dump_backtrace+0x0/0x130&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:879] [ 0.000000] show_stack+0x14/0x20&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:879] [ 0.000000] dump_stack+0xb4/0x100&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:879] [ 0.000000] panic+0x158/0x324&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:879] [ 0.000000] nmi_panic+0x84/0x90&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:895] [ 0.000000] arm64_serror_panic+0x74/0x80&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:895] [ 0.000000] enter_from_user_mode+0x0/0x10&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:895] [ 0.000000] el1_error+0x84/0xf8&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:895] [ 0.000000] set_pageblock_migratetype+0x0/0x50&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:911] [ 0.000000] memmap_init+0x14/0x1c&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:911] [ 0.000000] free_area_init_node+0x34c/0x470&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:911] [ 0.000000] free_area_init_nodes+0x5c8/0x658&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:911] [ 0.000000] bootmem_init+0xa0/0xd8&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:927] [ 0.000000] setup_arch+0x264/0x5cc&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;[22:07:08:927] [ 0.000000] start_kernel+0x84/0x448&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;I am not an expert in Linux kernel so if somebody could give me a light about why this error is happening, I would be grateful.&lt;BR /&gt;&lt;BR /&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Tue, 23 Jul 2024 21:27:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-booting-Linux-in-imx8qm/m-p/1915564#M226532</guid>
      <dc:creator>carloscs11</dc:creator>
      <dc:date>2024-07-23T21:27:10Z</dc:date>
    </item>
    <item>
      <title>Re: Error booting Linux in imx8qm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-booting-Linux-in-imx8qm/m-p/1916769#M226576</link>
      <description>&lt;P&gt;hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/235870"&gt;@carloscs11&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;what is your DDR type? what is your BSP version?&lt;/P&gt;</description>
      <pubDate>Thu, 25 Jul 2024 03:04:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-booting-Linux-in-imx8qm/m-p/1916769#M226576</guid>
      <dc:creator>pengyong_zhang</dc:creator>
      <dc:date>2024-07-25T03:04:04Z</dc:date>
    </item>
  </channel>
</rss>