<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Modifying imx8mp_evk.dts File on i.MX 8M Plus Board: Direct Edits or Patches Needed? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Modifying-imx8mp-evk-dts-File-on-i-MX-8M-Plus-Board-Direct-Edits/m-p/1916045#M226559</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using an i.MX 8M Plus board and want to modify the imx8mp_evk.dts file. Currently, I modify the DTS file directly and then compile it. Is this the correct way to do it, or do I need to apply any patches or bindings? If anyone knows, please help me.&lt;/P&gt;&lt;P&gt;Regaeds&lt;/P&gt;&lt;P&gt;srinivas&lt;/P&gt;&lt;HR /&gt;</description>
    <pubDate>Wed, 24 Jul 2024 09:58:47 GMT</pubDate>
    <dc:creator>srinivas_123</dc:creator>
    <dc:date>2024-07-24T09:58:47Z</dc:date>
    <item>
      <title>Modifying imx8mp_evk.dts File on i.MX 8M Plus Board: Direct Edits or Patches Needed?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Modifying-imx8mp-evk-dts-File-on-i-MX-8M-Plus-Board-Direct-Edits/m-p/1916045#M226559</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using an i.MX 8M Plus board and want to modify the imx8mp_evk.dts file. Currently, I modify the DTS file directly and then compile it. Is this the correct way to do it, or do I need to apply any patches or bindings? If anyone knows, please help me.&lt;/P&gt;&lt;P&gt;Regaeds&lt;/P&gt;&lt;P&gt;srinivas&lt;/P&gt;&lt;HR /&gt;</description>
      <pubDate>Wed, 24 Jul 2024 09:58:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Modifying-imx8mp-evk-dts-File-on-i-MX-8M-Plus-Board-Direct-Edits/m-p/1916045#M226559</guid>
      <dc:creator>srinivas_123</dc:creator>
      <dc:date>2024-07-24T09:58:47Z</dc:date>
    </item>
  </channel>
</rss>