<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IMX8MN Boot From NOR Flash</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MN-Boot-From-NOR-Flash/m-p/1910354#M226269</link>
    <description>&lt;P&gt;Are you using NXP reference board or the board you designed yourself? Which version BSP are you using?&lt;/P&gt;</description>
    <pubDate>Wed, 17 Jul 2024 07:23:07 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2024-07-17T07:23:07Z</dc:date>
    <item>
      <title>IMX8MN Boot From NOR Flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MN-Boot-From-NOR-Flash/m-p/1906344#M226085</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;We are using IMX8MNano processor with wind bond NOR Flash (W25Q01JV ). We are trying&amp;nbsp; to use NOR Flash as boot device.&lt;/P&gt;&lt;P&gt;we built&amp;nbsp;imx-boot-imx8mn-ddr4-evk-fspi.bin-flash_ddr4_evk_flexspi using Yocto.&lt;/P&gt;&lt;P&gt;I copied this file&amp;nbsp; in NOR Flash and changed switch settings.&amp;nbsp;&lt;/P&gt;&lt;P&gt;mtdinfo /dev/mtd0&lt;BR /&gt;mtd0&lt;BR /&gt;Name: u-boot&lt;BR /&gt;Type: nor&lt;BR /&gt;Erase lock size: 65536 bytes, 64.0 KiB&lt;BR /&gt;Amount of erase blocks: 32 (2097152 bytes, 2.0 MiB)&lt;BR /&gt;Minimum input/output unit size: 1 byte&lt;BR /&gt;Sub-page size: 1 byte&lt;BR /&gt;Character device major/minor: 90:0&lt;BR /&gt;Bad blocks are allowed: false&lt;BR /&gt;Device is writable: true&lt;/P&gt;&lt;P&gt;flash_erase /dev/mtd0 0x0 32&lt;BR /&gt;flashcp imx-boot-phyboard-polis-imx8mm-5-fspi.bin-flash_evk_flexspi /dev/mtd0&lt;/P&gt;&lt;P&gt;We are not seeing any log over UART Console.&lt;/P&gt;&lt;P&gt;Could you please guide us for this issue.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ramji Mishra&lt;/P&gt;</description>
      <pubDate>Thu, 11 Jul 2024 13:37:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MN-Boot-From-NOR-Flash/m-p/1906344#M226085</guid>
      <dc:creator>ramji1</dc:creator>
      <dc:date>2024-07-11T13:37:36Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MN Boot From NOR Flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MN-Boot-From-NOR-Flash/m-p/1910354#M226269</link>
      <description>&lt;P&gt;Are you using NXP reference board or the board you designed yourself? Which version BSP are you using?&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jul 2024 07:23:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MN-Boot-From-NOR-Flash/m-p/1910354#M226269</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2024-07-17T07:23:07Z</dc:date>
    </item>
  </channel>
</rss>