<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX95 LCDIF in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX95-LCDIF/m-p/1910188#M226256</link>
    <description>&lt;P&gt;what's your request from imx95? as I known, imx95 doesn't have LCDIF&lt;/P&gt;</description>
    <pubDate>Wed, 17 Jul 2024 02:41:47 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2024-07-17T02:41:47Z</dc:date>
    <item>
      <title>iMX95 LCDIF</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX95-LCDIF/m-p/1909566#M226218</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am considering the new family of iMX 9 for an upcoming series of products. The 93 is a good fit for the base model, but is limited for the upgraded version. The upgraded version could be on the 95. One specification is dual display using MIPI DSI and/or LVDS. The 93 is limited to only one of those interfaces since it only has one LCDIF.&lt;/P&gt;&lt;P&gt;What is the LCDIF configurations of the 95? I can't check if it has more than one since the reference manual is not yet available (or at least I can't find it).&lt;/P&gt;&lt;P&gt;Thank you for taking the time to read my question &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 16 Jul 2024 08:28:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX95-LCDIF/m-p/1909566#M226218</guid>
      <dc:creator>SoftTransistor</dc:creator>
      <dc:date>2024-07-16T08:28:36Z</dc:date>
    </item>
    <item>
      <title>Re: iMX95 LCDIF</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX95-LCDIF/m-p/1910188#M226256</link>
      <description>&lt;P&gt;what's your request from imx95? as I known, imx95 doesn't have LCDIF&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jul 2024 02:41:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX95-LCDIF/m-p/1910188#M226256</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2024-07-17T02:41:47Z</dc:date>
    </item>
  </channel>
</rss>