<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 IMX8QXP  NVMe SSD support</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-NVMe-SSD-support/m-p/1899970#M225914</link>
    <description>&lt;P&gt;Dear NXP Team,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;We are exploring options to connect an SATA SSD to our custom-designed IMX8QXP board, but we've observed that the processor lacks SATA support. Therefore, we are considering connecting an NVMe-based SSD via the PCIe interface on the M.2 connector instead. Could you confirm if this is feasible? Also, do we have driver support available for this configuration?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 05 Jul 2024 06:24:11 GMT</pubDate>
    <dc:creator>Chethanbg</dc:creator>
    <dc:date>2024-07-05T06:24:11Z</dc:date>
    <item>
      <title>IMX8QXP  NVMe SSD support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-NVMe-SSD-support/m-p/1899970#M225914</link>
      <description>&lt;P&gt;Dear NXP Team,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;We are exploring options to connect an SATA SSD to our custom-designed IMX8QXP board, but we've observed that the processor lacks SATA support. Therefore, we are considering connecting an NVMe-based SSD via the PCIe interface on the M.2 connector instead. Could you confirm if this is feasible? Also, do we have driver support available for this configuration?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 05 Jul 2024 06:24:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-NVMe-SSD-support/m-p/1899970#M225914</guid>
      <dc:creator>Chethanbg</dc:creator>
      <dc:date>2024-07-05T06:24:11Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QXP  NVMe SSD support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-NVMe-SSD-support/m-p/1901880#M225980</link>
      <description>&lt;P&gt;checked the imx8qxp schematic, which support M.2 KEY E, if you need connect SSD via M.2 connector, you need convert M.2 KEY E to M.2 KEY M to support this, the cable like this&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.ebay.nl/itm/386952338953?itmmeta=01J28KZ1HAFDHGFEGXSRBY1VB8&amp;amp;hash=item5a18281e09:g:j30AAOSwU-dmJ6rq&amp;amp;itmprp=enc%3AAQAJAAABELoHS1smZIzgFFruqSTh3Roh9ZXjJH2r8b5CQH1TfimEcK8%2FkLdgw39vrKUVvmPllQifm5unPLGdzRbSpgpAYPYolnvZ6YXri07VSK6Qwutfx7TJs8ta4xuJvQdnXy%2FaGyStsfl8naWNIXIy3H0rbJ5pfpio%2FL89af7bYOPov3WQPRuxbyGyFOOJE0wbgXEST9d5yW2Js5%2BVwEDKUlCoirZ%2FXJEali9JEcbdtOQu0HGL9SzS%2FmEL%2FkW982jRak3fWt18zwWRelCHlbgTFzLbo--QD4ZiPB2faK%2F9j0lD9j2csqFW0lvK2Z1khpfffdnopiEQYu%2FSZ1bUh2yJdgBv0nwXulDb6n1nLec4BSsD62Le%7Ctkp%3ABFBM3Jj8k5Jk" target="_self"&gt;Sintech M.2 (NGFF) NVME SSD to M2 A/E Key WiFi Port with 20cm Cable&lt;/A&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 08 Jul 2024 07:31:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-NVMe-SSD-support/m-p/1901880#M225980</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2024-07-08T07:31:04Z</dc:date>
    </item>
  </channel>
</rss>