<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Code Signing Tool with keys in HSM in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Code-Signing-Tool-with-keys-in-HSM/m-p/1898519#M225826</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;when signing an bootloader with code signing tool (cst) the private key is needed to create the signature.&lt;/P&gt;&lt;P&gt;We want to have the private keys in a HSM but not the certificates (which are stored on the file system)&lt;/P&gt;&lt;P&gt;All the examples define the certificate to be used for signing (e.g. in the CSF file):&lt;/P&gt;&lt;P&gt;&lt;EM&gt;[Install CSFK]&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;File = "pkcs11:token=CST-HSM-DEMO;object=CSF1_1_sha256_2048_65537_v3_usr;type=&lt;STRONG&gt;cert&lt;/STRONG&gt;;pin-value=${USR_PIN}"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;So I wondering how I can tell the cst which private key it should use.&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;Thomas&lt;/P&gt;</description>
    <pubDate>Wed, 03 Jul 2024 16:27:12 GMT</pubDate>
    <dc:creator>ThomasGu</dc:creator>
    <dc:date>2024-07-03T16:27:12Z</dc:date>
    <item>
      <title>Code Signing Tool with keys in HSM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Code-Signing-Tool-with-keys-in-HSM/m-p/1898519#M225826</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;when signing an bootloader with code signing tool (cst) the private key is needed to create the signature.&lt;/P&gt;&lt;P&gt;We want to have the private keys in a HSM but not the certificates (which are stored on the file system)&lt;/P&gt;&lt;P&gt;All the examples define the certificate to be used for signing (e.g. in the CSF file):&lt;/P&gt;&lt;P&gt;&lt;EM&gt;[Install CSFK]&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;File = "pkcs11:token=CST-HSM-DEMO;object=CSF1_1_sha256_2048_65537_v3_usr;type=&lt;STRONG&gt;cert&lt;/STRONG&gt;;pin-value=${USR_PIN}"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;So I wondering how I can tell the cst which private key it should use.&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;Thomas&lt;/P&gt;</description>
      <pubDate>Wed, 03 Jul 2024 16:27:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Code-Signing-Tool-with-keys-in-HSM/m-p/1898519#M225826</guid>
      <dc:creator>ThomasGu</dc:creator>
      <dc:date>2024-07-03T16:27:12Z</dc:date>
    </item>
  </channel>
</rss>