<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Steps to connect a microcontroller to  imx8mp using a usb cdc class</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Steps-to-connect-a-microcontroller-to-imx8mp-using-a-usb-cdc/m-p/1897545#M225754</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;For my project, I am meant to send data to my imx8mp device from the usb port of a microcontroller.&amp;nbsp; This is a completely new topic for me and I would like to know if nxp have some material in this light.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Below are some information to my project&lt;/P&gt;&lt;P&gt;1.&amp;nbsp; IMX8 is the host device and would fetch data from the microcontoller when it needs the data.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2.&amp;nbsp; There is a 2 port USB hub between the imx8 and the microcontroller.&lt;/P&gt;&lt;P&gt;3. I have selected the usb cdc class for my usb operation and high speed.&lt;/P&gt;&lt;P&gt;4. I would like to use the libusb library.&lt;/P&gt;&lt;P&gt;5.&amp;nbsp; I also want to write a linux user space app?&lt;/P&gt;&lt;P&gt;6.&amp;nbsp; I would also write a c# application to receive data from the imx8mp&lt;/P&gt;&lt;P&gt;Are there any NXP application report or link or previous issues that can help me in this&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Tue, 02 Jul 2024 13:46:15 GMT</pubDate>
    <dc:creator>ababatola</dc:creator>
    <dc:date>2024-07-02T13:46:15Z</dc:date>
    <item>
      <title>Steps to connect a microcontroller to  imx8mp using a usb cdc class</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Steps-to-connect-a-microcontroller-to-imx8mp-using-a-usb-cdc/m-p/1897545#M225754</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;For my project, I am meant to send data to my imx8mp device from the usb port of a microcontroller.&amp;nbsp; This is a completely new topic for me and I would like to know if nxp have some material in this light.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Below are some information to my project&lt;/P&gt;&lt;P&gt;1.&amp;nbsp; IMX8 is the host device and would fetch data from the microcontoller when it needs the data.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2.&amp;nbsp; There is a 2 port USB hub between the imx8 and the microcontroller.&lt;/P&gt;&lt;P&gt;3. I have selected the usb cdc class for my usb operation and high speed.&lt;/P&gt;&lt;P&gt;4. I would like to use the libusb library.&lt;/P&gt;&lt;P&gt;5.&amp;nbsp; I also want to write a linux user space app?&lt;/P&gt;&lt;P&gt;6.&amp;nbsp; I would also write a c# application to receive data from the imx8mp&lt;/P&gt;&lt;P&gt;Are there any NXP application report or link or previous issues that can help me in this&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jul 2024 13:46:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Steps-to-connect-a-microcontroller-to-imx8mp-using-a-usb-cdc/m-p/1897545#M225754</guid>
      <dc:creator>ababatola</dc:creator>
      <dc:date>2024-07-02T13:46:15Z</dc:date>
    </item>
    <item>
      <title>Re: Steps to connect a microcontroller to  imx8mp using a usb cdc class</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Steps-to-connect-a-microcontroller-to-imx8mp-using-a-usb-cdc/m-p/1898477#M225824</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;All the previous question work with linux BSP, so please download, we have no an application ready but you can download someone for it.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank"&gt;https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 03 Jul 2024 15:36:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Steps-to-connect-a-microcontroller-to-imx8mp-using-a-usb-cdc/m-p/1898477#M225824</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-07-03T15:36:35Z</dc:date>
    </item>
  </channel>
</rss>