<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx8mp-debix-model-a.dts syntax error in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-debix-model-a-dts-syntax-error/m-p/1897422#M225739</link>
    <description>&lt;P&gt;it seems MX8MP_IOMUXC_GPIO1_IO14__USB2_OTG_PWR is not defined.&lt;/P&gt;&lt;P&gt;I could only find #define MX8MP_IOMUXC_GPIO1_IO14__USB2_PWR 0x04C 0x2AC 0x000 0x1 0x0&lt;/P&gt;&lt;P&gt;in &lt;A href="https://github.com/nxp-imx/linux-imx/blob/lf-6.6.y/arch/arm64/boot/dts/freescale/imx8mp-pinfunc.h" target="_self"&gt;https://github.com/nxp-imx/linux-imx/blob/lf-6.6.y/arch/arm64/boot/dts/freescale/imx8mp-pinfunc.h&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 02 Jul 2024 10:22:36 GMT</pubDate>
    <dc:creator>qbic</dc:creator>
    <dc:date>2024-07-02T10:22:36Z</dc:date>
    <item>
      <title>imx8mp-debix-model-a.dts syntax error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-debix-model-a-dts-syntax-error/m-p/1897414#M225736</link>
      <description>&lt;P&gt;hello,&lt;/P&gt;&lt;P&gt;I want to build a yocto image for the debix model a board. but when I try to compile linux-imx I get a syntax error for the corresponding .dts file&lt;/P&gt;&lt;P&gt;console output:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;|   DTC     arch/arm64/boot/dts/freescale/imx8mp-debix-model-a.dtb
| Error: /home/querner/debix-sxos/build/tmp/work-shared/imx8mp-debix-model-a/kernel-source/arch/arm64/boot/dts/freescale/imx8mp-debix-model-a.dts:443.4-5 syntax error
| FATAL ERROR: Unable to parse input tree
| make[3]: *** [/home/querner/debix-sxos/build/tmp/work-shared/imx8mp-debix-model-a/kernel-source/scripts/Makefile.lib:419: arch/arm64/boot/dts/freescale/imx8mp-debix-model-a.dtb] Error 1
| make[2]: *** [/home/querner/debix-sxos/build/tmp/work-shared/imx8mp-debix-model-a/kernel-source/scripts/Makefile.build:480: arch/arm64/boot/dts/freescale] Error 2
| make[1]: *** [/home/querner/debix-sxos/build/tmp/work-shared/imx8mp-debix-model-a/kernel-source/Makefile:1384: freescale/imx8mp-debix-model-a.dtb] Error 2
| make: *** [/home/querner/debix-sxos/build/tmp/work-shared/imx8mp-debix-model-a/kernel-source/Makefile:234: __sub-make] Error 2
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
ERROR: Task (/home/querner/debix-sxos/sources/meta-imx/meta-imx-bsp/recipes-kernel/linux/linux-imx_6.6.bb:do_compile) failed with exit code '1'&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;this is the .dts file I want to use: &lt;A href="https://github.com/nxp-imx/linux-imx/blob/lf-6.6.y/arch/arm64/boot/dts/freescale/imx8mp-debix-model-a.dts" target="_self"&gt;https://github.com/nxp-imx/linux-imx/blob/lf-6.6.y/arch/arm64/boot/dts/freescale/imx8mp-debix-model-a.dts&lt;/A&gt;&lt;/P&gt;&lt;P&gt;It says syntax error on line 443.&lt;/P&gt;&lt;P&gt;I am quite new in the yocto eco system, so any help would be appreciated.&lt;/P&gt;&lt;P&gt;Best Regards.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jul 2024 10:05:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-debix-model-a-dts-syntax-error/m-p/1897414#M225736</guid>
      <dc:creator>qbic</dc:creator>
      <dc:date>2024-07-02T10:05:40Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp-debix-model-a.dts syntax error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-debix-model-a-dts-syntax-error/m-p/1897422#M225739</link>
      <description>&lt;P&gt;it seems MX8MP_IOMUXC_GPIO1_IO14__USB2_OTG_PWR is not defined.&lt;/P&gt;&lt;P&gt;I could only find #define MX8MP_IOMUXC_GPIO1_IO14__USB2_PWR 0x04C 0x2AC 0x000 0x1 0x0&lt;/P&gt;&lt;P&gt;in &lt;A href="https://github.com/nxp-imx/linux-imx/blob/lf-6.6.y/arch/arm64/boot/dts/freescale/imx8mp-pinfunc.h" target="_self"&gt;https://github.com/nxp-imx/linux-imx/blob/lf-6.6.y/arch/arm64/boot/dts/freescale/imx8mp-pinfunc.h&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jul 2024 10:22:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-debix-model-a-dts-syntax-error/m-p/1897422#M225739</guid>
      <dc:creator>qbic</dc:creator>
      <dc:date>2024-07-02T10:22:36Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp-debix-model-a.dts syntax error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-debix-model-a-dts-syntax-error/m-p/1897631#M225761</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/235796"&gt;@qbic&lt;/a&gt;!&lt;/P&gt;
&lt;P&gt;Thank you for contacting NXP Support!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The problem could be that you are using our BSP for that board and our BSP is only based for our boards.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I recommend to check the DEBIX documentation because they should proportionate to their BSP for their board.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://debix.io/Document/manual/id/1.html" target="_blank"&gt;https://debix.io/Document/manual/id/1.html&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Sorry for the mistake!&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards!&lt;/P&gt;
&lt;P&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jul 2024 16:07:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-debix-model-a-dts-syntax-error/m-p/1897631#M225761</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2024-07-02T16:07:20Z</dc:date>
    </item>
  </channel>
</rss>