<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MCUXpresso freezes when we debug multicore code.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MCUXpresso-freezes-when-we-debug-multicore-code/m-p/1897134#M225703</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Below are the OS specifications which i am using&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Edition Windows 11 Home Single Language&lt;BR /&gt;Version 23H2&lt;BR /&gt;Installed on ‎20-‎05-‎2023&lt;BR /&gt;OS build 22631.3810&lt;BR /&gt;Experience Windows Feature Experience Pack 1000.22700.1020.0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have already referred the above application note but still facing the same issue.&lt;/P&gt;&lt;P&gt;Also we are using the default configurations of the EVK hardware.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you please share your CPU and OS configurations?&lt;/P&gt;</description>
    <pubDate>Tue, 02 Jul 2024 04:59:23 GMT</pubDate>
    <dc:creator>techexplorer_139</dc:creator>
    <dc:date>2024-07-02T04:59:23Z</dc:date>
    <item>
      <title>MCUXpresso freezes when we debug multicore code.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCUXpresso-freezes-when-we-debug-multicore-code/m-p/1894114#M225482</link>
      <description>&lt;P&gt;&lt;SPAN&gt;We are working on IMX RT 1170 dev kit. We want to debug sdk example code for multicore. We are facing issue with MCUXpresso i.e. when we start debug for the first time it will work properly. Now when we terminate all sessions and restart debug the IDE freezes and we need to forcefully close from task manager. We found the temporary solution i.e. we need to delete Debug folder. Also we tried to delete the metadata and also we made new workspaces, but still same issue is faced.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Please provide the permanent solution and the actual reason if anyone is facing the same.&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jun 2024 07:08:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCUXpresso-freezes-when-we-debug-multicore-code/m-p/1894114#M225482</guid>
      <dc:creator>techexplorer_139</dc:creator>
      <dc:date>2024-06-26T07:08:32Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso freezes when we debug multicore code.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCUXpresso-freezes-when-we-debug-multicore-code/m-p/1894666#M225523</link>
      <description>&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;" lang="es-MX"&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/235526"&gt;@techexplorer_139&lt;/a&gt;&amp;nbsp;,&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;In order to support you better, could you please provide me the next information when you presented the error?&lt;/FONT&gt;&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;-SDK example that you cannot debug.&lt;/FONT&gt;&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;-SDK version.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;-MCUXpresso version.&lt;/FONT&gt;&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;BR,&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;Habib.&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jun 2024 20:31:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCUXpresso-freezes-when-we-debug-multicore-code/m-p/1894666#M225523</guid>
      <dc:creator>Habib_MS</dc:creator>
      <dc:date>2024-06-26T20:31:33Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso freezes when we debug multicore code.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCUXpresso-freezes-when-we-debug-multicore-code/m-p/1894835#M225533</link>
      <description>&lt;P&gt;SDK Example:&amp;nbsp;evkbmimxrt1170_hello_world_cm7 linked to&amp;nbsp;evkbmimxrt1170_hello_world_cm4&lt;/P&gt;&lt;P&gt;SDK Version: 2.15.100 (831 2024-04-26)&lt;/P&gt;&lt;P&gt;MCUXpresso IDE v11.9.0 [Build 2144] [2024-01-05]&lt;/P&gt;</description>
      <pubDate>Thu, 27 Jun 2024 04:15:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCUXpresso-freezes-when-we-debug-multicore-code/m-p/1894835#M225533</guid>
      <dc:creator>techexplorer_139</dc:creator>
      <dc:date>2024-06-27T04:15:43Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso freezes when we debug multicore code.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCUXpresso-freezes-when-we-debug-multicore-code/m-p/1896054#M225628</link>
      <description>&lt;P&gt;Hello again &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/235526"&gt;@techexplorer_139&lt;/a&gt;,&lt;BR /&gt;Corroborating the example in RT1170EVKB, whit the same SDK and MCUxpresso version.&amp;nbsp; I did not see any issue respect to debug (I can debug constantly).&lt;/P&gt;
&lt;P&gt;In order to support you better, can you provide me which OS are you currently using?&lt;/P&gt;
&lt;P&gt;In the other hand. In order to try an pinpoint if the issue is in the configuration of the IDE, can you create a workspace in the root directory? It is advisable to install MCUxpresso in the root directory because long paths or special characters may produce issues with the workspace.&lt;/P&gt;
&lt;P&gt;Respect with the multicore, this &lt;A href="https://www.nxp.com/docs/en/application-note/AN13264.pdf" target="_blank"&gt;application note&lt;/A&gt; could help you, inside has a section about how debug examples of multicores which is called "Dual-core debug in different tool chain".&lt;/P&gt;
&lt;P&gt;Also, if you experience any issue, do not hesitate to let me know.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Habib.&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jun 2024 17:28:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCUXpresso-freezes-when-we-debug-multicore-code/m-p/1896054#M225628</guid>
      <dc:creator>Habib_MS</dc:creator>
      <dc:date>2024-06-28T17:28:09Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso freezes when we debug multicore code.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCUXpresso-freezes-when-we-debug-multicore-code/m-p/1897134#M225703</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Below are the OS specifications which i am using&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Edition Windows 11 Home Single Language&lt;BR /&gt;Version 23H2&lt;BR /&gt;Installed on ‎20-‎05-‎2023&lt;BR /&gt;OS build 22631.3810&lt;BR /&gt;Experience Windows Feature Experience Pack 1000.22700.1020.0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have already referred the above application note but still facing the same issue.&lt;/P&gt;&lt;P&gt;Also we are using the default configurations of the EVK hardware.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you please share your CPU and OS configurations?&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jul 2024 04:59:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCUXpresso-freezes-when-we-debug-multicore-code/m-p/1897134#M225703</guid>
      <dc:creator>techexplorer_139</dc:creator>
      <dc:date>2024-07-02T04:59:23Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso freezes when we debug multicore code.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCUXpresso-freezes-when-we-debug-multicore-code/m-p/1899805#M225904</link>
      <description>&lt;P&gt;Hello again &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/235526"&gt;@techexplorer_139&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The objective of asking about your OS was to confirm if you are currently using the same OS as me. Which you are.&lt;/P&gt;
&lt;P&gt;Could you confirm if you installed MCUxpresso on the root directory or you tried to change the installation location?&lt;/P&gt;
&lt;P&gt;If is the case, can you install the newest version (11.9.1) of MCUxpresso with the recommendation that I provided you? this in order to try if this solves the issue.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;Also, can you provide me the steps that you follow about terminate a debug session?&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Habib.&lt;/P&gt;</description>
      <pubDate>Thu, 04 Jul 2024 22:52:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCUXpresso-freezes-when-we-debug-multicore-code/m-p/1899805#M225904</guid>
      <dc:creator>Habib_MS</dc:creator>
      <dc:date>2024-07-04T22:52:12Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso freezes when we debug multicore code.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCUXpresso-freezes-when-we-debug-multicore-code/m-p/2024061#M232784</link>
      <description>&lt;P&gt;I have the same issue while debugging multi-core projects sometimes.&lt;/P&gt;&lt;P&gt;The tool launches the master core (CM7) debug session successfully, but sometimes when it tries to launch the slave core debug session, it freezes on the middle of process (about 82%). In this case the mcuXpresso is freezed and needs to be force-closed.&lt;/P&gt;</description>
      <pubDate>Wed, 08 Jan 2025 12:44:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCUXpresso-freezes-when-we-debug-multicore-code/m-p/2024061#M232784</guid>
      <dc:creator>alanreal</dc:creator>
      <dc:date>2025-01-08T12:44:10Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso freezes when we debug multicore code.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCUXpresso-freezes-when-we-debug-multicore-code/m-p/2025421#M232852</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We close the debug sessions using the terminate all debug sessions button on menu bar. Is there any special point about it?&lt;/P&gt;</description>
      <pubDate>Fri, 10 Jan 2025 04:00:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCUXpresso-freezes-when-we-debug-multicore-code/m-p/2025421#M232852</guid>
      <dc:creator>alanreal</dc:creator>
      <dc:date>2025-01-10T04:00:05Z</dc:date>
    </item>
  </channel>
</rss>