<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックImplementing Runtime Validation for Custom Application on I.MX6DL Linux Platform</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Implementing-Runtime-Validation-for-Custom-Application-on-I/m-p/1895674#M225602</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am planning to run Linux on the I.MX6DL platform and add my own application. For security reasons, I want to implement a validation mechanism: the application will perform a verification during runtime. If the verification succeeds, the application will run normally; if it fails, the application will not proceed further. Could anyone suggest a good approach to achieve this?&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;Best wish!&lt;/P&gt;</description>
    <pubDate>Fri, 28 Jun 2024 06:19:30 GMT</pubDate>
    <dc:creator>hank2024</dc:creator>
    <dc:date>2024-06-28T06:19:30Z</dc:date>
    <item>
      <title>Implementing Runtime Validation for Custom Application on I.MX6DL Linux Platform</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Implementing-Runtime-Validation-for-Custom-Application-on-I/m-p/1895674#M225602</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am planning to run Linux on the I.MX6DL platform and add my own application. For security reasons, I want to implement a validation mechanism: the application will perform a verification during runtime. If the verification succeeds, the application will run normally; if it fails, the application will not proceed further. Could anyone suggest a good approach to achieve this?&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;Best wish!&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jun 2024 06:19:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Implementing-Runtime-Validation-for-Custom-Application-on-I/m-p/1895674#M225602</guid>
      <dc:creator>hank2024</dc:creator>
      <dc:date>2024-06-28T06:19:30Z</dc:date>
    </item>
    <item>
      <title>Re: Implementing Runtime Validation for Custom Application on I.MX6DL Linux Platform</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Implementing-Runtime-Validation-for-Custom-Application-on-I/m-p/1899144#M225863</link>
      <description>&lt;P&gt;Hope this can be helpful for you, such as &lt;A href="https://www.kernel.org/doc/html/v5.16/filesystems/fsverity.html" target="_blank"&gt;fs-verity: read-only file-based authenticity protection — The Linux Kernel documentation&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Thu, 04 Jul 2024 05:45:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Implementing-Runtime-Validation-for-Custom-Application-on-I/m-p/1899144#M225863</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2024-07-04T05:45:28Z</dc:date>
    </item>
  </channel>
</rss>