<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックlpddr4 configurations</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/lpddr4-configurations/m-p/1895130#M225562</link>
    <description>&lt;P&gt;Hi NXP team,&lt;BR /&gt;&lt;BR /&gt;I am working on i.MX93 EVK as it contains LPDDR4x ram so my question is if the hardware changed to LPDDR4 ram then will it affect the imx93-lpm.c driver, because I have seen some ddr dependency, is there in the driver.&lt;BR /&gt;&lt;BR /&gt;if so, then what configurations do we need to do for lpddr4 memory so that imx93-lpm.c driver works fine?&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;Shubham&lt;/P&gt;</description>
    <pubDate>Thu, 27 Jun 2024 11:24:46 GMT</pubDate>
    <dc:creator>sbmd_1234</dc:creator>
    <dc:date>2024-06-27T11:24:46Z</dc:date>
    <item>
      <title>lpddr4 configurations</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/lpddr4-configurations/m-p/1895130#M225562</link>
      <description>&lt;P&gt;Hi NXP team,&lt;BR /&gt;&lt;BR /&gt;I am working on i.MX93 EVK as it contains LPDDR4x ram so my question is if the hardware changed to LPDDR4 ram then will it affect the imx93-lpm.c driver, because I have seen some ddr dependency, is there in the driver.&lt;BR /&gt;&lt;BR /&gt;if so, then what configurations do we need to do for lpddr4 memory so that imx93-lpm.c driver works fine?&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;Shubham&lt;/P&gt;</description>
      <pubDate>Thu, 27 Jun 2024 11:24:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/lpddr4-configurations/m-p/1895130#M225562</guid>
      <dc:creator>sbmd_1234</dc:creator>
      <dc:date>2024-06-27T11:24:46Z</dc:date>
    </item>
    <item>
      <title>Re: lpddr4 configurations</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/lpddr4-configurations/m-p/1896080#M225631</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I do not see anything that may block this on the driver, unless I missed something.&lt;BR /&gt;&lt;BR /&gt;Please note that this low power control module provides four interface to control the system wide OD/ND mode swithcing with DDR frequency scaling by HWFFC, DDR scaling down to a frequency &amp;lt; half of the full speed, DDR auto clock gating enable &amp;amp; auto clock gating idl strap to fine tuning the performance &amp;amp; power based on the user case.&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jun 2024 18:45:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/lpddr4-configurations/m-p/1896080#M225631</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2024-06-28T18:45:17Z</dc:date>
    </item>
  </channel>
</rss>