<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx8mp jailhouse can not boot another kernel,boot kernel fail</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-jailhouse-can-not-boot-another-kernel-boot-kernel-fail/m-p/1894978#M225546</link>
    <description>&lt;P&gt;[root@jailhouse]#insmod jailhouse.ko&lt;BR /&gt;[root@jailhouse]#cat fdf_[ 64.477482] cfg80211: failed to load regulatory.db&lt;BR /&gt;kernel.sh&lt;BR /&gt;#!/bin/bash&lt;BR /&gt;./jailhouse enable ./imx8mp.cell&lt;BR /&gt;./jailhouse cell linux ./imx8mp-linux-demo.cell /run/media/mmcblk2p1/Image -d /r un/media/mmcblk2p1/imx8mp-evk-inmate.dtb -c "clk_ignore_unused console=ttymxc1,1 15200 earlycon=ec_imx6q,0x30860000,115200 root=/dev/mmcblk2p2 rootwait rw"&lt;/P&gt;&lt;P&gt;[root@jailhouse]#cat fdf_kernel.sh&lt;BR /&gt;#!/bin/bash&lt;BR /&gt;./jailhouse enable ./imx8mp.cell&lt;BR /&gt;./jailhouse cell linux ./imx8mp-linux-demo.cell /run/media/mmcblk2p1/Image -d /r un/media/mmcblk2p1/imx8mp-evk-inmate.dtb -c "clk_ignore_unused console=ttymxc1,1 15200 earlycon=ec_imx6q,0x30860000,115200 root=/dev/mmcblk2p2 rootwait rw"&lt;/P&gt;&lt;P&gt;[root@jailhouse]#./fdf_kernel.sh&lt;/P&gt;&lt;P&gt;Initializing Jailhouse hypervisor v0.12 (334-gd9fffb80) on CPU 1&lt;BR /&gt;Code location: 0x0000ffffc0200800&lt;BR /&gt;Page pool usage after early setup: mem 39/993, remap 0/131072&lt;BR /&gt;Initializing processors:&lt;BR /&gt;CPU 1... OK&lt;BR /&gt;CPU 3... OK&lt;BR /&gt;CPU 2... OK&lt;BR /&gt;CPU 0... OK&lt;BR /&gt;Initializing unit: irqchip&lt;BR /&gt;Initializing unit: ARM SMMU v3&lt;BR /&gt;Initializing unit: ARM SMMU&lt;BR /&gt;Initializing unit: PVU IOMMU&lt;BR /&gt;Initializing unit: PCI&lt;BR /&gt;Adding virtual PCI device 00:02.0 to cell "imx8mp"&lt;BR /&gt;Adding virtual PCI device 00:03.0 to cell "imx8mp"&lt;BR /&gt;Adding virtual PCI device 00:00.0 to cell "imx8mp"&lt;BR /&gt;Adding virtual PCI device 00:01.0 to cell "imx8mp"&lt;BR /&gt;Page pool usage after late setup: mem 69/993, remap 144/131072&lt;BR /&gt;Activating hypervisor&lt;BR /&gt;[ 87.808445] pci-host-generic fd700000.pci: host bridge /pci@0 ranges:&lt;BR /&gt;[ 87.814951] pci-host-generic fd700000.pci: MEM 0x00fd800000..0x00fd807ff f -&amp;gt; 0x00fd800000&lt;BR /&gt;[ 87.823628] pci-host-generic fd700000.pci: ECAM at [mem 0xfd700000-0xfd7fffff ] for [bus 00]&lt;BR /&gt;[ 87.832078] pci-host-generic fd700000.pci: PCI host bridge to bus 0002:00&lt;BR /&gt;[ 87.838898] pci_bus 0002:00: root bus resource [bus 00]&lt;BR /&gt;[ 87.844143] pci_bus 0002:00: root bus resource [mem 0xfd800000-0xfd807fff]&lt;BR /&gt;[ 87.851058] pci 0002:00:00.0: [110a:4106] type 00 class 0xff0000&lt;BR /&gt;[ 87.857095] pci 0002:00:00.0: reg 0x10: [mem 0x00000000-0x00000fff]&lt;BR /&gt;[ 87.863735] pci 0002:00:01.0: [110a:4106] type 00 class 0xff0001&lt;BR /&gt;[ 87.869776] pci 0002:00:01.0: reg 0x10: [mem 0x00000000-0x00000fff]&lt;BR /&gt;[ 87.876348] pci 0002:00:02.0: [110a:4106] type 00 class 0xffc002&lt;BR /&gt;[ 87.882382] pci 0002:00:02.0: reg 0x10: [mem 0x00000000-0x00000fff]&lt;BR /&gt;[ 87.888910] pci 0002:00:03.0: [110a:4106] type 00 class 0xffc003&lt;BR /&gt;[ 87.894943] pci 0002:00:03.0: reg 0x10: [mem 0x00000000-0x00000fff]&lt;BR /&gt;[ 87.903413] pci 0002:00:00.0: BAR 0: assigned [mem 0xfd800000-0xfd800fff]&lt;BR /&gt;[ 87.910223] pci 0002:00:01.0: BAR 0: assigned [mem 0xfd801000-0xfd801fff]&lt;BR /&gt;[ 87.917025] pci 0002:00:02.0: BAR 0: assigned [mem 0xfd802000-0xfd802fff]&lt;BR /&gt;[ 87.923830] pci 0002:00:03.0: BAR 0: assigned [mem 0xfd803000-0xfd803fff]&lt;BR /&gt;[ 87.930844] uio_ivshmem 0002:00:00.0: enabling device (0000 -&amp;gt; 0002)&lt;BR /&gt;[ 87.937267] uio_ivshmem 0002:00:00.0: state_table at 0x00000000fd9f0000, size 0x0000000000001000&lt;BR /&gt;[ 87.946070] uio_ivshmem 0002:00:00.0: rw_section at 0x00000000fd9f1000, size 0x0000000000009000&lt;BR /&gt;[ 87.954787] uio_ivshmem 0002:00:00.0: input_sections at 0x00000000fd9fa000, s ize 0x0000000000006000&lt;BR /&gt;[ 87.963852] uio_ivshmem 0002:00:00.0: output_section at 0x00000000fd9fa000, s ize 0x0000000000002000&lt;BR /&gt;[ 87.973376] ivshmem-net 0002:00:01.0: enabling device (0000 -&amp;gt; 0002)&lt;BR /&gt;[ 87.979836] ivshmem-net 0002:00:01.0: TX memory at 0x00000000fda01000, size 0 x000000000007f000&lt;BR /&gt;[ 87.988462] ivshmem-net 0002:00:01.0: RX memory at 0x00000000fda80000, size 0 x000000000007f000&lt;BR /&gt;[ 87.997779] The Jailhouse is opening.&lt;BR /&gt;[ 88.928879] config size=1164,cell_params.config_address=0x00000000d9ed0850&lt;BR /&gt;[ 88.935795] jailhouse_cmd_cell_create,193&lt;BR /&gt;[ 88.939813] jailhouse_cmd_cell_create,204&lt;BR /&gt;[ 88.943828] jailhouse_cmd_cell_create,209&lt;BR /&gt;[ 88.947843] jailhouse_cmd_cell_create,216&lt;BR /&gt;[ 88.989480] psci: CPU2 killed (polled 0 ms)&lt;BR /&gt;[ 89.045455] psci: CPU3 killed (polled 0 ms)&lt;BR /&gt;Adding virtual PCI device 00:02.0 to cell "linux-inmate-demo"&lt;BR /&gt;Shared memory connection established, peer cells:&lt;BR /&gt;"imx8mp"&lt;BR /&gt;Adding virtual PCI device 00:03.0 to cell "linux-inmate-demo"&lt;BR /&gt;Shared memory connection established, peer cells:&lt;BR /&gt;"imx8mp"&lt;BR /&gt;Adding virtual PCI device 00:00.0 to cell "linux-inmate-demo"&lt;BR /&gt;Shared memory connection established, peer cells:&lt;BR /&gt;"imx8mp"&lt;BR /&gt;Adding virtual PCI device 00:01.0 to cell "linux-inmate-demo"&lt;BR /&gt;Shared memory connection established, peer cells:&lt;BR /&gt;"imx8mp"&lt;BR /&gt;Created cell "linux-inmate-demo"&lt;BR /&gt;Page pool usage after cell creation: mem 86/993, remap 144/131072&lt;BR /&gt;[ 89.126900] Created Jailhouse cell "linux-inmate-demo"&lt;BR /&gt;Unhandled data read at 0x30b600c0(4)&lt;/P&gt;&lt;P&gt;FATAL: unhandled trap (exception class 0x24)&lt;BR /&gt;Cell state before exception:&lt;BR /&gt;pc: ffff800008d464b4 lr: ffff800008d467d8 spsr: 20000005 EL1&lt;BR /&gt;sp: ffff80000a4238c0 elr: ffff800008d464b4 esr: 24 1 1810007&lt;BR /&gt;x0: ffff000004c80580 x1: ffff80000a7c00c0 x2: 0000000000000001&lt;BR /&gt;x3: 0000000000000000 x4: 0000000000000000 x5: ffff0000046a2a00&lt;BR /&gt;x6: ffff0000046a2a00 x7: 0000000000000000 x8: fefefefefefefeff&lt;BR /&gt;x9: ffff00000467b574 x10: 0000000000000990 x11: 0000000000000000&lt;BR /&gt;x12: 0000000000000001 x13: 0000000000000001 x14: 0000000000000260&lt;BR /&gt;x15: 00000003d495f450 x16: 0000000000000fcc x17: 0000000000000000&lt;BR /&gt;x18: 0000000000000001 x19: 0000000000000000 x20: ffff000004c80a40&lt;BR /&gt;x21: 000000000bebc200 x22: 0000000000000002 x23: 0000000000000000&lt;BR /&gt;x24: ffff000004c80580 x25: 0000000017d78400 x26: ffff000004419d38&lt;BR /&gt;x27: 0000000000000000 x28: 0000000000000000 x29: ffff80000a4238c0&lt;/P&gt;&lt;P&gt;Parking CPU 0 (Cell: "imx8mp")&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 27 Jun 2024 08:12:33 GMT</pubDate>
    <dc:creator>jimmyhua</dc:creator>
    <dc:date>2024-06-27T08:12:33Z</dc:date>
    <item>
      <title>imx8mp jailhouse can not boot another kernel,boot kernel fail</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-jailhouse-can-not-boot-another-kernel-boot-kernel-fail/m-p/1894978#M225546</link>
      <description>&lt;P&gt;[root@jailhouse]#insmod jailhouse.ko&lt;BR /&gt;[root@jailhouse]#cat fdf_[ 64.477482] cfg80211: failed to load regulatory.db&lt;BR /&gt;kernel.sh&lt;BR /&gt;#!/bin/bash&lt;BR /&gt;./jailhouse enable ./imx8mp.cell&lt;BR /&gt;./jailhouse cell linux ./imx8mp-linux-demo.cell /run/media/mmcblk2p1/Image -d /r un/media/mmcblk2p1/imx8mp-evk-inmate.dtb -c "clk_ignore_unused console=ttymxc1,1 15200 earlycon=ec_imx6q,0x30860000,115200 root=/dev/mmcblk2p2 rootwait rw"&lt;/P&gt;&lt;P&gt;[root@jailhouse]#cat fdf_kernel.sh&lt;BR /&gt;#!/bin/bash&lt;BR /&gt;./jailhouse enable ./imx8mp.cell&lt;BR /&gt;./jailhouse cell linux ./imx8mp-linux-demo.cell /run/media/mmcblk2p1/Image -d /r un/media/mmcblk2p1/imx8mp-evk-inmate.dtb -c "clk_ignore_unused console=ttymxc1,1 15200 earlycon=ec_imx6q,0x30860000,115200 root=/dev/mmcblk2p2 rootwait rw"&lt;/P&gt;&lt;P&gt;[root@jailhouse]#./fdf_kernel.sh&lt;/P&gt;&lt;P&gt;Initializing Jailhouse hypervisor v0.12 (334-gd9fffb80) on CPU 1&lt;BR /&gt;Code location: 0x0000ffffc0200800&lt;BR /&gt;Page pool usage after early setup: mem 39/993, remap 0/131072&lt;BR /&gt;Initializing processors:&lt;BR /&gt;CPU 1... OK&lt;BR /&gt;CPU 3... OK&lt;BR /&gt;CPU 2... OK&lt;BR /&gt;CPU 0... OK&lt;BR /&gt;Initializing unit: irqchip&lt;BR /&gt;Initializing unit: ARM SMMU v3&lt;BR /&gt;Initializing unit: ARM SMMU&lt;BR /&gt;Initializing unit: PVU IOMMU&lt;BR /&gt;Initializing unit: PCI&lt;BR /&gt;Adding virtual PCI device 00:02.0 to cell "imx8mp"&lt;BR /&gt;Adding virtual PCI device 00:03.0 to cell "imx8mp"&lt;BR /&gt;Adding virtual PCI device 00:00.0 to cell "imx8mp"&lt;BR /&gt;Adding virtual PCI device 00:01.0 to cell "imx8mp"&lt;BR /&gt;Page pool usage after late setup: mem 69/993, remap 144/131072&lt;BR /&gt;Activating hypervisor&lt;BR /&gt;[ 87.808445] pci-host-generic fd700000.pci: host bridge /pci@0 ranges:&lt;BR /&gt;[ 87.814951] pci-host-generic fd700000.pci: MEM 0x00fd800000..0x00fd807ff f -&amp;gt; 0x00fd800000&lt;BR /&gt;[ 87.823628] pci-host-generic fd700000.pci: ECAM at [mem 0xfd700000-0xfd7fffff ] for [bus 00]&lt;BR /&gt;[ 87.832078] pci-host-generic fd700000.pci: PCI host bridge to bus 0002:00&lt;BR /&gt;[ 87.838898] pci_bus 0002:00: root bus resource [bus 00]&lt;BR /&gt;[ 87.844143] pci_bus 0002:00: root bus resource [mem 0xfd800000-0xfd807fff]&lt;BR /&gt;[ 87.851058] pci 0002:00:00.0: [110a:4106] type 00 class 0xff0000&lt;BR /&gt;[ 87.857095] pci 0002:00:00.0: reg 0x10: [mem 0x00000000-0x00000fff]&lt;BR /&gt;[ 87.863735] pci 0002:00:01.0: [110a:4106] type 00 class 0xff0001&lt;BR /&gt;[ 87.869776] pci 0002:00:01.0: reg 0x10: [mem 0x00000000-0x00000fff]&lt;BR /&gt;[ 87.876348] pci 0002:00:02.0: [110a:4106] type 00 class 0xffc002&lt;BR /&gt;[ 87.882382] pci 0002:00:02.0: reg 0x10: [mem 0x00000000-0x00000fff]&lt;BR /&gt;[ 87.888910] pci 0002:00:03.0: [110a:4106] type 00 class 0xffc003&lt;BR /&gt;[ 87.894943] pci 0002:00:03.0: reg 0x10: [mem 0x00000000-0x00000fff]&lt;BR /&gt;[ 87.903413] pci 0002:00:00.0: BAR 0: assigned [mem 0xfd800000-0xfd800fff]&lt;BR /&gt;[ 87.910223] pci 0002:00:01.0: BAR 0: assigned [mem 0xfd801000-0xfd801fff]&lt;BR /&gt;[ 87.917025] pci 0002:00:02.0: BAR 0: assigned [mem 0xfd802000-0xfd802fff]&lt;BR /&gt;[ 87.923830] pci 0002:00:03.0: BAR 0: assigned [mem 0xfd803000-0xfd803fff]&lt;BR /&gt;[ 87.930844] uio_ivshmem 0002:00:00.0: enabling device (0000 -&amp;gt; 0002)&lt;BR /&gt;[ 87.937267] uio_ivshmem 0002:00:00.0: state_table at 0x00000000fd9f0000, size 0x0000000000001000&lt;BR /&gt;[ 87.946070] uio_ivshmem 0002:00:00.0: rw_section at 0x00000000fd9f1000, size 0x0000000000009000&lt;BR /&gt;[ 87.954787] uio_ivshmem 0002:00:00.0: input_sections at 0x00000000fd9fa000, s ize 0x0000000000006000&lt;BR /&gt;[ 87.963852] uio_ivshmem 0002:00:00.0: output_section at 0x00000000fd9fa000, s ize 0x0000000000002000&lt;BR /&gt;[ 87.973376] ivshmem-net 0002:00:01.0: enabling device (0000 -&amp;gt; 0002)&lt;BR /&gt;[ 87.979836] ivshmem-net 0002:00:01.0: TX memory at 0x00000000fda01000, size 0 x000000000007f000&lt;BR /&gt;[ 87.988462] ivshmem-net 0002:00:01.0: RX memory at 0x00000000fda80000, size 0 x000000000007f000&lt;BR /&gt;[ 87.997779] The Jailhouse is opening.&lt;BR /&gt;[ 88.928879] config size=1164,cell_params.config_address=0x00000000d9ed0850&lt;BR /&gt;[ 88.935795] jailhouse_cmd_cell_create,193&lt;BR /&gt;[ 88.939813] jailhouse_cmd_cell_create,204&lt;BR /&gt;[ 88.943828] jailhouse_cmd_cell_create,209&lt;BR /&gt;[ 88.947843] jailhouse_cmd_cell_create,216&lt;BR /&gt;[ 88.989480] psci: CPU2 killed (polled 0 ms)&lt;BR /&gt;[ 89.045455] psci: CPU3 killed (polled 0 ms)&lt;BR /&gt;Adding virtual PCI device 00:02.0 to cell "linux-inmate-demo"&lt;BR /&gt;Shared memory connection established, peer cells:&lt;BR /&gt;"imx8mp"&lt;BR /&gt;Adding virtual PCI device 00:03.0 to cell "linux-inmate-demo"&lt;BR /&gt;Shared memory connection established, peer cells:&lt;BR /&gt;"imx8mp"&lt;BR /&gt;Adding virtual PCI device 00:00.0 to cell "linux-inmate-demo"&lt;BR /&gt;Shared memory connection established, peer cells:&lt;BR /&gt;"imx8mp"&lt;BR /&gt;Adding virtual PCI device 00:01.0 to cell "linux-inmate-demo"&lt;BR /&gt;Shared memory connection established, peer cells:&lt;BR /&gt;"imx8mp"&lt;BR /&gt;Created cell "linux-inmate-demo"&lt;BR /&gt;Page pool usage after cell creation: mem 86/993, remap 144/131072&lt;BR /&gt;[ 89.126900] Created Jailhouse cell "linux-inmate-demo"&lt;BR /&gt;Unhandled data read at 0x30b600c0(4)&lt;/P&gt;&lt;P&gt;FATAL: unhandled trap (exception class 0x24)&lt;BR /&gt;Cell state before exception:&lt;BR /&gt;pc: ffff800008d464b4 lr: ffff800008d467d8 spsr: 20000005 EL1&lt;BR /&gt;sp: ffff80000a4238c0 elr: ffff800008d464b4 esr: 24 1 1810007&lt;BR /&gt;x0: ffff000004c80580 x1: ffff80000a7c00c0 x2: 0000000000000001&lt;BR /&gt;x3: 0000000000000000 x4: 0000000000000000 x5: ffff0000046a2a00&lt;BR /&gt;x6: ffff0000046a2a00 x7: 0000000000000000 x8: fefefefefefefeff&lt;BR /&gt;x9: ffff00000467b574 x10: 0000000000000990 x11: 0000000000000000&lt;BR /&gt;x12: 0000000000000001 x13: 0000000000000001 x14: 0000000000000260&lt;BR /&gt;x15: 00000003d495f450 x16: 0000000000000fcc x17: 0000000000000000&lt;BR /&gt;x18: 0000000000000001 x19: 0000000000000000 x20: ffff000004c80a40&lt;BR /&gt;x21: 000000000bebc200 x22: 0000000000000002 x23: 0000000000000000&lt;BR /&gt;x24: ffff000004c80580 x25: 0000000017d78400 x26: ffff000004419d38&lt;BR /&gt;x27: 0000000000000000 x28: 0000000000000000 x29: ffff80000a4238c0&lt;/P&gt;&lt;P&gt;Parking CPU 0 (Cell: "imx8mp")&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 27 Jun 2024 08:12:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-jailhouse-can-not-boot-another-kernel-boot-kernel-fail/m-p/1894978#M225546</guid>
      <dc:creator>jimmyhua</dc:creator>
      <dc:date>2024-06-27T08:12:33Z</dc:date>
    </item>
  </channel>
</rss>