<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックmix93evk matter</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/mix93evk-matter/m-p/1893517#M225434</link>
    <description>&lt;PRE&gt;Hi NXP&lt;BR /&gt;&lt;SPAN class=""&gt;Executing the following command failed.&lt;/SPAN&gt;&lt;SPAN class=""&gt;What to do?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;MACHINE=imx93evk-matter DISTRO=fsl-imx-xwayland source sources/meta-matter/tools/imx-matter-setup.sh bld-xwayland-imx93&lt;/PRE&gt;&lt;PRE&gt; bitbake imx-image-multimedia&lt;/PRE&gt;&lt;P&gt;ERROR: linux-imx-6.1.22+gitAUTOINC+66e442bc7f-r0 do_patch: Could not apply patches for imx93evk-matter.&lt;BR /&gt;ERROR: linux-imx-6.1.22+gitAUTOINC+66e442bc7f-r0 do_patch: Patch failures can be resolved in the linux source directory /home/ubuntu/nxp8ulp/bld-xwayland-imx93/tmp/work/imx93evk_matter-poky-linux/linux-imx/6.1.22+gitAUTOINC+66e442bc7f-r0/git)&lt;BR /&gt;ERROR: linux-imx-6.1.22+gitAUTOINC+66e442bc7f-r0 do_patch: ExecutionError('/home/ubuntu/nxp8ulp/bld-xwayland-imx93/tmp/work/imx93evk_matter-poky-linux/linux-imx/6.1.22+gitAUTOINC+66e442bc7f-r0/temp/run.do_patch.44034', 1, None, None)&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/ubuntu/nxp8ulp/bld-xwayland-imx93/tmp/work/imx93evk_matter-poky-linux/linux-imx/6.1.22+gitAUTOINC+66e442bc7f-r0/temp/log.do_patch.44034&lt;BR /&gt;Log data follows:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 25 Jun 2024 09:31:59 GMT</pubDate>
    <dc:creator>tgt007</dc:creator>
    <dc:date>2024-06-25T09:31:59Z</dc:date>
    <item>
      <title>mix93evk matter</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mix93evk-matter/m-p/1893517#M225434</link>
      <description>&lt;PRE&gt;Hi NXP&lt;BR /&gt;&lt;SPAN class=""&gt;Executing the following command failed.&lt;/SPAN&gt;&lt;SPAN class=""&gt;What to do?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;MACHINE=imx93evk-matter DISTRO=fsl-imx-xwayland source sources/meta-matter/tools/imx-matter-setup.sh bld-xwayland-imx93&lt;/PRE&gt;&lt;PRE&gt; bitbake imx-image-multimedia&lt;/PRE&gt;&lt;P&gt;ERROR: linux-imx-6.1.22+gitAUTOINC+66e442bc7f-r0 do_patch: Could not apply patches for imx93evk-matter.&lt;BR /&gt;ERROR: linux-imx-6.1.22+gitAUTOINC+66e442bc7f-r0 do_patch: Patch failures can be resolved in the linux source directory /home/ubuntu/nxp8ulp/bld-xwayland-imx93/tmp/work/imx93evk_matter-poky-linux/linux-imx/6.1.22+gitAUTOINC+66e442bc7f-r0/git)&lt;BR /&gt;ERROR: linux-imx-6.1.22+gitAUTOINC+66e442bc7f-r0 do_patch: ExecutionError('/home/ubuntu/nxp8ulp/bld-xwayland-imx93/tmp/work/imx93evk_matter-poky-linux/linux-imx/6.1.22+gitAUTOINC+66e442bc7f-r0/temp/run.do_patch.44034', 1, None, None)&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/ubuntu/nxp8ulp/bld-xwayland-imx93/tmp/work/imx93evk_matter-poky-linux/linux-imx/6.1.22+gitAUTOINC+66e442bc7f-r0/temp/log.do_patch.44034&lt;BR /&gt;Log data follows:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jun 2024 09:31:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mix93evk-matter/m-p/1893517#M225434</guid>
      <dc:creator>tgt007</dc:creator>
      <dc:date>2024-06-25T09:31:59Z</dc:date>
    </item>
    <item>
      <title>Re: mix93evk matter</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mix93evk-matter/m-p/1895199#M225567</link>
      <description>&lt;P&gt;Hi, &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/230987"&gt;@tgt007&lt;/a&gt;!&lt;/P&gt;
&lt;P&gt;Try to limit the cores and tasks of the Yocto project.&lt;/P&gt;
&lt;P&gt;We recommend using 4 GB of RAM for each core.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you have 16GB of RAM you should use 4 Cores only and you only have to add the next lines to your local.conf of the Yocto Project.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;BB_NUMBER_THREADS = "4"
PARALLEL_MAKE = "-j 4"&lt;/LI-CODE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards!&lt;/P&gt;
&lt;P&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Thu, 27 Jun 2024 13:34:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mix93evk-matter/m-p/1895199#M225567</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2024-06-27T13:34:34Z</dc:date>
    </item>
  </channel>
</rss>