<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX8QXP  2 x 1Gb Ethernet</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-2-x-1Gb-Ethernet/m-p/1891348#M225278</link>
    <description>&lt;P&gt;Dear NXP Team,&lt;/P&gt;&lt;P&gt;We are designing a custom SOM module using the IMX8QXP processor. We require two 1Gb Ethernet ports. According to the pin configuration of the MiMX8QX6AVLFZAC, the ENET interface pins B32 (ENET0_MDIO), D30 (ENET1_MDC), and F28 (ENET0_REFCLK_125M_25M) are shared between ENET0 and ENET1.&lt;/P&gt;&lt;P&gt;Can we connect these three pins to both Ethernet PHY ICs?&lt;/P&gt;&lt;P&gt;Below is the pin config tool image for your reference.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Chethanbg_0-1718878704413.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/285055i8C8FBFD0ABEC2CC7/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Chethanbg_0-1718878704413.png" alt="Chethanbg_0-1718878704413.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Chethanbg_0-1718878704413.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Chethanbg_1-1718878731251.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/285056i1C886FD0D265CAA3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Chethanbg_1-1718878731251.png" alt="Chethanbg_1-1718878731251.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Chethanbg_1-1718878731251.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 20 Jun 2024 10:21:25 GMT</pubDate>
    <dc:creator>Chethanbg</dc:creator>
    <dc:date>2024-06-20T10:21:25Z</dc:date>
    <item>
      <title>IMX8QXP  2 x 1Gb Ethernet</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-2-x-1Gb-Ethernet/m-p/1891348#M225278</link>
      <description>&lt;P&gt;Dear NXP Team,&lt;/P&gt;&lt;P&gt;We are designing a custom SOM module using the IMX8QXP processor. We require two 1Gb Ethernet ports. According to the pin configuration of the MiMX8QX6AVLFZAC, the ENET interface pins B32 (ENET0_MDIO), D30 (ENET1_MDC), and F28 (ENET0_REFCLK_125M_25M) are shared between ENET0 and ENET1.&lt;/P&gt;&lt;P&gt;Can we connect these three pins to both Ethernet PHY ICs?&lt;/P&gt;&lt;P&gt;Below is the pin config tool image for your reference.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Chethanbg_0-1718878704413.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/285055i8C8FBFD0ABEC2CC7/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Chethanbg_0-1718878704413.png" alt="Chethanbg_0-1718878704413.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Chethanbg_0-1718878704413.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Chethanbg_1-1718878731251.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/285056i1C886FD0D265CAA3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Chethanbg_1-1718878731251.png" alt="Chethanbg_1-1718878731251.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Chethanbg_1-1718878731251.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jun 2024 10:21:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-2-x-1Gb-Ethernet/m-p/1891348#M225278</guid>
      <dc:creator>Chethanbg</dc:creator>
      <dc:date>2024-06-20T10:21:25Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QXP  2 x 1Gb Ethernet</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-2-x-1Gb-Ethernet/m-p/1891520#M225299</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Yes, but you have to create the proper driver to work with it since linux BSP and/or android BSP works with one ethernet.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jun 2024 15:36:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-2-x-1Gb-Ethernet/m-p/1891520#M225299</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-06-20T15:36:09Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QXP  2 x 1Gb Ethernet</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-2-x-1Gb-Ethernet/m-p/2013877#M231984</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi,&lt;BR /&gt;In the above topic I am working with chethan.&lt;BR /&gt;&lt;BR /&gt;-&amp;gt;Enet 0 is functional and we are able to ping through it. Here we are able to set IP address automaticlly.&lt;BR /&gt;&lt;BR /&gt;-&amp;gt;Enet 1 is not working, and not able to set IP address automatically, but manually we are able to set.&lt;BR /&gt;&lt;BR /&gt;-&amp;gt; We have also tried to Up the ethernet individually(disabling ethernet 0 in the DTSI file), but&amp;nbsp; ethernet 1 was not functional.&lt;BR /&gt;&lt;BR /&gt;-&amp;gt;Additionally, I am attaching the ethernet section Schematics, Logs and DTSI file in this post.&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Sadeed&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 14 Dec 2024 12:16:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8QXP-2-x-1Gb-Ethernet/m-p/2013877#M231984</guid>
      <dc:creator>Sadeed</dc:creator>
      <dc:date>2024-12-14T12:16:10Z</dc:date>
    </item>
  </channel>
</rss>