<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Difference between MCIMX6 and PCIMX6 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Difference-between-MCIMX6-and-PCIMX6/m-p/1890944#M225251</link>
    <description>&lt;P&gt;For Special Qualification level, is the SC marked at the package body for this type of device?&lt;/P&gt;</description>
    <pubDate>Thu, 20 Jun 2024 01:35:33 GMT</pubDate>
    <dc:creator>brian_21</dc:creator>
    <dc:date>2024-06-20T01:35:33Z</dc:date>
    <item>
      <title>Difference between MCIMX6 and PCIMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Difference-between-MCIMX6-and-PCIMX6/m-p/683608#M105658</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've been developing on the MX6UL EVK with the PCIMX6G2CVM05AA, but am now looking to port to a custom PCB with the MCIMX6G2AVM07AA part on it. Where can I find information on the differences between these parts that I need to be aware of for the port?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Jul 2017 16:28:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Difference-between-MCIMX6-and-PCIMX6/m-p/683608#M105658</guid>
      <dc:creator>danielbujak</dc:creator>
      <dc:date>2017-07-04T16:28:53Z</dc:date>
    </item>
    <item>
      <title>Re: Difference between MCIMX6 and PCIMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Difference-between-MCIMX6-and-PCIMX6/m-p/683609#M105659</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Danielbujak,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The PC in front of the par number refers to the part being a prototype sample. You can see more details on what the part number nomenclature means in figure 1 of the i.MX6UL Datahseet (link below):&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.nxp.com/docs/en/data-sheet/IMX6ULCEC.pdf"&gt;http://www.nxp.com/docs/en/data-sheet/IMX6ULCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Jul 2017 20:48:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Difference-between-MCIMX6-and-PCIMX6/m-p/683609#M105659</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2017-07-04T20:48:45Z</dc:date>
    </item>
    <item>
      <title>Re: Difference between MCIMX6 and PCIMX6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Difference-between-MCIMX6-and-PCIMX6/m-p/1890944#M225251</link>
      <description>&lt;P&gt;For Special Qualification level, is the SC marked at the package body for this type of device?&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jun 2024 01:35:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Difference-between-MCIMX6-and-PCIMX6/m-p/1890944#M225251</guid>
      <dc:creator>brian_21</dc:creator>
      <dc:date>2024-06-20T01:35:33Z</dc:date>
    </item>
  </channel>
</rss>