<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to Run 32 bit application on imx 8m plus in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-Run-32-bit-application-on-imx-8m-plus/m-p/1890342#M225224</link>
    <description>&lt;P&gt;I need to run a 32-bit application on the imx8m plus board but that needs multilib support.While bitbaking, I had an error with the devIL recipe, which I fixed by a method followed by the same issue fixed in the community, after which I received a linker error with imx-gpu-sdk saying that the lIL lib was not found.How can I fix this error?&lt;/P&gt;&lt;P&gt;DemoApp.Util.Graphics.a -lIL DemoFramework/FslDemoHost/Console/libFslDemoHost.Console.a DemoFramework/FslDemoPlatform/Link/libFslDemoPlatform.Link.a DemoFramework/FslDemoPlatform/libFslDemoPlatform.a DemoFramework/FslDemoHost/Base/libFslDemoHost.Base.a DemoFramework/FslDemoApp/Base/libFslDemoApp.Base.a DemoFramework/FslNativeWindow/Base/libFslNativeWindow.Base.a DemoFramework/FslDemoApp/Shared/libFslDemoApp.Shared.a DemoFramework/FslGraphics/libFslGraphics.a DemoFramework/FslDemoService/CpuStats/Impl/libFslDemoService.CpuStats.Impl.a DemoFramework/FslService/Impl/libFslService.Impl.a DemoFramework/FslService/Consumer/libFslService.Consumer.a DemoFramework/FslVersion/libFslVersion.a DemoFramework/FslBase/libFslBase.a -s -lfmt &amp;amp;&amp;amp; :&lt;BR /&gt;| /home/mysticp0004/var-fsl-yocto/build_xwayland/tmp/work/armv8a-mx8mp-fslc-linux/imx-gpu-sdk/6.0.2-r0/recipe-sysroot-native/usr/bin/aarch64-fslc-linux/../../libexec/aarch64-fslc-linux/gcc/aarch64-fslc-linux/11.3.0/ld: cannot find -lIL: No such file or directory&lt;BR /&gt;| collect2: error: ld returned 1 exit status&lt;BR /&gt;| [1450/2889] Building CXX object DemoFramework/FslUtil/Vulkan1_0/UnitTest/Helper/CMakeFiles/FslUtil.Vulkan1_0.UnitTest.Helper.dir/home/mysticp0004/var-fsl-yocto/build_xwayland/tmp/work/armv8a-mx8mp-fslc-linux/imx-gpu-sdk/6.0.2-r0/git/DemoFramework/FslUtil/Vulkan1_0/UnitTest/Helper/source/FslUtil/Vulkan1_0/UnitTest/Helper/Dummy.cpp.o&lt;BR /&gt;| [1451/2889] Building CXX object DemoFramework/FslUtil/Vulkan1_0/UnitTest/CMakeFiles/FslUtil.Vulkan1_0.UnitTest.dir/home/mysticp0004/var-fsl-yocto/build_xwayland/tmp/work/armv8a-mx8mp-fslc-linux/imx-gpu-sdk/6.0.2-r0/git/DemoFramework/FslUtil/Vulkan1_0/UnitTest/source/FslUtil/Vulkan1_0/UnitTest/Util/Test_DeviceMemoryUtil.cpp.o&lt;BR /&gt;| [1452/2889] Building CXX object DemoFramework/FslUtil/Vulkan1_0/UnitTest/CMakeFiles/FslUtil.Vulkan1_0.UnitTest.dir/home/mysticp0004/var-fsl-yocto/build_xwayland/tmp/work/armv8a-mx8mp-fslc-linux/imx-gpu-sdk/6.0.2-r0/git/DemoFramework/FslUtil/Vulkan1_0/UnitTest/source/FslUtil/Vulkan1_0/UnitTest/Util/Test_VUBufferMemory.cpp.o&lt;BR /&gt;| ninja: build stopped: subcommand failed.&lt;BR /&gt;| WARNING: The build command 'cmake --build . --target install -- -j 4' failed with '1'. It was run with CWD: '/home/mysticp0004/var-fsl-yocto/build_xwayland/tmp/work/armv8a-mx8mp-fslc-linux/imx-gpu-sdk/6.0.2-r0/git/build/Yocto/Ninja/release'&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 20 Jun 2024 10:25:36 GMT</pubDate>
    <dc:creator>goudam</dc:creator>
    <dc:date>2024-06-20T10:25:36Z</dc:date>
    <item>
      <title>How to Run 32 bit application on imx 8m plus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-Run-32-bit-application-on-imx-8m-plus/m-p/1890342#M225224</link>
      <description>&lt;P&gt;I need to run a 32-bit application on the imx8m plus board but that needs multilib support.While bitbaking, I had an error with the devIL recipe, which I fixed by a method followed by the same issue fixed in the community, after which I received a linker error with imx-gpu-sdk saying that the lIL lib was not found.How can I fix this error?&lt;/P&gt;&lt;P&gt;DemoApp.Util.Graphics.a -lIL DemoFramework/FslDemoHost/Console/libFslDemoHost.Console.a DemoFramework/FslDemoPlatform/Link/libFslDemoPlatform.Link.a DemoFramework/FslDemoPlatform/libFslDemoPlatform.a DemoFramework/FslDemoHost/Base/libFslDemoHost.Base.a DemoFramework/FslDemoApp/Base/libFslDemoApp.Base.a DemoFramework/FslNativeWindow/Base/libFslNativeWindow.Base.a DemoFramework/FslDemoApp/Shared/libFslDemoApp.Shared.a DemoFramework/FslGraphics/libFslGraphics.a DemoFramework/FslDemoService/CpuStats/Impl/libFslDemoService.CpuStats.Impl.a DemoFramework/FslService/Impl/libFslService.Impl.a DemoFramework/FslService/Consumer/libFslService.Consumer.a DemoFramework/FslVersion/libFslVersion.a DemoFramework/FslBase/libFslBase.a -s -lfmt &amp;amp;&amp;amp; :&lt;BR /&gt;| /home/mysticp0004/var-fsl-yocto/build_xwayland/tmp/work/armv8a-mx8mp-fslc-linux/imx-gpu-sdk/6.0.2-r0/recipe-sysroot-native/usr/bin/aarch64-fslc-linux/../../libexec/aarch64-fslc-linux/gcc/aarch64-fslc-linux/11.3.0/ld: cannot find -lIL: No such file or directory&lt;BR /&gt;| collect2: error: ld returned 1 exit status&lt;BR /&gt;| [1450/2889] Building CXX object DemoFramework/FslUtil/Vulkan1_0/UnitTest/Helper/CMakeFiles/FslUtil.Vulkan1_0.UnitTest.Helper.dir/home/mysticp0004/var-fsl-yocto/build_xwayland/tmp/work/armv8a-mx8mp-fslc-linux/imx-gpu-sdk/6.0.2-r0/git/DemoFramework/FslUtil/Vulkan1_0/UnitTest/Helper/source/FslUtil/Vulkan1_0/UnitTest/Helper/Dummy.cpp.o&lt;BR /&gt;| [1451/2889] Building CXX object DemoFramework/FslUtil/Vulkan1_0/UnitTest/CMakeFiles/FslUtil.Vulkan1_0.UnitTest.dir/home/mysticp0004/var-fsl-yocto/build_xwayland/tmp/work/armv8a-mx8mp-fslc-linux/imx-gpu-sdk/6.0.2-r0/git/DemoFramework/FslUtil/Vulkan1_0/UnitTest/source/FslUtil/Vulkan1_0/UnitTest/Util/Test_DeviceMemoryUtil.cpp.o&lt;BR /&gt;| [1452/2889] Building CXX object DemoFramework/FslUtil/Vulkan1_0/UnitTest/CMakeFiles/FslUtil.Vulkan1_0.UnitTest.dir/home/mysticp0004/var-fsl-yocto/build_xwayland/tmp/work/armv8a-mx8mp-fslc-linux/imx-gpu-sdk/6.0.2-r0/git/DemoFramework/FslUtil/Vulkan1_0/UnitTest/source/FslUtil/Vulkan1_0/UnitTest/Util/Test_VUBufferMemory.cpp.o&lt;BR /&gt;| ninja: build stopped: subcommand failed.&lt;BR /&gt;| WARNING: The build command 'cmake --build . --target install -- -j 4' failed with '1'. It was run with CWD: '/home/mysticp0004/var-fsl-yocto/build_xwayland/tmp/work/armv8a-mx8mp-fslc-linux/imx-gpu-sdk/6.0.2-r0/git/build/Yocto/Ninja/release'&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jun 2024 10:25:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-Run-32-bit-application-on-imx-8m-plus/m-p/1890342#M225224</guid>
      <dc:creator>goudam</dc:creator>
      <dc:date>2024-06-20T10:25:36Z</dc:date>
    </item>
  </channel>
</rss>