<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Does the dual screen display based on the IMX8MQ chip support dual interface display of QT softw</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Does-the-dual-screen-display-based-on-the-IMX8MQ-chip-support/m-p/1888994#M225085</link>
    <description>&lt;P&gt;Can IMX8MQ's DCSS connect multiple outputs? For example, connecting HDMI and MIPI-DSI? Can this achieve multi screen display?&lt;/P&gt;</description>
    <pubDate>Tue, 18 Jun 2024 00:55:51 GMT</pubDate>
    <dc:creator>ximenbingmeng</dc:creator>
    <dc:date>2024-06-18T00:55:51Z</dc:date>
    <item>
      <title>Does the dual screen display based on the IMX8MQ chip support dual interface display of QT software?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-the-dual-screen-display-based-on-the-IMX8MQ-chip-support/m-p/1888330#M225019</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;we can see from the reference manual that the block diagram for achieving "dual screen display" is as follows,&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ximenbingmeng_0-1718594126943.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/284356iE291368BA34DAF9F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ximenbingmeng_0-1718594126943.png" alt="ximenbingmeng_0-1718594126943.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;And I saw the following explanation,&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ximenbingmeng_1-1718594172123.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/284357i4A35DEEA24A71C5A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ximenbingmeng_1-1718594172123.png" alt="ximenbingmeng_1-1718594172123.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;So if QT is in a "flow" mode, wouldn't displaying two QT interfaces work? If feasible, are there any reference examples? The kernel version we are using is 5.10.72.&lt;BR /&gt;Looking forward to your reply, thank you very much!&lt;/P&gt;</description>
      <pubDate>Mon, 17 Jun 2024 03:17:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-the-dual-screen-display-based-on-the-IMX8MQ-chip-support/m-p/1888330#M225019</guid>
      <dc:creator>ximenbingmeng</dc:creator>
      <dc:date>2024-06-17T03:17:28Z</dc:date>
    </item>
    <item>
      <title>Re: Does the dual screen display based on the IMX8MQ chip support dual interface display of QT softw</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-the-dual-screen-display-based-on-the-IMX8MQ-chip-support/m-p/1888499#M225039</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;As far as I know it isn't possible as the i.MX 8MQ exposes 2 different DRM/KMS devices for each output, 1DCSS &amp;amp; 1LCDIF.&lt;/P&gt;&lt;P&gt;All Qt examples show multiple displays examples using 1 and only 1 DRM device:&lt;/P&gt;&lt;P&gt;&lt;A href="https://doc.qt.io/qt-6/embedded-linux.html#active-outputs-and-qscreen-instances" target="_blank"&gt;https://doc.qt.io/qt-6/embedded-linux.html#active-outputs-and-qscreen-instances&lt;/A&gt;&lt;/P&gt;&lt;P&gt;That would work on the i.MX 8MP as it exposes 1 DRM/KMS device with several connectors/outputs (HDMI, LVDS, MIPI-DSI).&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Mon, 17 Jun 2024 08:18:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-the-dual-screen-display-based-on-the-IMX8MQ-chip-support/m-p/1888499#M225039</guid>
      <dc:creator>gary_bisson</dc:creator>
      <dc:date>2024-06-17T08:18:17Z</dc:date>
    </item>
    <item>
      <title>Re: Does the dual screen display based on the IMX8MQ chip support dual interface display of QT softw</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-the-dual-screen-display-based-on-the-IMX8MQ-chip-support/m-p/1888994#M225085</link>
      <description>&lt;P&gt;Can IMX8MQ's DCSS connect multiple outputs? For example, connecting HDMI and MIPI-DSI? Can this achieve multi screen display?&lt;/P&gt;</description>
      <pubDate>Tue, 18 Jun 2024 00:55:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-the-dual-screen-display-based-on-the-IMX8MQ-chip-support/m-p/1888994#M225085</guid>
      <dc:creator>ximenbingmeng</dc:creator>
      <dc:date>2024-06-18T00:55:51Z</dc:date>
    </item>
    <item>
      <title>Re: Does the dual screen display based on the IMX8MQ chip support dual interface display of QT softw</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-the-dual-screen-display-based-on-the-IMX8MQ-chip-support/m-p/1890386#M225228</link>
      <description>&lt;P&gt;No the DCSS can only connect to 1 output at a time.&lt;/P&gt;</description>
      <pubDate>Wed, 19 Jun 2024 12:27:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-the-dual-screen-display-based-on-the-IMX8MQ-chip-support/m-p/1890386#M225228</guid>
      <dc:creator>gary_bisson</dc:creator>
      <dc:date>2024-06-19T12:27:09Z</dc:date>
    </item>
  </channel>
</rss>