<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx-linux-fb not able to run QT6 application</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx-linux-fb-not-able-to-run-QT6-application/m-p/1887973#M224996</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Make sure you are using the qt-validation image in you board since apparently you have correct all the dtb and previous packages.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Fri, 14 Jun 2024 14:45:30 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2024-06-14T14:45:30Z</dc:date>
    <item>
      <title>imx-linux-fb not able to run QT6 application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-linux-fb-not-able-to-run-QT6-application/m-p/1887875#M224987</link>
      <description>&lt;P&gt;hi&lt;/P&gt;&lt;P&gt;command to build yoctos is:(imx-linux-nanbield -m imx-6.6.3-1.0.0.xml)&lt;/P&gt;&lt;P&gt;DISTRO=fsl-imx-fb MACHINE=imx6dlsabresd source imx-setup-release.sh -b build-imx-fb&lt;BR /&gt;bitbake imx-image-full&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;we are unable to run the QT, psplash screen works good and we can see graphics.&lt;/P&gt;&lt;P&gt;root@imx6dlsabresd:/usr/share/examples/quick3d/antialiasing# fbset&lt;/P&gt;&lt;P&gt;mode "1024x600-101"&lt;BR /&gt;# &lt;LI-EMOJI id="lia_anguished-face" title=":anguished_face:"&gt;&lt;/LI-EMOJI&gt; 71.901 MHz, H: 62.851 kHz, V: 100.722 Hz&lt;BR /&gt;geometry 1024 600 1024 1200 24&lt;BR /&gt;timings 13908 24 72 10 12 24 2&lt;BR /&gt;rgba 8/16,8/8,8/0,0/0&lt;BR /&gt;endmode&lt;/P&gt;&lt;P&gt;root@imx6dlsabresd:/usr/share/examples/quick3d/hellocube# ./hellocube&lt;BR /&gt;Detected locale "C" with character encoding "ANSI_X3.4-1968", which is not UTF-8.&lt;BR /&gt;Qt depends on a UTF-8 locale, and has switched to "C.UTF-8" instead.&lt;BR /&gt;If this causes problems, reconfigure your locale. See the locale(1) manual&lt;BR /&gt;for more information.&lt;BR /&gt;QEglFSVivIntegration will set environment variable FB_MULTI_BUFFER=2 to enable double buffering and vsync.&lt;BR /&gt;If this is not desired, you can override this via: export QT_EGLFS_IMX6_NO_FB_MULTI_BUFFER=1&lt;BR /&gt;QEGLPlatformContext: Failed to create context: 3009&lt;BR /&gt;QQuickItem: Cannot set FocusScope once item has children and is in a window.&lt;BR /&gt;EGL Error : Could not create the egl surface: error = 0x300b&lt;/P&gt;&lt;P&gt;Aborted (core dumped)&lt;BR /&gt;root@imx6dlsabresd:/usr/share/examples/quick3d/hellocube#&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;after export&amp;nbsp;QT_EGLFS_IMX6_NO_FB_MULTI_BUFFER still application not works.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;root@imx6dlsabresd:/usr/share/examples/quick3d/hellocube# ./hellocube&lt;BR /&gt;Detected locale "C" with character encoding "ANSI_X3.4-1968", which is not UTF-8.&lt;BR /&gt;Qt depends on a UTF-8 locale, and has switched to "C.UTF-8" instead.&lt;BR /&gt;If this causes problems, reconfigure your locale. See the locale(1) manual&lt;BR /&gt;for more information.&lt;BR /&gt;QEGLPlatformContext: Failed to create context: 3009&lt;BR /&gt;QQuickItem: Cannot set FocusScope once item has children and is in a window.&lt;BR /&gt;EGL Error : Could not create the egl surface: error = 0x300b&lt;/P&gt;&lt;P&gt;Aborted (core dumped)&lt;BR /&gt;root@imx6dlsabresd:/usr/share/examples/quick3d/hellocube#&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jun 2024 11:58:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-linux-fb-not-able-to-run-QT6-application/m-p/1887875#M224987</guid>
      <dc:creator>Chandrashekhar_MVE</dc:creator>
      <dc:date>2024-06-14T11:58:31Z</dc:date>
    </item>
    <item>
      <title>Re: imx-linux-fb not able to run QT6 application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-linux-fb-not-able-to-run-QT6-application/m-p/1887973#M224996</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Make sure you are using the qt-validation image in you board since apparently you have correct all the dtb and previous packages.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jun 2024 14:45:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-linux-fb-not-able-to-run-QT6-application/m-p/1887973#M224996</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-06-14T14:45:30Z</dc:date>
    </item>
    <item>
      <title>Re: imx-linux-fb not able to run QT6 application</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-linux-fb-not-able-to-run-QT6-application/m-p/1888056#M225006</link>
      <description>&lt;P&gt;what you mean by&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;qt-validation image, We are using the examples which is generated by bitbake.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;examples in rootfs -&amp;gt; /usr/share/examples/quick3d/hellocube/&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Rgds&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Chandra&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jun 2024 17:53:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-linux-fb-not-able-to-run-QT6-application/m-p/1888056#M225006</guid>
      <dc:creator>Chandrashekhar_MVE</dc:creator>
      <dc:date>2024-06-14T17:53:29Z</dc:date>
    </item>
  </channel>
</rss>