<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックLinux built-in module pci-endpoint-test does not create misc device node under /dev on i.MX8 MP</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Linux-built-in-module-pci-endpoint-test-does-not-create-misc/m-p/1887120#M224935</link>
    <description>&lt;P&gt;The Linux built-in module pci-endpoint-test should create a misc device node under /dev on the Root Comples side. But this is missing on our system. No error message is visible via dmesg.&lt;/P&gt;&lt;P&gt;Does anyone see the same issue and what is the solution?&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
    <pubDate>Thu, 13 Jun 2024 15:30:56 GMT</pubDate>
    <dc:creator>dwang2</dc:creator>
    <dc:date>2024-06-13T15:30:56Z</dc:date>
    <item>
      <title>Linux built-in module pci-endpoint-test does not create misc device node under /dev on i.MX8 MP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-built-in-module-pci-endpoint-test-does-not-create-misc/m-p/1887120#M224935</link>
      <description>&lt;P&gt;The Linux built-in module pci-endpoint-test should create a misc device node under /dev on the Root Comples side. But this is missing on our system. No error message is visible via dmesg.&lt;/P&gt;&lt;P&gt;Does anyone see the same issue and what is the solution?&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jun 2024 15:30:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-built-in-module-pci-endpoint-test-does-not-create-misc/m-p/1887120#M224935</guid>
      <dc:creator>dwang2</dc:creator>
      <dc:date>2024-06-13T15:30:56Z</dc:date>
    </item>
    <item>
      <title>Re: Linux built-in module pci-endpoint-test does not create misc device node under /dev on i.MX8 MP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-built-in-module-pci-endpoint-test-does-not-create-misc/m-p/1887361#M224950</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;Could you share the steps to reproduce?&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jun 2024 22:42:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-built-in-module-pci-endpoint-test-does-not-create-misc/m-p/1887361#M224950</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2024-06-13T22:42:15Z</dc:date>
    </item>
  </channel>
</rss>