<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX93 A core M core cannot be activated simultaneously</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX93-A-core-M-core-cannot-be-activated-simultaneously/m-p/1886555#M224892</link>
    <description>&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;SPAN&gt;I use the make SOC=iMX9 REV=A1 flash_singleboot_m33 command to compile flash.bin into the chip. During the uboot phase, the debugging port of M core has printed information, but after entering the linux system, the debugging port of M core does not print information.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
    <pubDate>Thu, 13 Jun 2024 03:53:30 GMT</pubDate>
    <dc:creator>meeeeeei</dc:creator>
    <dc:date>2024-06-13T03:53:30Z</dc:date>
    <item>
      <title>iMX93 A core M core cannot be activated simultaneously</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX93-A-core-M-core-cannot-be-activated-simultaneously/m-p/1886555#M224892</link>
      <description>&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;SPAN&gt;I use the make SOC=iMX9 REV=A1 flash_singleboot_m33 command to compile flash.bin into the chip. During the uboot phase, the debugging port of M core has printed information, but after entering the linux system, the debugging port of M core does not print information.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Thu, 13 Jun 2024 03:53:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX93-A-core-M-core-cannot-be-activated-simultaneously/m-p/1886555#M224892</guid>
      <dc:creator>meeeeeei</dc:creator>
      <dc:date>2024-06-13T03:53:30Z</dc:date>
    </item>
    <item>
      <title>Re: iMX93 A core M core cannot be activated simultaneously</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX93-A-core-M-core-cannot-be-activated-simultaneously/m-p/1887671#M224978</link>
      <description>&lt;P&gt;refer to the user guide, please add the parameter "clk_ignore_unused" to the uboot bootargs like this&lt;/P&gt;
&lt;P&gt;“setenv mmcargs 'setenv bootargs ${jh_clk} console=${console} root=${mmcroot} clk_ignore_unused”&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jun 2024 07:54:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX93-A-core-M-core-cannot-be-activated-simultaneously/m-p/1887671#M224978</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2024-06-14T07:54:07Z</dc:date>
    </item>
  </channel>
</rss>