<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Secure Boot Mode</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Secure-Boot-Mode/m-p/1885567#M224824</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am currently in the development phase and would like to test secure boot mode. I have been reading the guide [here](&lt;A href="https://github.com/nxp-imx/uboot-imx/blob/lf_v2023.04/doc/imx/ahab/introduction_ahab.txt" target="_blank"&gt;https://github.com/nxp-imx/uboot-imx/blob/lf_v2023.04/doc/imx/ahab/introduction_ahab.txt&lt;/A&gt;).&lt;/P&gt;&lt;P&gt;During development, there will be lots of trial and error. According to [this section](&lt;A href="https://github.com/nxp-imx/uboot-imx/blob/lf_v2023.04/doc/imx/ahab/guides/mx8ulp_9x_secure_boot.txt#L395" target="_blank"&gt;https://github.com/nxp-imx/uboot-imx/blob/lf_v2023.04/doc/imx/ahab/guides/mx8ulp_9x_secure_boot.txt#L395&lt;/A&gt;) on reading the fuses, it does not mention whether I can run in emulation mode without burning the fuses permanently and potentially bricking the board.&lt;/P&gt;&lt;P&gt;Has anyone implemented secure boot mode during the development phase with the i.MX93? What is the correct procedure to follow without risking bricking the board?&lt;/P&gt;&lt;P&gt;Any help would be highly appreciated.&lt;/P&gt;&lt;P&gt;Cheers,&lt;BR /&gt;Nitesh&lt;/P&gt;</description>
    <pubDate>Wed, 12 Jun 2024 00:27:39 GMT</pubDate>
    <dc:creator>pilotnite</dc:creator>
    <dc:date>2024-06-12T00:27:39Z</dc:date>
    <item>
      <title>Secure Boot Mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Secure-Boot-Mode/m-p/1885567#M224824</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am currently in the development phase and would like to test secure boot mode. I have been reading the guide [here](&lt;A href="https://github.com/nxp-imx/uboot-imx/blob/lf_v2023.04/doc/imx/ahab/introduction_ahab.txt" target="_blank"&gt;https://github.com/nxp-imx/uboot-imx/blob/lf_v2023.04/doc/imx/ahab/introduction_ahab.txt&lt;/A&gt;).&lt;/P&gt;&lt;P&gt;During development, there will be lots of trial and error. According to [this section](&lt;A href="https://github.com/nxp-imx/uboot-imx/blob/lf_v2023.04/doc/imx/ahab/guides/mx8ulp_9x_secure_boot.txt#L395" target="_blank"&gt;https://github.com/nxp-imx/uboot-imx/blob/lf_v2023.04/doc/imx/ahab/guides/mx8ulp_9x_secure_boot.txt#L395&lt;/A&gt;) on reading the fuses, it does not mention whether I can run in emulation mode without burning the fuses permanently and potentially bricking the board.&lt;/P&gt;&lt;P&gt;Has anyone implemented secure boot mode during the development phase with the i.MX93? What is the correct procedure to follow without risking bricking the board?&lt;/P&gt;&lt;P&gt;Any help would be highly appreciated.&lt;/P&gt;&lt;P&gt;Cheers,&lt;BR /&gt;Nitesh&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jun 2024 00:27:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Secure-Boot-Mode/m-p/1885567#M224824</guid>
      <dc:creator>pilotnite</dc:creator>
      <dc:date>2024-06-12T00:27:39Z</dc:date>
    </item>
    <item>
      <title>Re: Secure Boot Mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Secure-Boot-Mode/m-p/1886759#M224909</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Don't close device before signing image verification passed and the SRK fuse should be fused when in production. otherwise, any images can run on the device.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jun 2024 08:10:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Secure-Boot-Mode/m-p/1886759#M224909</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2024-06-13T08:10:02Z</dc:date>
    </item>
    <item>
      <title>Re: Secure Boot Mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Secure-Boot-Mode/m-p/1887394#M224957</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/192970"&gt;@Harvey021&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hi Harvey,&lt;/P&gt;&lt;P&gt;Thank you for your response.&lt;/P&gt;&lt;P&gt;I have a few more questions regarding the SRK fuse:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;What exactly happens when the SRK fuse is burned?&lt;/LI&gt;&lt;LI&gt;Once the SRK fuse is burned, can I still re-flash the unit using the same certificates and keys?&lt;/LI&gt;&lt;LI&gt;Will I be able to perform OTA updates to the filesystem or update the bootloader after the SRK fuse is burned?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Your clarification on these points would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Nitesh&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jun 2024 00:50:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Secure-Boot-Mode/m-p/1887394#M224957</guid>
      <dc:creator>pilotnite</dc:creator>
      <dc:date>2024-06-14T00:50:49Z</dc:date>
    </item>
    <item>
      <title>Re: Secure Boot Mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Secure-Boot-Mode/m-p/1887560#M224969</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;SRK fuse helps the root of trust established if SRK table in signed image verify successfully against SRK fuse in Fuse box.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jun 2024 06:01:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Secure-Boot-Mode/m-p/1887560#M224969</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2024-06-14T06:01:33Z</dc:date>
    </item>
  </channel>
</rss>