<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: devtool build-image does not work</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/devtool-build-image-does-not-work/m-p/1883687#M224705</link>
    <description>&lt;P&gt;&lt;U&gt;I do get a bitbake failure if I cha&lt;FONT color="#000000"&gt;nge the &lt;FONT color="#FF0000"&gt;highlighted line of my local.conf&lt;/FONT&gt; to 1... from&lt;/FONT&gt; 0. There appears to be a connection in my devtool build-image failure and the failure I get when I make the local.conf change below.&amp;nbsp;&lt;/U&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;# Bsp default build values.&lt;BR /&gt;MACHINE ??= "xxxxx"&lt;BR /&gt;DISTRO ??= "xxxxx-xxxxxxx"&lt;/P&gt;&lt;P&gt;# Multiconfig list of targets&lt;BR /&gt;# You need to create a single configuration file for&lt;BR /&gt;# each build target (each multiconfig) for more info&lt;BR /&gt;# look at meta-oem/conf/templates/multiconfig/&lt;BR /&gt;BBMULTICONFIG = "ngpd2"&lt;/P&gt;&lt;P&gt;PACKAGE_CLASSES = "package_deb"&lt;/P&gt;&lt;P&gt;USER_CLASSES ?= "buildstats "&lt;BR /&gt;PATCHRESOLVE = "noop"&lt;BR /&gt;BB_DISKMON_DIRS = "\&lt;BR /&gt;STOPTASKS,${TMPDIR},1G,100K \&lt;BR /&gt;STOPTASKS,${DL_DIR},1G,100K \&lt;BR /&gt;STOPTASKS,${SSTATE_DIR},1G,100K \&lt;BR /&gt;STOPTASKS,/tmp,100M,100K \&lt;BR /&gt;HALT,${TMPDIR},100M,1K \&lt;BR /&gt;HALT,${DL_DIR},100M,1K \&lt;BR /&gt;HALT,${SSTATE_DIR},100M,1K \&lt;BR /&gt;HALT,/tmp,10M,1K"&lt;/P&gt;&lt;P&gt;CONF_VERSION = "2"&lt;BR /&gt;ACCEPT_FSL_EULA = "1"&lt;/P&gt;&lt;P&gt;# Share dirs between build targets&lt;BR /&gt;DL_DIR ?= "${TOPDIR}/../downloads/"&lt;BR /&gt;SSTATE_DIR ?= "${TOPDIR}/../sstate/"&lt;/P&gt;&lt;P&gt;# This prevents searching the network anywhere but PREMIRRORS, populated solely from SOURCE_MIRROR_URL&lt;BR /&gt;# BB_FETCH_PREMIRRORONLY = "1"&lt;/P&gt;&lt;P&gt;# SDK Variables&lt;BR /&gt;SDKMACHINE ?= "x86_64"&lt;BR /&gt;SDK_EXT_TYPE = "minimal"&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;SDK_INCLUDE_TOOLCHAIN = "1"&lt;/FONT&gt;&lt;BR /&gt;SDK_INCLUDE_BUILDTOOLS = "0"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I do get an error.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;ERROR: xxx-xxxxx-xxxxxxx-xxxxx-1.0-r0 do_populate_sdk_ext: Failed to generate filtered task list for extensible SDK:&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;### Shell environment set up for builds. ###&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;You can now run 'bitbake &amp;lt;target&amp;gt;'&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;Common targets are:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;core-image-minimal&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;core-image-full-cmdline&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;core-image-sato&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;core-image-weston&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;meta-toolchain&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;meta-ide-support&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;You can also run generated qemu images with a command like 'runqemu qemux86-64'.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;Other commonly useful commands are:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;- 'devtool' and 'recipetool' handle common recipe tasks&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;- 'bitbake-layers' handles common layer tasks&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;- 'oe-pkgdata-util' handles common target package tasks&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;ERROR: bitbake failed:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;WARNING: You are using a local hash equivalence server but have configured an sstate mirror. This will likely mean no sstate will match from the mirror. You may wish to disable the hash equivalence use (BB_HASHSERVE), or use a hash equivalence server alongside the sstate mirror.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;WARNING: You are using a local hash equivalence server but have configured an sstate mirror. This will likely mean no sstate will match from the mirror. You may wish to disable the hash equivalence use (BB_HASHSERVE), or use a hash equivalence server alongside the sstate mirror.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;Loading cache...done.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;Loaded 0 entries from dependency cache.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;Parsing recipes...done.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;ERROR: No recipes in default available for:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;/layers/meta-freescale/recipes-graphics/vulkan/vulkan-loader_1.2.182.0.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;/recipes-bsp/imx-atf/imx-atf_%.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;recipes-bsp/imx-mkimage/imx-boot_1.0.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;/recipes-bsp/imx-mkimage/imx-mkimage_git.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;/recipes-bsp/scfw-deere-display/imx-sc-firmware_%.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;No recipes in ngpd2 available for:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;layers/meta-freescale/recipes-graphics/vulkan/vulkan-loader_1.2.182.0.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;/imx-atf/imx-atf_%.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;p/imx-mkimage/imx-boot_1.0.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;imx-mkimage_git.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;y/imx-sc-firmware_%.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;Parsing of 5594 .bb files complete (0 cached, 5594 parsed). 8682 targets, 1176 skipped, 0 masked, 0 errors.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;Summary: There were 2 WARNING messages.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;Summary: There was 1 ERROR message, returning a non-zero exit code.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;ERROR: Logfile of failure stored in: /log.do_populate_sdk_ext.2230270&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;ERROR: Task .bb:do_populate_sdk_ext) failed with exit code '1'&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;Pseudo log:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;path mismatch [8 links]: ino 28324762 db '/meta-freescale/EULA'.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;Setup complete, sending SIGUSR1 to pid 2229735.&lt;/FONT&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 07 Jun 2024 20:57:06 GMT</pubDate>
    <dc:creator>TimNew</dc:creator>
    <dc:date>2024-06-07T20:57:06Z</dc:date>
    <item>
      <title>devtool build-image does not work</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/devtool-build-image-does-not-work/m-p/1883072#M224668</link>
      <description>&lt;P&gt;When I try to build `pokyuser@92da2e39ecdd:~/oem-deere-display_sdk$ &lt;STRONG&gt;devtool build-image&lt;/STRONG&gt;`&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I get the following failures:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;Parsing of 5594 .bb files complete (0 cached, 5594 parsed). 8682 targets, 1176 skipped, 0 masked, 0 errors.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;ERROR: No recipes in default available for:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#FF0000"&gt;/home/pokyuser/oem-deere-display_sdk/layers/meta-freescale/recipes-graphics/vulkan/vulkan-loader_1.2.182.0.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#FF0000"&gt;/home/pokyuser/oem-deere-display_sdk/layers/meta-deere-oem/meta-deere-display-oem/recipes-bsp/imx-atf/imx-atf_%.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#FF0000"&gt;/home/pokyuser/oem-deere-display_sdk/layers/meta-deere-oem/meta-deere-display-oem/recipes-bsp/imx-mkimage/imx-boot_1.0.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#FF0000"&gt;/home/pokyuser/oem-deere-display_sdk/layers/meta-deere-oem/meta-deere-display-oem/recipes-bsp/imx-mkimage/imx-mkimage_git.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#FF0000"&gt;/home/pokyuser/oem-deere-display_sdk/layers/meta-deere-oem/meta-deere-display-oem/recipes-bsp/scfw-deere-display/imx-sc-firmware_%.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;No recipes in ngpd2 available for:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#FF0000"&gt;/home/pokyuser/oem-deere-display_sdk/layers/meta-freescale/recipes-graphics/vulkan/vulkan-loader_1.2.182.0.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#FF0000"&gt;/home/pokyuser/oem-deere-display_sdk/layers/meta-deere-oem/meta-deere-display-oem/recipes-bsp/imx-atf/imx-atf_%.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#FF0000"&gt;/home/pokyuser/oem-deere-display_sdk/layers/meta-deere-oem/meta-deere-display-oem/recipes-bsp/imx-mkimage/imx-boot_1.0.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#FF0000"&gt;/home/pokyuser/oem-deere-display_sdk/layers/meta-deere-oem/meta-deere-display-oem/recipes-bsp/imx-mkimage/imx-mkimage_git.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#FF0000"&gt;/home/pokyuser/oem-deere-display_sdk/layers/meta-deere-oem/meta-deere-display-oem/recipes-bsp/scfw-deere-display/imx-sc-firmware_%.bbappend&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I know why those errors occur, when i run the sdk install .sh script not all the directories in the mete-freescale layer are copied. I'm not sure why.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is what the meta-freescale layer has in my normal build. You can see the recipes-downgrade directory. The missing .bb recipe is included there.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;tn70742@wdx24n1rn3:~/Projects/OEMBSP/oem-ref-BSP/sources/meta-freescale$ ls -ll&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;total 140&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 2 tn70742 tn70742 4096 Jun 5 12:17 classes&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 3 tn70742 tn70742 4096 Jun 5 12:17 conf&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;-rw-rw-r-- 1 tn70742 tn70742 1035 Jun 5 12:17 COPYING.MIT&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 2 tn70742 tn70742 4096 Jun 5 12:17 custom-licenses&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 13 tn70742 tn70742 4096 Jun 5 12:17 dynamic-layers&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;-rw-r--r-- 8 tn70742 tn70742 43342 Mar 9 2018 EULA&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;-rw-rw-r-- 1 tn70742 tn70742 495 Jun 5 12:17 LICENSE&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;-rw-rw-r-- 1 tn70742 tn70742 1006 Jun 5 12:17 README&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 34 tn70742 tn70742 4096 Jun 5 12:17 recipes-bsp&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 3 tn70742 tn70742 4096 Jun 5 12:17 recipes-connectivity&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 5 tn70742 tn70742 4096 Jun 5 12:17 recipes-core&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 8 tn70742 tn70742 4096 Jun 5 12:17 recipes-devtools&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;&lt;STRONG&gt;drwxrwxr-x 3 tn70742 tn70742 4096 Jun 5 12:17 recipes-downgrade&lt;/STRONG&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 6 tn70742 tn70742 4096 Jun 5 12:17 recipes-dpaa&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 8 tn70742 tn70742 4096 Jun 5 12:17 recipes-dpaa2&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 17 tn70742 tn70742 4096 Jun 5 12:17 recipes-extended&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 4 tn70742 tn70742 4096 Jun 5 12:17 recipes-fsl&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 22 tn70742 tn70742 4096 Jun 5 12:17 recipes-graphics&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 7 tn70742 tn70742 4096 Jun 5 12:17 recipes-kernel&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 14 tn70742 tn70742 4096 Jun 5 12:17 recipes-multimedia&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 4 tn70742 tn70742 4096 Jun 5 12:17 recipes-security&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 3 tn70742 tn70742 4096 Jun 5 12:17 recipes-support&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 2 tn70742 tn70742 4096 Jun 5 12:17 SCR&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 2 tn70742 tn70742 4096 Jun 5 12:17 scripts&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 2 tn70742 tn70742 4096 Jun 5 12:17 wic&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;When I look at the equivalent directory in the sdk environement, there is no recipes-downgrade directory.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;pokyuser@92da2e39ecdd:~/oem-deere-display_sdk/layers/meta-freescale$ ls -ll&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;total 88&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 2 pokyuser pokyuser 4096 Jun 6 21:19 classes&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 3 pokyuser pokyuser 4096 Jun 6 21:19 conf&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;-rw-rw-r-- 1 pokyuser pokyuser 1035 Jun 6 21:19 COPYING.MIT&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 2 pokyuser pokyuser 4096 Jun 6 21:19 custom-licenses&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 13 pokyuser pokyuser 4096 Jun 6 21:19 dynamic-layers&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;-rw-rw-r-- 1 pokyuser pokyuser 495 Jun 6 21:19 LICENSE&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;-rw-rw-r-- 1 pokyuser pokyuser 1006 Jun 6 21:19 README&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 3 pokyuser pokyuser 4096 Jun 6 21:19 recipes-connectivity&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 5 pokyuser pokyuser 4096 Jun 6 21:19 recipes-core&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 8 pokyuser pokyuser 4096 Jun 6 21:19 recipes-devtools&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 6 pokyuser pokyuser 4096 Jun 6 21:19 recipes-dpaa&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 8 pokyuser pokyuser 4096 Jun 6 21:19 recipes-dpaa2&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 17 pokyuser pokyuser 4096 Jun 6 21:19 recipes-extended&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 4 pokyuser pokyuser 4096 Jun 6 21:19 recipes-fsl&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 22 pokyuser pokyuser 4096 Jun 6 21:19 recipes-graphics&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 7 pokyuser pokyuser 4096 Jun 6 21:19 recipes-kernel&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 14 pokyuser pokyuser 4096 Jun 6 21:19 recipes-multimedia&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 4 pokyuser pokyuser 4096 Jun 6 21:19 recipes-security&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 3 pokyuser pokyuser 4096 Jun 6 21:19 recipes-support&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 2 pokyuser pokyuser 4096 Jun 6 21:19 SCR&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 2 pokyuser pokyuser 4096 Jun 6 21:19 scripts&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;drwxrwxr-x 2 pokyuser pokyuser 4096 Jun 6 21:19 wic&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm not sure why the r&lt;STRONG&gt;ecipes-downgrade&lt;/STRONG&gt; directory is not being copied into the sdk environment.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jun 2024 21:31:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/devtool-build-image-does-not-work/m-p/1883072#M224668</guid>
      <dc:creator>TimNew</dc:creator>
      <dc:date>2024-06-06T21:31:26Z</dc:date>
    </item>
    <item>
      <title>Re: devtool build-image does not work</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/devtool-build-image-does-not-work/m-p/1883127#M224670</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;Do bitbake work in your environment?&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jun 2024 23:24:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/devtool-build-image-does-not-work/m-p/1883127#M224670</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2024-06-06T23:24:52Z</dc:date>
    </item>
    <item>
      <title>Re: devtool build-image does not work</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/devtool-build-image-does-not-work/m-p/1883176#M224674</link>
      <description>&lt;P&gt;Yes, bitbake works. I used it to generate the SDK and normal images&lt;/P&gt;</description>
      <pubDate>Fri, 07 Jun 2024 20:52:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/devtool-build-image-does-not-work/m-p/1883176#M224674</guid>
      <dc:creator>TimNew</dc:creator>
      <dc:date>2024-06-07T20:52:37Z</dc:date>
    </item>
    <item>
      <title>Re: devtool build-image does not work</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/devtool-build-image-does-not-work/m-p/1883687#M224705</link>
      <description>&lt;P&gt;&lt;U&gt;I do get a bitbake failure if I cha&lt;FONT color="#000000"&gt;nge the &lt;FONT color="#FF0000"&gt;highlighted line of my local.conf&lt;/FONT&gt; to 1... from&lt;/FONT&gt; 0. There appears to be a connection in my devtool build-image failure and the failure I get when I make the local.conf change below.&amp;nbsp;&lt;/U&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;# Bsp default build values.&lt;BR /&gt;MACHINE ??= "xxxxx"&lt;BR /&gt;DISTRO ??= "xxxxx-xxxxxxx"&lt;/P&gt;&lt;P&gt;# Multiconfig list of targets&lt;BR /&gt;# You need to create a single configuration file for&lt;BR /&gt;# each build target (each multiconfig) for more info&lt;BR /&gt;# look at meta-oem/conf/templates/multiconfig/&lt;BR /&gt;BBMULTICONFIG = "ngpd2"&lt;/P&gt;&lt;P&gt;PACKAGE_CLASSES = "package_deb"&lt;/P&gt;&lt;P&gt;USER_CLASSES ?= "buildstats "&lt;BR /&gt;PATCHRESOLVE = "noop"&lt;BR /&gt;BB_DISKMON_DIRS = "\&lt;BR /&gt;STOPTASKS,${TMPDIR},1G,100K \&lt;BR /&gt;STOPTASKS,${DL_DIR},1G,100K \&lt;BR /&gt;STOPTASKS,${SSTATE_DIR},1G,100K \&lt;BR /&gt;STOPTASKS,/tmp,100M,100K \&lt;BR /&gt;HALT,${TMPDIR},100M,1K \&lt;BR /&gt;HALT,${DL_DIR},100M,1K \&lt;BR /&gt;HALT,${SSTATE_DIR},100M,1K \&lt;BR /&gt;HALT,/tmp,10M,1K"&lt;/P&gt;&lt;P&gt;CONF_VERSION = "2"&lt;BR /&gt;ACCEPT_FSL_EULA = "1"&lt;/P&gt;&lt;P&gt;# Share dirs between build targets&lt;BR /&gt;DL_DIR ?= "${TOPDIR}/../downloads/"&lt;BR /&gt;SSTATE_DIR ?= "${TOPDIR}/../sstate/"&lt;/P&gt;&lt;P&gt;# This prevents searching the network anywhere but PREMIRRORS, populated solely from SOURCE_MIRROR_URL&lt;BR /&gt;# BB_FETCH_PREMIRRORONLY = "1"&lt;/P&gt;&lt;P&gt;# SDK Variables&lt;BR /&gt;SDKMACHINE ?= "x86_64"&lt;BR /&gt;SDK_EXT_TYPE = "minimal"&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;SDK_INCLUDE_TOOLCHAIN = "1"&lt;/FONT&gt;&lt;BR /&gt;SDK_INCLUDE_BUILDTOOLS = "0"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I do get an error.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;ERROR: xxx-xxxxx-xxxxxxx-xxxxx-1.0-r0 do_populate_sdk_ext: Failed to generate filtered task list for extensible SDK:&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;### Shell environment set up for builds. ###&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;You can now run 'bitbake &amp;lt;target&amp;gt;'&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;Common targets are:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;core-image-minimal&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;core-image-full-cmdline&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;core-image-sato&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;core-image-weston&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;meta-toolchain&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;meta-ide-support&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;You can also run generated qemu images with a command like 'runqemu qemux86-64'.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;Other commonly useful commands are:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;- 'devtool' and 'recipetool' handle common recipe tasks&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;- 'bitbake-layers' handles common layer tasks&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;- 'oe-pkgdata-util' handles common target package tasks&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;ERROR: bitbake failed:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;WARNING: You are using a local hash equivalence server but have configured an sstate mirror. This will likely mean no sstate will match from the mirror. You may wish to disable the hash equivalence use (BB_HASHSERVE), or use a hash equivalence server alongside the sstate mirror.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;WARNING: You are using a local hash equivalence server but have configured an sstate mirror. This will likely mean no sstate will match from the mirror. You may wish to disable the hash equivalence use (BB_HASHSERVE), or use a hash equivalence server alongside the sstate mirror.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;Loading cache...done.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;Loaded 0 entries from dependency cache.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;Parsing recipes...done.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;ERROR: No recipes in default available for:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;/layers/meta-freescale/recipes-graphics/vulkan/vulkan-loader_1.2.182.0.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;/recipes-bsp/imx-atf/imx-atf_%.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;recipes-bsp/imx-mkimage/imx-boot_1.0.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;/recipes-bsp/imx-mkimage/imx-mkimage_git.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;/recipes-bsp/scfw-deere-display/imx-sc-firmware_%.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;No recipes in ngpd2 available for:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;layers/meta-freescale/recipes-graphics/vulkan/vulkan-loader_1.2.182.0.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;/imx-atf/imx-atf_%.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;p/imx-mkimage/imx-boot_1.0.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;imx-mkimage_git.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;y/imx-sc-firmware_%.bbappend&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;Parsing of 5594 .bb files complete (0 cached, 5594 parsed). 8682 targets, 1176 skipped, 0 masked, 0 errors.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;Summary: There were 2 WARNING messages.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;Summary: There was 1 ERROR message, returning a non-zero exit code.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;ERROR: Logfile of failure stored in: /log.do_populate_sdk_ext.2230270&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;ERROR: Task .bb:do_populate_sdk_ext) failed with exit code '1'&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;Pseudo log:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;path mismatch [8 links]: ino 28324762 db '/meta-freescale/EULA'.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="1 2 3 4 5 6 7"&gt;Setup complete, sending SIGUSR1 to pid 2229735.&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 07 Jun 2024 20:57:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/devtool-build-image-does-not-work/m-p/1883687#M224705</guid>
      <dc:creator>TimNew</dc:creator>
      <dc:date>2024-06-07T20:57:06Z</dc:date>
    </item>
  </channel>
</rss>