<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: SPL in iMX8QM boot process</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SPL-in-iMX8QM-boot-process/m-p/1879034#M224424</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;A1. No its not used.&lt;/P&gt;
&lt;P&gt;A2. No, is just uboot.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Fri, 31 May 2024 14:38:00 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2024-05-31T14:38:00Z</dc:date>
    <item>
      <title>SPL in iMX8QM boot process</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPL-in-iMX8QM-boot-process/m-p/1878349#M224377</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have some queries regarding the boot process of the i.MX8QM.&lt;/P&gt;&lt;P&gt;While referring to the boot process of the i.MX8QM from this link(&lt;A href="https://imxdev.gitlab.io/tutorial/System_controller_unit_introduction_for_imx_8qxp_mek/" target="_self"&gt;https://imxdev.gitlab.io/tutorial/System_controller_unit_introduction_for_imx_8qxp_mek/&lt;/A&gt;&amp;nbsp;), it appears that SPL is not used in the boot process. The Linux user's guide also states that the i.MX8QM does not use U-Boot SPL (I have attached the relevant portion to this post).&lt;/P&gt;&lt;P&gt;However, when we boot the board with Linux (version 5.15.52), the log starts like this:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;U-Boot SPL 2022.04-lf_v2022.04+g16e8414193 (Oct 08 2022 - 13:33:43 +0000)&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Normal Boot&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Trying to boot from MMC2_2&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Primary set selected&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Load image from MMC/SD 0x7b400&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;U-Boot 2022.04-lf_v2022.04+g16e8414193 (Oct 08 2022 - 13:33:43 +0000)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;CPU: NXP i.MX8QM RevB A53 at 1200 MHz at 32C&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Model: NXP i.MX8QM MEK&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Board: iMX8QM MEK&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Boot: SD1&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;DRAM: 5.8 GiB&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Given the above, I have a couple of questions:&lt;/P&gt;&lt;P&gt;1. Why are we seeing SPL in the log, if SPL is not used in the boot process of the i.MX8QM?&lt;BR /&gt;2. Is the u-boot.bin used in the i.MX8QM folder of the mkimage tool a combination of U-Boot SPL and U-Boot?&lt;/P&gt;&lt;P&gt;Thank you for your assistance.&lt;/P&gt;</description>
      <pubDate>Thu, 30 May 2024 17:30:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPL-in-iMX8QM-boot-process/m-p/1878349#M224377</guid>
      <dc:creator>AbhijithShaji</dc:creator>
      <dc:date>2024-05-30T17:30:25Z</dc:date>
    </item>
    <item>
      <title>Re: SPL in iMX8QM boot process</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPL-in-iMX8QM-boot-process/m-p/1879034#M224424</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;A1. No its not used.&lt;/P&gt;
&lt;P&gt;A2. No, is just uboot.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Fri, 31 May 2024 14:38:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPL-in-iMX8QM-boot-process/m-p/1879034#M224424</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-05-31T14:38:00Z</dc:date>
    </item>
    <item>
      <title>Re: SPL in iMX8QM boot process</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPL-in-iMX8QM-boot-process/m-p/1879562#M224476</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I checked the config file of U-Boot used for the default i.MX8QM build, and it specifies CONFIG_SPL=y.&lt;BR /&gt;Since the config file indicates CONFIG_SPL=y, it appears that SPL is indeed being built and used.&lt;BR /&gt;This is the source of my confusion. Could you please elaborate on your answer?&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;</description>
      <pubDate>Mon, 03 Jun 2024 07:36:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPL-in-iMX8QM-boot-process/m-p/1879562#M224476</guid>
      <dc:creator>AbhijithShaji</dc:creator>
      <dc:date>2024-06-03T07:36:29Z</dc:date>
    </item>
  </channel>
</rss>