<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX8QM USB boot Fail in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QM-USB-boot-Fail/m-p/1878525#M224390</link>
    <description>&lt;P&gt;你好，&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;我用i.MX8QM制作了一个板子，默认boot模式为eMMC0 boot，可手动切换为USB Serial Download模式。&lt;/P&gt;&lt;P&gt;我出现的问题是：&lt;/P&gt;&lt;P&gt;在默认boot模式下，板子上电正常。外部稳压源给板子的供电电压为5V，实际输出电流为0.65A。在手动切换到USB Serial Download模式后，稳压源电压输出保持不变，但输出电流降低到0.44A。经测PMIC1和PMIC2的SW regulator输出电压，发现异常。比如：SW7应该输出3.3V，实测为3.0V。SW6应该输出1.1V，实测为0.8V。将boot模式切换为默认模式后，稳压源输出电流又恢复至0.65A，PMIC的输出电压又恢复正常。&lt;/P&gt;&lt;P&gt;因为切换到USB Serial Download模式后，PMIC输出电压异常，导致上位机无法识别i.MX8这个USB设备。&lt;/P&gt;&lt;P&gt;感谢你的关注，期待你的解答与帮助，谢谢！&lt;/P&gt;</description>
    <pubDate>Fri, 31 May 2024 02:23:54 GMT</pubDate>
    <dc:creator>st_hw</dc:creator>
    <dc:date>2024-05-31T02:23:54Z</dc:date>
    <item>
      <title>i.MX8QM USB boot Fail</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QM-USB-boot-Fail/m-p/1878525#M224390</link>
      <description>&lt;P&gt;你好，&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;我用i.MX8QM制作了一个板子，默认boot模式为eMMC0 boot，可手动切换为USB Serial Download模式。&lt;/P&gt;&lt;P&gt;我出现的问题是：&lt;/P&gt;&lt;P&gt;在默认boot模式下，板子上电正常。外部稳压源给板子的供电电压为5V，实际输出电流为0.65A。在手动切换到USB Serial Download模式后，稳压源电压输出保持不变，但输出电流降低到0.44A。经测PMIC1和PMIC2的SW regulator输出电压，发现异常。比如：SW7应该输出3.3V，实测为3.0V。SW6应该输出1.1V，实测为0.8V。将boot模式切换为默认模式后，稳压源输出电流又恢复至0.65A，PMIC的输出电压又恢复正常。&lt;/P&gt;&lt;P&gt;因为切换到USB Serial Download模式后，PMIC输出电压异常，导致上位机无法识别i.MX8这个USB设备。&lt;/P&gt;&lt;P&gt;感谢你的关注，期待你的解答与帮助，谢谢！&lt;/P&gt;</description>
      <pubDate>Fri, 31 May 2024 02:23:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QM-USB-boot-Fail/m-p/1878525#M224390</guid>
      <dc:creator>st_hw</dc:creator>
      <dc:date>2024-05-31T02:23:54Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8QM USB boot Fail</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8QM-USB-boot-Fail/m-p/1880077#M224497</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Could you please share the power, boot mode switches and USB sections? To discard any issue on hardware side.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Mon, 03 Jun 2024 21:21:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8QM-USB-boot-Fail/m-p/1880077#M224497</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2024-06-03T21:21:27Z</dc:date>
    </item>
  </channel>
</rss>