<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx8mp Embedded ISP Gamma encoding</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-Embedded-ISP-Gamma-encoding/m-p/1876391#M224265</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;No gamma encoding is supported by ISP you better check your camera is causing the gamma encoding.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12060.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12060.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Tue, 28 May 2024 14:33:46 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2024-05-28T14:33:46Z</dc:date>
    <item>
      <title>imx8mp Embedded ISP Gamma encoding</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-Embedded-ISP-Gamma-encoding/m-p/1876254#M224251</link>
      <description>&lt;P&gt;&lt;STRONG&gt;Hello,&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Our images look good,&lt;/SPAN&gt;&lt;SPAN&gt; but I don't quite understand a factual situation regarding the gamma.&lt;/SPAN&gt;&lt;SPAN&gt; The ISP seems to be applying gamma correction even though it is explicitly turned off.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I don't quite understand where the gamma encoding should come from.&lt;/SPAN&gt;&lt;SPAN&gt; Maybe you can help me here.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The following points are known:&lt;/SPAN&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN&gt;The image sensor (Sony IMX477) delivers linear image data.&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;Gamma decoding in the ISP (degamma) is programmed to pass-through (see XML):&lt;/SPAN&gt;&lt;SPAN&gt; input array == output array.&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;Gamma encoding in the ISP is turned off (see XML:&lt;/SPAN&gt;&lt;SPAN&gt; gc enable="false").&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;The ISP-CCM was set to the identity matrix and AWB was turned off.&lt;/SPAN&gt;&lt;SPAN&gt; Manual WB was set to 1,&lt;/SPAN&gt;&lt;SPAN&gt;1,&lt;/SPAN&gt;&lt;SPAN&gt;1,&lt;/SPAN&gt;&lt;SPAN&gt;1 (pass-through).&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;Gamma decoding of 2.&lt;/SPAN&gt;&lt;SPAN&gt;2 is applied in the LCD display controller (implemented in the kernel driver).&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;SPAN&gt;The black values are correctly reproduced both from the LCD live images and from the YUYV snapshots (directly after the embedded ISP),&lt;/SPAN&gt;&lt;SPAN&gt; which means that a gamma must have been set in the ISP.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;However,&lt;/SPAN&gt;&lt;SPAN&gt; since this is turned off,&lt;/SPAN&gt;&lt;SPAN&gt; I don't understand where the gamma comes from?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Thx, M.Cisse&lt;/STRONG&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 28 May 2024 10:25:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-Embedded-ISP-Gamma-encoding/m-p/1876254#M224251</guid>
      <dc:creator>malik_cisse</dc:creator>
      <dc:date>2024-05-28T10:25:48Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp Embedded ISP Gamma encoding</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-Embedded-ISP-Gamma-encoding/m-p/1876391#M224265</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;No gamma encoding is supported by ISP you better check your camera is causing the gamma encoding.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12060.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12060.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 28 May 2024 14:33:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-Embedded-ISP-Gamma-encoding/m-p/1876391#M224265</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-05-28T14:33:46Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp Embedded ISP Gamma encoding</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-Embedded-ISP-Gamma-encoding/m-p/1876407#M224268</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for the quick feedback.&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt;&lt;SPAN&gt;No gamma encoding is supported by ISP you better check your camera is causing the gamma encoding.&lt;/SPAN&gt;&lt;BR /&gt;This statement might be correct for the software software ISP (SW-ISP). I am referring to the i.MX8M-Plus embedded ISP which definitely has deGamma (or sensor linearization) as well as Gamma encoding (also referred in the xml ISP config file as "&lt;STRONG&gt;gc enable"&lt;/STRONG&gt;).&lt;/P&gt;&lt;P&gt;The whole point using the i.MX8M-Plus is to avoid the SW-ISP.&lt;BR /&gt;But thank you for trying to help.&lt;BR /&gt;Cheers&lt;/P&gt;</description>
      <pubDate>Tue, 28 May 2024 14:59:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-Embedded-ISP-Gamma-encoding/m-p/1876407#M224268</guid>
      <dc:creator>malik_cisse</dc:creator>
      <dc:date>2024-05-28T14:59:17Z</dc:date>
    </item>
  </channel>
</rss>