<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックAutomatically switching eMMC boot partition with i.MX8MM</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Automatically-switching-eMMC-boot-partition-with-i-MX8MM/m-p/1870580#M224049</link>
    <description>&lt;P&gt;We use eMMC memory with our i.MX8MM. The memory has two boot partitions, each containing a copy of the bootloader. Secure boot is used.&lt;/P&gt;&lt;P&gt;Is there any way to automatically recover from the case that the selected boot partition contains an invalid bootloader? For example signed with a revoked key or corrupted somehow.&lt;/P&gt;&lt;P&gt;If I update an unsigned bootloader to the active partition, the device will go into serial download mode after rebooting.&lt;/P&gt;&lt;P&gt;Is there any way to configure the processor or Boot ROM to automatically try the other partition, if the active one fails to start?&lt;/P&gt;</description>
    <pubDate>Wed, 22 May 2024 09:57:17 GMT</pubDate>
    <dc:creator>Sampo</dc:creator>
    <dc:date>2024-05-22T09:57:17Z</dc:date>
    <item>
      <title>Automatically switching eMMC boot partition with i.MX8MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Automatically-switching-eMMC-boot-partition-with-i-MX8MM/m-p/1870580#M224049</link>
      <description>&lt;P&gt;We use eMMC memory with our i.MX8MM. The memory has two boot partitions, each containing a copy of the bootloader. Secure boot is used.&lt;/P&gt;&lt;P&gt;Is there any way to automatically recover from the case that the selected boot partition contains an invalid bootloader? For example signed with a revoked key or corrupted somehow.&lt;/P&gt;&lt;P&gt;If I update an unsigned bootloader to the active partition, the device will go into serial download mode after rebooting.&lt;/P&gt;&lt;P&gt;Is there any way to configure the processor or Boot ROM to automatically try the other partition, if the active one fails to start?&lt;/P&gt;</description>
      <pubDate>Wed, 22 May 2024 09:57:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Automatically-switching-eMMC-boot-partition-with-i-MX8MM/m-p/1870580#M224049</guid>
      <dc:creator>Sampo</dc:creator>
      <dc:date>2024-05-22T09:57:17Z</dc:date>
    </item>
    <item>
      <title>Re: Automatically switching eMMC boot partition with i.MX8MM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Automatically-switching-eMMC-boot-partition-with-i-MX8MM/m-p/1873782#M224107</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Yes, please refer to the Reference Manual chapter 6.1.5.4.5 Redundant boot support for expansion device.&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;For the secondary image support, the primary image must reserve the space for the secondary image table.&lt;BR /&gt;&lt;BR /&gt;Also, for the Closed mode, if there are failures during primary image authentication, the boot ROM turns on the PERSIST_SECONDARY_BOOT bit (see Table 6-8) and performs the software reset. (After the software reset, the secondary image is used).&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Thu, 23 May 2024 18:37:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Automatically-switching-eMMC-boot-partition-with-i-MX8MM/m-p/1873782#M224107</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2024-05-23T18:37:51Z</dc:date>
    </item>
  </channel>
</rss>