<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 imx8mplus - webgl not running issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mplus-webgl-not-running-issue/m-p/1870372#M224039</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;After installing the android14.1.2 demo bsp on the imx8mplus-evk board, run webview from the main menu and enter the address threejs.org - examples menu, the first sample is not executed.&lt;/P&gt;&lt;P&gt;It seems that web-gl is not running normally, and when I create a webview program in android studio and upload it, the window closes with an error.&lt;/P&gt;&lt;P&gt;Is there anything else I need to do in the bsp settings or bsp source code to use web-gl or web-gpu?&lt;/P&gt;&lt;P&gt;Doesn't the GC7000UL support webgl?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 22 May 2024 07:29:14 GMT</pubDate>
    <dc:creator>bluey2ks</dc:creator>
    <dc:date>2024-05-22T07:29:14Z</dc:date>
    <item>
      <title>imx8mplus - webgl not running issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mplus-webgl-not-running-issue/m-p/1870372#M224039</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;After installing the android14.1.2 demo bsp on the imx8mplus-evk board, run webview from the main menu and enter the address threejs.org - examples menu, the first sample is not executed.&lt;/P&gt;&lt;P&gt;It seems that web-gl is not running normally, and when I create a webview program in android studio and upload it, the window closes with an error.&lt;/P&gt;&lt;P&gt;Is there anything else I need to do in the bsp settings or bsp source code to use web-gl or web-gpu?&lt;/P&gt;&lt;P&gt;Doesn't the GC7000UL support webgl?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 22 May 2024 07:29:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mplus-webgl-not-running-issue/m-p/1870372#M224039</guid>
      <dc:creator>bluey2ks</dc:creator>
      <dc:date>2024-05-22T07:29:14Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mplus - webgl not running issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mplus-webgl-not-running-issue/m-p/1875276#M224192</link>
      <description>&lt;P&gt;Hi，&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/233839"&gt;@bluey2ks&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I thinks the following link can help you:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/iMX-and-Vybrid-Support/i-MX-8X-WebGL-not-working-when-using-WPE-Webkit-s-ANGLE-backend/m-p/1806655" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/iMX-and-Vybrid-Support/i-MX-8X-WebGL-not-working-when-using-WPE-Webkit-s-ANGLE-backend/m-p/1806655&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="pengyong_zhang_0-1716793637525.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/280922i6C4399DDF33961E1/image-size/medium?v=v2&amp;amp;px=400" role="button" title="pengyong_zhang_0-1716793637525.png" alt="pengyong_zhang_0-1716793637525.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;pengyong_zhang_0-1716793637525.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R&lt;/P&gt;</description>
      <pubDate>Mon, 27 May 2024 07:07:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mplus-webgl-not-running-issue/m-p/1875276#M224192</guid>
      <dc:creator>pengyong_zhang</dc:creator>
      <dc:date>2024-05-27T07:07:27Z</dc:date>
    </item>
  </channel>
</rss>