<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Can UART3 in the iMX6 SDK function as Debug Uart ?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-UART3-in-the-iMX6-SDK-function-as-Debug-Uart/m-p/249075#M22377</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Oswald&lt;/P&gt;&lt;P&gt;This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Jul 2014 03:12:58 GMT</pubDate>
    <dc:creator>YixingKong</dc:creator>
    <dc:date>2014-07-02T03:12:58Z</dc:date>
    <item>
      <title>Can UART3 in the iMX6 SDK function as Debug Uart ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-UART3-in-the-iMX6-SDK-function-as-Debug-Uart/m-p/249073#M22375</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a board similar to the iMX6Q Sabre SDB. I have the debug serial port connected to UART3 (pins EIM_D24/25). I am running the "Platform SDK (1.1) for MX6DQ TO1.2 Smart Device (SD) rev. C" I use the IOMux tool to configure UART3 on EIM_D24/25 pins. And in the source code to use UART3 as the debug uart. When I power up the board the Test Menu is displayed but my typed response is ignored. It appears as if the RX pin is not configured properly. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Feb 2014 17:18:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-UART3-in-the-iMX6-SDK-function-as-Debug-Uart/m-p/249073#M22375</guid>
      <dc:creator>os</dc:creator>
      <dc:date>2014-02-20T17:18:37Z</dc:date>
    </item>
    <item>
      <title>Re: Can UART3 in the iMX6 SDK function as Debug Uart ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-UART3-in-the-iMX6-SDK-function-as-Debug-Uart/m-p/249074#M22376</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Oswald&lt;/P&gt;&lt;P&gt;We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow resolved the issue, can we close the discussion? If you still need help, please feel free to reply with an update to this discussion.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jun 2014 05:32:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-UART3-in-the-iMX6-SDK-function-as-Debug-Uart/m-p/249074#M22376</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-06-10T05:32:09Z</dc:date>
    </item>
    <item>
      <title>Re: Can UART3 in the iMX6 SDK function as Debug Uart ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-UART3-in-the-iMX6-SDK-function-as-Debug-Uart/m-p/249075#M22377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Oswald&lt;/P&gt;&lt;P&gt;This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yixing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jul 2014 03:12:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-UART3-in-the-iMX6-SDK-function-as-Debug-Uart/m-p/249075#M22377</guid>
      <dc:creator>YixingKong</dc:creator>
      <dc:date>2014-07-02T03:12:58Z</dc:date>
    </item>
  </channel>
</rss>