<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: USB OTG Port as USB Host on Sabre-SD card...</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-Port-as-USB-Host-on-Sabre-SD-card/m-p/248796#M22336</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Make sure the USBOTG ID pin (#4) is connected to GND in order to make an OTG port as host (officially "A-device"). The micro-AB to USB-A conversion connector I got as part of Emerge USB conversion kit has apparently open ID pin, making USB OTG port as device (officially "B-device").&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Feb 2013 17:56:08 GMT</pubDate>
    <dc:creator>YS</dc:creator>
    <dc:date>2013-02-11T17:56:08Z</dc:date>
    <item>
      <title>USB OTG Port as USB Host on Sabre-SD card...</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-Port-as-USB-Host-on-Sabre-SD-card/m-p/248794#M22334</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have not been able to get the USB OTG port on my Sabre-SD card to work as a USB host. It clearly works when I get the MfGTools v2 working but I believe it is a client in this mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I plug in my Belkin hub with a mouse and keyboard attached they are not recognized. Any help in getitng these up and running would be greatly apprecaited.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Feb 2013 17:06:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-Port-as-USB-Host-on-Sabre-SD-card/m-p/248794#M22334</guid>
      <dc:creator>KeithSugawara</dc:creator>
      <dc:date>2013-02-05T17:06:13Z</dc:date>
    </item>
    <item>
      <title>Re: USB OTG Port as USB Host on Sabre-SD card...</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-Port-as-USB-Host-on-Sabre-SD-card/m-p/248795#M22335</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;What you need is adapter: USB Type A female to USB micro A male.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;This is the one I used succesfully:&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;A href="http://www.kauppasatama.fi/?tuote=USB-74&amp;amp;cid=332200"&gt;http://www.kauppasatama.fi/?tuote=USB-74&amp;amp;cid=332200&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Feb 2013 18:04:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-Port-as-USB-Host-on-Sabre-SD-card/m-p/248795#M22335</guid>
      <dc:creator>VladanJovanovic</dc:creator>
      <dc:date>2013-02-05T18:04:50Z</dc:date>
    </item>
    <item>
      <title>Re: USB OTG Port as USB Host on Sabre-SD card...</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-Port-as-USB-Host-on-Sabre-SD-card/m-p/248796#M22336</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Make sure the USBOTG ID pin (#4) is connected to GND in order to make an OTG port as host (officially "A-device"). The micro-AB to USB-A conversion connector I got as part of Emerge USB conversion kit has apparently open ID pin, making USB OTG port as device (officially "B-device").&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Feb 2013 17:56:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-Port-as-USB-Host-on-Sabre-SD-card/m-p/248796#M22336</guid>
      <dc:creator>YS</dc:creator>
      <dc:date>2013-02-11T17:56:08Z</dc:date>
    </item>
  </channel>
</rss>