<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX7 OTP</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-OTP/m-p/1857977#M223204</link>
    <description>&lt;P&gt;Dear NXP Support,&lt;/P&gt;&lt;P&gt;This question pertains to the cl-som-imx7 board.&lt;/P&gt;&lt;P&gt;According to the i.MX-7Dual reference manual, OTP Bank 14 (OCOTP_GPXX) can be used to store general-purpose data, but this only fits 16 bytes.&lt;/P&gt;&lt;P&gt;We would like to know if we could use any other banks/words for storing our own arbitrary data. Some potential options could be:&lt;/P&gt;&lt;P&gt;- Bank 15 is dedicated to some sort of CRC key, but is suffixed GP (OCOTP_CRC_GPXX)&lt;/P&gt;&lt;P&gt;- Banks 12-13 and Banks 24-29 are zeroed, but are not mentioned at all in the reference manual&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in avances,&lt;/P&gt;&lt;P&gt;Valentin.&lt;/P&gt;</description>
    <pubDate>Wed, 01 May 2024 13:30:53 GMT</pubDate>
    <dc:creator>vraevsky</dc:creator>
    <dc:date>2024-05-01T13:30:53Z</dc:date>
    <item>
      <title>i.MX7 OTP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-OTP/m-p/1857977#M223204</link>
      <description>&lt;P&gt;Dear NXP Support,&lt;/P&gt;&lt;P&gt;This question pertains to the cl-som-imx7 board.&lt;/P&gt;&lt;P&gt;According to the i.MX-7Dual reference manual, OTP Bank 14 (OCOTP_GPXX) can be used to store general-purpose data, but this only fits 16 bytes.&lt;/P&gt;&lt;P&gt;We would like to know if we could use any other banks/words for storing our own arbitrary data. Some potential options could be:&lt;/P&gt;&lt;P&gt;- Bank 15 is dedicated to some sort of CRC key, but is suffixed GP (OCOTP_CRC_GPXX)&lt;/P&gt;&lt;P&gt;- Banks 12-13 and Banks 24-29 are zeroed, but are not mentioned at all in the reference manual&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in avances,&lt;/P&gt;&lt;P&gt;Valentin.&lt;/P&gt;</description>
      <pubDate>Wed, 01 May 2024 13:30:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7-OTP/m-p/1857977#M223204</guid>
      <dc:creator>vraevsky</dc:creator>
      <dc:date>2024-05-01T13:30:53Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX7 OTP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX7-OTP/m-p/1859109#M223290</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The only fuse banks that are used for general porpoise are OCOTP_GP.&lt;/P&gt;
&lt;P&gt;OCOTP_CRC_GP is used exclusively for Cyclic Redundancy Checking functions.&lt;/P&gt;
&lt;P&gt;In the case of undocumented fuse banks you are referring, we do not recommend to read/write on them since we cannot determinate the behavior after do it.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Fri, 03 May 2024 20:31:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX7-OTP/m-p/1859109#M223290</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2024-05-03T20:31:47Z</dc:date>
    </item>
  </channel>
</rss>