<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRunning Qt application on IMX8 MINI</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Running-Qt-application-on-IMX8-MINI/m-p/1856143#M223078</link>
    <description>&lt;P&gt;Hi, I've built a minimal Yocto image for imx8 mini with Qt6 and&amp;nbsp;&lt;STRONG&gt;fsl-imx-xwayland&amp;nbsp;&lt;/STRONG&gt;and&amp;nbsp;&lt;STRONG&gt;fsl-imx-wayland&lt;/STRONG&gt;&amp;nbsp;as the distro and there is a Qt/Qml application to be run on the board. I have tried a bunch of different configs yet I had no success in running the application. It only runs on &lt;EM&gt;linuxfb&amp;nbsp;&lt;/EM&gt;but I'm trying to run it using either&amp;nbsp;&lt;EM&gt;eglfs&lt;/EM&gt;,&amp;nbsp;&lt;EM&gt;x11&lt;/EM&gt; or&amp;nbsp;&lt;EM&gt;wayland&lt;/EM&gt;. All are complaining about not finding and connecting the display.&amp;nbsp;&amp;nbsp;How can I run this application on the board using one of the mentioned plugins?&amp;nbsp;&lt;/P&gt;&lt;P&gt;P.S: I am installing&amp;nbsp;&lt;EM&gt;qtwayland&lt;/EM&gt; on the image, I'm also using a bbappend file to enagle opengles for qtbase and the plugins seems to be built and added with no problem.&lt;/P&gt;</description>
    <pubDate>Sun, 28 Apr 2024 04:32:02 GMT</pubDate>
    <dc:creator>Alirezah95</dc:creator>
    <dc:date>2024-04-28T04:32:02Z</dc:date>
    <item>
      <title>Running Qt application on IMX8 MINI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Running-Qt-application-on-IMX8-MINI/m-p/1856143#M223078</link>
      <description>&lt;P&gt;Hi, I've built a minimal Yocto image for imx8 mini with Qt6 and&amp;nbsp;&lt;STRONG&gt;fsl-imx-xwayland&amp;nbsp;&lt;/STRONG&gt;and&amp;nbsp;&lt;STRONG&gt;fsl-imx-wayland&lt;/STRONG&gt;&amp;nbsp;as the distro and there is a Qt/Qml application to be run on the board. I have tried a bunch of different configs yet I had no success in running the application. It only runs on &lt;EM&gt;linuxfb&amp;nbsp;&lt;/EM&gt;but I'm trying to run it using either&amp;nbsp;&lt;EM&gt;eglfs&lt;/EM&gt;,&amp;nbsp;&lt;EM&gt;x11&lt;/EM&gt; or&amp;nbsp;&lt;EM&gt;wayland&lt;/EM&gt;. All are complaining about not finding and connecting the display.&amp;nbsp;&amp;nbsp;How can I run this application on the board using one of the mentioned plugins?&amp;nbsp;&lt;/P&gt;&lt;P&gt;P.S: I am installing&amp;nbsp;&lt;EM&gt;qtwayland&lt;/EM&gt; on the image, I'm also using a bbappend file to enagle opengles for qtbase and the plugins seems to be built and added with no problem.&lt;/P&gt;</description>
      <pubDate>Sun, 28 Apr 2024 04:32:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Running-Qt-application-on-IMX8-MINI/m-p/1856143#M223078</guid>
      <dc:creator>Alirezah95</dc:creator>
      <dc:date>2024-04-28T04:32:02Z</dc:date>
    </item>
    <item>
      <title>Re: Running Qt application on IMX8 MINI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Running-Qt-application-on-IMX8-MINI/m-p/1856813#M223118</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;This can help:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/How-to-build-QT5-base-image-for-i-MX8MM-evk-board/td-p/944130" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/How-to-build-QT5-base-image-for-i-MX8MM-evk-board/td-p/944130&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Mon, 29 Apr 2024 14:52:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Running-Qt-application-on-IMX8-MINI/m-p/1856813#M223118</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-04-29T14:52:26Z</dc:date>
    </item>
  </channel>
</rss>