<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: How fast is imxcompositor_g2d</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-fast-is-imxcompositor-g2d/m-p/1853537#M222918</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The limit is due to your framework you have to use the gpu for obtain more fps but in this case apparently the camera framework is going to dev/video0 devices.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Wed, 24 Apr 2024 14:55:00 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2024-04-24T14:55:00Z</dc:date>
    <item>
      <title>How fast is imxcompositor_g2d</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-fast-is-imxcompositor-g2d/m-p/1852729#M222872</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;SPAN&gt;I'm using an imx8mp on a variscite dart board and a basler camera.&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;I'm trying to merge an appsrc defined overlay with a video from the basler camera with an&amp;nbsp;imxcompositor_g2d. When I push up buffers to the appsrc the framerate is very low, about 15 fps while not pushing up the buffer displays the video at 55 fps through my current pipeline. One of the things I was wondering about is how fast is the compositor? The outputed video will have to run at 90 fps and the video from the camera is 1280x960. What are the limits of the overlay I can have for the compositor to successfully merge at 90 fps and how would a pipeline that does that look?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 23 Apr 2024 17:58:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-fast-is-imxcompositor-g2d/m-p/1852729#M222872</guid>
      <dc:creator>itaigolan</dc:creator>
      <dc:date>2024-04-23T17:58:23Z</dc:date>
    </item>
    <item>
      <title>Re: How fast is imxcompositor_g2d</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-fast-is-imxcompositor-g2d/m-p/1853537#M222918</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The limit is due to your framework you have to use the gpu for obtain more fps but in this case apparently the camera framework is going to dev/video0 devices.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 24 Apr 2024 14:55:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-fast-is-imxcompositor-g2d/m-p/1853537#M222918</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-04-24T14:55:00Z</dc:date>
    </item>
    <item>
      <title>Re: How fast is imxcompositor_g2d</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-fast-is-imxcompositor-g2d/m-p/1853850#M222936</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for your response, if it makes a difference, we are actually using dev/video2. What do you mean that the camera framework is going to dev/video2? Is there a way for me to force it to use the gpu?&lt;/P&gt;</description>
      <pubDate>Wed, 24 Apr 2024 19:41:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-fast-is-imxcompositor-g2d/m-p/1853850#M222936</guid>
      <dc:creator>itaigolan</dc:creator>
      <dc:date>2024-04-24T19:41:50Z</dc:date>
    </item>
  </channel>
</rss>